element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum esp32 C3 with mpu6050
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 141 subscribers
  • Views 8443 views
  • Users 0 members are here
  • projects
  • mpu6050
  • Embedded Systems
  • ESP32C3
Related

esp32 C3 with mpu6050

alen10
alen10 over 2 years ago

Hi , i saw this video : www.youtube.com/watch . I want to know if i could use esp32 c3 instead of what you are using in the video . In this case , can you specify the pin diagram in order to connect to mpu6050 ?.

Below is the image of my connection (esp32 C3) with MPU6050 

Code is :

#include <MPU6050_light.h>
MPU6050 mpu(Wire);
unsigned long timer = 0;
#include <BleMouse.h>

BleMouse bleMouse;

#define btnL 2
#define btnR 1
#define btnM 3


#include <Wire.h>
#define SDA 9
#define SCL 10

#define AD0 11
#define INT 12
void setup() {

pinMode(btnR,INPUT);
pinMode(btnL,INPUT);
pinMode(btnM,INPUT);

pinMode(INT, INPUT); //int goes high when activity is detected(wakeup?)
pinMode(AD0, OUTPUT);
digitalWrite(AD0, LOW);//sets I2C adress
delay(50);
Serial.begin(115200);
Wire.begin(SDA,SCL);

Serial.println("Starting BLE work!");
bleMouse.begin();
byte status = mpu.begin();
Serial.print(F("MPU6050 status: "));
Serial.println(status);
while(status!=0){ } // stop everything if could not connect to MPU6050

Serial.println(F("Calculating offsets, do not move MPU6050"));
delay(2000);
// mpu.upsideDownMounting = true; // uncomment this line if the MPU6050 is mounted upside-down
mpu.calcOffsets(); // gyro and accelero
Serial.println("Done!\n");
}

void loop() {
if(bleMouse.isConnected()) {
clicking();
mpu.update();
int x = map(mpu.getAngleX(),-90,90,10,-10);
int y = map(mpu.getAngleY(),-90,90,-10,10);
int z = map(mpu.getAngleZ(),-90,90,-10,10);

bleMouse.move(x,y);


if((millis()-timer)>10){ // print data every 10ms
Serial.print("X : ");
Serial.print(mpu.getAngleX());
Serial.print(x);
Serial.print("\tY : ");
Serial.print(mpu.getAngleY());
Serial.print(y);
Serial.print("\tZ : ");
Serial.println(mpu.getAngleZ());
Serial.print(z);

timer = millis();
}
}


}
void clicking(){

bool Lclick = digitalRead(btnL);
bool Mclick = digitalRead(btnM);
bool Rclick = digitalRead(btnR);
if (Lclick == 0){
bleMouse.click(MOUSE_LEFT);
}

if (Rclick == 0){
bleMouse.click(MOUSE_RIGHT);
}


if (Mclick == 0){
bleMouse.click(MOUSE_MIDDLE);
}

}



image                                     image

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 2 years ago in reply to alen10 +1 suggested
    alen10 said: esp32 c3 mini development kit .Even shared the picture of it Hey alen10 , Looks like you have one of these? https://docs.espressif.com/projects/esp-idf/en/stable/esp32c3/hw-reference/esp32c3…
Parents
  • mayermakes
    0 mayermakes over 2 years ago

    there is no requirement to use the s3 like in the video it will also work with a C3, you only need to specify and connect the right pins for i2C.
    so either use the pinmux to define which pins are used for SDA&SCL by the wire library or look up the default i2c pins for your particular board(which appears to be some random clone board so that might be not the simplest to find out.) and connect to these.
    also check if the breakout board you are using has the pullop resistors for i2c fitted, if not you nalso need to add them in your config/physically.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mayermakes
    0 mayermakes over 2 years ago in reply to mayermakes
    mayermakes said:
    so either use the pinmux to define which pins are used for SDA&SCL by the wire library
    Wire.begin(SDA, SCL);


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mayermakes
    0 mayermakes over 2 years ago in reply to mayermakes
    mayermakes said:
    so either use the pinmux to define which pins are used for SDA&SCL by the wire library
    Wire.begin(SDA, SCL);


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • alen10
    0 alen10 over 2 years ago in reply to mayermakes

    Hi , The SDA and SCL connection had been solved .

    I got the virtual mouse working with my smartphone .

    I am doing a  project . The Project is based on Finger module that has esp32 C3 and mpu6050 attached to my Index Finger  .In the prototype , I do not need button to click the screen . It will be done using my finger movement along the Z direction .I can  move the mouse cursor  along (X-Y direction )  and scrolling too with my finger module attached to my finger  . 

    I will attach my code , Can you tell me if the code is correct or not ? 

    Secondly i used  "int x = map(mpu.getAngleX(),-90,90,0,255)" instead of "int x = map(mpu.getAngleX(),-90,90,-10,10)" , Can you tell me which one is good for precise cursor control and without timelag . If timelag shows up , how can i avoid it by either using hardware /Software ?

    #include <MPU6050_light.h>
    MPU6050 mpu(Wire);
    unsigned long timer = 0;
    #include <BleMouse.h>
    #define MPU_ADDR 0x68 
     
    BleMouse bleMouse;
    
    
    int prevX = 0, prevY = 0, prevZ = 0; // Previous sensor readings for movement detection
    // Thresholds for click and scroll detection (adjust as needed)
    #define CLICK_THRESHOLD 1000
    
    
    #include <Wire.h>
    int SDA_pin= 6;
    int Scl_pin= 7;
    
    //#define AD0 11 
    //#define INT 12
    void setup() {
      //pinMode(INT, INPUT); //int goes high when activity is detected(wakeup?)
      //pinMode(AD0, OUTPUT);
      //digitalWrite(AD0, LOW);//sets I2C adress
      delay(50);
      Serial.begin(115200);
      Wire.setPins(SDA_pin ,Scl_pin);
        pinMode(SDA_pin,INPUT_PULLUP );
     
       pinMode(Scl_pin,INPUT_PULLUP );
      Wire.begin();
    
      Serial.println("Starting BLE work!");
      bleMouse.begin();
      byte status = mpu.begin();
      Serial.print(F("MPU6050 status: "));
      Serial.println(status);
      while(status!=0){ } // stop everything if could not connect to MPU6050
      
      Serial.println(F("Calculating offsets, do not move MPU6050"));
      delay(2000);
      // mpu.upsideDownMounting = true; // uncomment this line if the MPU6050 is mounted upside-down
      mpu.calcOffsets(); // gyro and accelero
      Serial.println("Done!\n");
      }
      
    
    void loop() {
      if(bleMouse.isConnected()) {
        Wire.write(0x3B); 
        Wire.write(0x43); 
     
      mpu.update();
      int x = map(mpu.getAngleX(),-90,90,0,255);
      int y = map(mpu.getAngleY(),-90,90,0,255);
      int z =abs(mpu.getAngleZ());
      prevX = x;
      prevY =y;
      
       bleMouse.move(x,y);
        // Click detection based on Z-axis acceleration change
        if (z > CLICK_THRESHOLD && prevZ < CLICK_THRESHOLD) {
         bleMouse.click();
          delay(10); // Debounce (optional)
         
        }
        prevZ = z;
        // Scrolling 
             Serial.println("Scroll up");
             unsigned long startTime;
      startTime = millis();
        while(millis()<startTime+2000) {
          bleMouse.move(0,0,1);
          delay(100);
        }
        delay(500);
    
        Serial.println("Scroll down");
        startTime = millis();
        while(millis()<startTime+2000) {
          bleMouse.move(0,0,-1);
          delay(100);
        }
        delay(500);
    
        Serial.println("Scroll left");
        startTime = millis();
        while(millis()<startTime+2000) {
          bleMouse.move(0,0,0,-1);
          delay(100);
        }
        delay(500);
    
        Serial.println("Scroll right");
        startTime = millis();
        while(millis()<startTime+2000) {
          bleMouse.move(0,0,0,1);
          delay(100);
        }
        delay(500);
    
    
      
      
      if((millis()-timer)>10){ // print data every 10ms
      Serial.print("X : ");
      Serial.print(mpu.getAngleX());
      Serial.print(x);
      Serial.print("\tY : ");
      Serial.print(mpu.getAngleY());
      Serial.print(y);
      Serial.print("\tZ : ");
      Serial.println(mpu.getAngleZ());
      Serial.print(z);
      
      timer = millis();  
      }
      }}