element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum modernizing the heathkit hero 2000, hero 1, and hero jr with modern day parts
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 150 subscribers
  • Views 9243 views
  • Users 0 members are here
Related

modernizing the heathkit hero 2000, hero 1, and hero jr with modern day parts

mr-robot5
mr-robot5 over 7 years ago

I am sure people have thought about this as I have, taking the old hero robots from the 80's and rebuilding them with modern day parts that one can get from radioshack or something.

 

I was born in the 90's and discovered the hero robots from youtube a couple years ago and had been wanting to make my own version at home using modern day parts if anyone has an idea on how to accomplish this it would be amazing to see.

I have been wanting to make my own robot ever since I was a child and with computers becoming so small now and the parts easy to find it would be an awesome project for me and my father to do together.

  • Sign in to reply
  • Cancel

Top Replies

  • bippy
    bippy over 7 years ago +7
    Hello Tech Friends, This is my very first post on element14. I was part of a four person team who built a 1983 Heathkit HERO-1 Educational Robot you've heard so much about. My wife soldered together the…
  • bippy
    bippy over 7 years ago in reply to dougw +6
    I forgot to include a few snaps of my Heathkit Hero-1 Educational Robot in our living room (Just waiting to be programmed in HEX by the keypad. And perhaps soon updated to some new modern tech!). We built…
  • bippy
    bippy over 7 years ago in reply to 14rhb +3
    Hi Rod... Thank you kindly! The Heathkit Hero-1 Educational Robot was truly ahead of it's 1983 time, well engineered, clear kit building instructions and good background information on microprocessors…
  • ovonel
    ovonel over 7 years ago +3
    So far, I have spent a lot of time De-Yellowing my Hero 2000 (ET-19). See left side example below. The front lower section still has to be De-Yellowed, but I left it till last since it was yellowed almost…
  • shabaz
    shabaz over 7 years ago +2
    Hi, There are many robot projects on this site, although they're not exact replacements or modifications to the Hero series. However, there have been some discussions about those robots, in case that helps…
  • mayermakes
    mayermakes over 7 years ago +2
    I actually like the Idea, I was not aware of these robots until now. Can it be that you also commented this idea on one of our videos on youtube? Am I right?
  • dougw
    dougw over 7 years ago in reply to bippy +2
    That is a great story. I sure we all would like to see picture or video of it in action. If you still have any documentation from the build, that would help a lot with suggestions.
  • just4mrg
    just4mrg over 7 years ago in reply to bippy +2
    Beautiful David. Just recently bought a very good condition HERO 1 and am having a blast learning. Oh the usual repairs (Broken wire, cracked 12 pin connector, new batteries, etc.). But when I fired him…
  • just4mrg
    just4mrg over 7 years ago in reply to ovonel +2
    Wow - a HERO 2000. Only about 50 of those were produced. Maybe one day.....for now I'm just starting to learn my (new to me HERO 1) and having an absolute blast!
  • beacon_dave
    beacon_dave over 7 years ago in reply to dougw +2
    Stumbled across this 1984 archive video footage of a HERO 1 robot recently on the BBC Computer Literacy Project. It includes an introduction to the HERO 1 robot by Jim Bartley of the Heath company, at…
Parents
  • ovonel
    ovonel over 7 years ago

    So far, I have spent a lot of time De-Yellowing my Hero 2000 (ET-19).   See left side example below.

     

    imageimage

    The front lower section still has to be De-Yellowed, but I left it till last since it was yellowed almost not at all.

    The side panels and the upper sections are now complete. It took a lot of work to get rid of the orange/yellow.

    Despite its age, everything is still up and going.    Modernizing will have to wait till I catch my breath.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jbashfield
    jbashfield over 6 years ago in reply to ovonel

    Hi I am also in the process of modernising the Hero 2000 and was really impressed how you de yellowed it! Is there any chance you could share how you did it,I would be very grateful.

    I cannot decide if the best way to modernize it, either to up grade the whole motherboard with new graphics and CPU or just to restore the original components with faster ones where possible.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ovonel
    ovonel over 6 years ago in reply to jbashfield

    To de-yellow the plastic, I used ice cream.    LOL 

     

    It's called "Ice Cream 40". It is a hair bleach product that contains 12% Hydrogen Peroxide.

    Lots of other hair bleach products are out there that also contain 12% Hydrogen Peroxide.

     

    Normally one would use ultraviolet light to assist in this Hydrogen Peroxide bleaching method, but instead I simply used a couple of cheap regular shaped Luminus "Daylight" led bulbs (15 watt, 1500LM, 5000 K Color Temp).  I purchased these at the Dollar store. Nothing expensive there.  The "Ice Cream 40"  was purchased at Shoppers Drug Mart.

     

    The bleaching procedure was to first coat the yellowed plastic with a layer of the "Ice Cream 40", and then cover that with your typical kitchen "Plastic Wrap" to prevent the "Ice Cream 40" from drying up. Try to keep the thickness of the Ice Cream 40 evenly distributed.  Next, typically working of course with just one plastic piece at a time, I placed the plastic in my kitchen stainless steel sink, since it reflects light.  After that I had two LED bulbs hanging just above the sink, and then I used additional " Tin Foil " placed over the sink to help trap the light in the sink via reflection.

     

    Another way to do it would be to line the walls, top, and bottom of a box, with Tin Foil.   Again have a couple of LED bulbs hanging from the top.   Of course those hot bulbs would best be kept at a safe distance from the box top itself.  Anyhow, It took from 6 to 8 hours for the bleaching to finish.  Of course there were times that I had to do some additional work to de-yellow some spots or edges that still were a tad bit yellow.

     

    Good Luck.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • airbornesurfer
    airbornesurfer over 6 years ago in reply to ovonel

    How were your results retrobrighting with the salon creme? A lot of us in the retro refurb scene have switched over to immersion because the creme would give splotchy or otherwise mixed results. A friend of mine has a HERO1 that we've been planning to get up and running, but alas! COVID has proven to be quite the obstacle!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • airbornesurfer
    airbornesurfer over 6 years ago in reply to ovonel

    How were your results retrobrighting with the salon creme? A lot of us in the retro refurb scene have switched over to immersion because the creme would give splotchy or otherwise mixed results. A friend of mine has a HERO1 that we've been planning to get up and running, but alas! COVID has proven to be quite the obstacle!