element14 presents
  • Challenges & Projects
  • More
element14 presents
Files Episode 573: Using a Pi Pico to Convert Keyboard Input to Morse Code Supplemental File
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
  • Author Author: cstanton
  • Views 2264 views
  • Downloads 79 downloads
  • Likes 0 likes
  • Comments 11 comments
Related
Recommended

Episode 573: Using a Pi Pico to Convert Keyboard Input to Morse Code Supplemental File

As used in Episode 573: Using a Pi Pico to Convert Keyboard Input to Morse Code.

Please create an account and/or login to see the ability to download this file if you do not see the Download button.

  • episode 573
  • supplemental content
cstanton
cstanton
  • 14 Oct 2022
  • 79 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply
  • Winters6
    Winters6 over 1 year ago

    This is great. Thank you for the video. Now don't have to reinvent the wheel. I already bought a keyboard and Pico. My purpose is to actually let the pins of the Pico fire off the trs tip and ring respectively and thus allow the keyboard to be a keyer for my radio. I'm hoping the code you have will allow the pins to do this. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stefanT64
    stefanT64 over 2 years ago

    Arduino project on pico for morse code with some changes works almost excellent with USB keyboard now after changing USB KEYCODE TO ASCII to match used keyboard for swedish special letters etc.
    This with possibility to change speed and frequency of tone from keyboard clicks.
    Will finalize with a added battery internal and possibility to change volume from keyboard. Needs to be a boost to around 5V for my keyboard to work correct.
    This to get a standalone working keyboard with morse sound.
    Unfortunate keyboard+pico takes around 100mA in current so not optimal for battery since it will give short time until battery is empty.
    But,
    This morse keyboard is a great thing for my grandchildren to learn morse by using this keyboard.
    Thanks for the inspiration although the original code was not useful to me since I did not get this to work.
    73

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stefanT64
    stefanT64 over 2 years ago

    Using the debug probe I can confirm that host_cdc_mdc_hid works as expected when installed on pico
    Both when connecting a mouse and a keyboard it is recognized as right type
    And when typing on keyboard serial port prints on screen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to stefanT64

    If you have a spare Pico, you can use it as Picoprobe. The approach is documented in the SDK documentation.

    If you happen to have a XIAO Pico, we've ported Picoprobe firmware to that. See here:  Seeed Studio XIAO RP2040 as DebugProbe 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stefanT64
    stefanT64 over 2 years ago

    Yes, I have compiled all examples and loaded the UF2 of the project that You point to several times and it loads.
    But I have not found any description in documentation what expected result is for this code does. The only description I found is this page:
    https://forums.raspberrypi.com/viewtopic.php?t=348689

    I don't have a serial port connected now to pico now, I assume picoprobe will show status on  USB port when connected and print on serial port.
    Will connect picoprobe when it has arrived to me.

    btw
    I tried the Arduino project below on pico for morse code on a LED and it worked and lights the LED as expected after some minor changes.
    It does not have the reading from USB port of course.
    https://www.arduino.cc/education/morse-code-project
    Might be my base for the morse code for keyboard...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>