The Electronics Inside
  • Challenges & Projects
  • element14 presents
  • The Electronics Inside
  • More
  • Cancel
The Electronics Inside
Blog Brother CE-650/EM-411/Xerox Memowriter Electronic Typewriter Teardown
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Electronics Inside to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 7 May 2022 10:04 PM Date Created
  • Views 7629 views
  • Likes 8 likes
  • Comments 6 comments
  • typewritter
  • brother
  • the electronics inside
Related
Recommended

Brother CE-650/EM-411/Xerox Memowriter Electronic Typewriter Teardown

javagoza
javagoza
7 May 2022
Brother CE-650/EM-411/Xerox Memowriter Electronic Typewriter Teardown

When watching the last  MAYER MAKES episode by mayermakes, Using a Teletype Machine as a USB Printer with Arduino, I remembered last month I found an old electronic typewriter on the street.

With the help of beacon_dave and other members of the community I have been able to learn more about this electronic typewriter.

WilliamF has made a typewriter interface for another model, the AX-300: Demo video of the typewriter

Brother CE-650 Electronic Typewriter

The typewriter is a Brother CE-650 (Brother EM-411 in the USA and Canada) is the same typewriter as the Xerox Memowriter.

Brother CE'650 Typewriter

This printer had as an optional accessory an IF-60 module that allowed the electronic typewriter to be used as a computer printer or as a terminal connected to a modem.

image

image

Some parts of the typewriter are missing but it works fine.

A serial port for the  IF-60 module is located at the center and a manufacturer badge sits above the lower vent on the right.

image

image

The typewriter has interchangeable daisy wheels to change mechanically the font type and the character set.

image

Daisy Wheel with Prestige Italic font for Spanish character set, including the Ñ/ñ 

image

So time to watch what's inside.

Removing the cassette daisy wheel is very easy.

From Brother USA FAQs: To remove the cassette daisy wheel you have to pull the motor lock lever toward you to release it, then grasp the 'ear' of the cassette daisy wheel between your thumb and forefinger and simply pull it out. The cassette ribbon does not need to be removed in order to remove the cassette daisy wheel.

Inserting the new cassette daisy wheel. Grasping the 'ear' of the new cassette daisy wheel between your thumb and forefinger, slit it into the cassette guide slot and slide it in as far as it will go.

Now push the motor lock lever back toward the platen until it clicks into place. Do not force the lever. If you have any difficulty, recheck the cassette daisy wheel to ensure that it is properly set and try again.

NOTE: Be sure that the 'ear' of the cassette daisy wheel is to the right during insertion. Putting it in backwards can damage both the cassette daisy wheel and the motor mechanism.

If the cassette daisy wheel is not properly locked into position, the characters will not be properly typed.

image

Cassette ribbon

Teardown

There are no screws visible anywhere, top or bottom. Only two inside the typewriter.

First remove the two screws [1] and [2]

image

image

Then you have to remove the roller. Press on the loops and pull out.

image

Remove the left cylinder knob then. Press on the loops and pull out.

image

Extract the cylinder or platen.

image

Before you can remove the case completely, you have to release the cable that goes to the LCD display.

Unplug the ribbon cable, 2 in the figure

image

Use a plastic lever to release the top case. Start from the front under the keyboard.

image

Then continue with the back.

image

We already have access to the interior of the typewriter

image

image

image

image

In order to extract the driver board you have to unplug all the cables. The board is fixed to the chassis by only two screws.

image

This is the mainboard

image

image

The keyboard

Slide tabs aside to free up keyboard

image

image

image

Serial connector

With the machine off I have identified the pins that are connected to ground and with the machine on I have taken note of the voltages on each of the pins with respect to ground.

There is a pin where the voltmeter reads 37v.

image

This serial port opens many possibilities to use this printer connected to a microcontroller.

image

References

  • https://archive.org/details/brother-if-60/page/n3/mode/2up
  • https://etzone.org/2020/10/27/plugged-in-with-brother-compacts/
  • https://etzone.org/2019/08/10/xerox-takes-a-memo/
  • https://typewriterdatabase.com/Xerox.MemoWriter.659.bmys
  • https://www.searspartsdirect.com/model/201y8ytluf-001277/xerox-memowriter-office-parts
  • https://www.brother-usa.com/support/em
  • https://github.com/WRFleete/8bitOutBus-serial
  • https://www.youtube.com/watch?v=1OXD0xdS4pA

Conclusion

I still have many things to learn about this typewriter, I hope to be able to do a project with it later.

image

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 4 years ago +1
    The IF-60 interface appears to have been used on at least two other typewriter models, the Brother Pro 440 and the the Brother AX-20. If you can find documentation for either of these models then it…
  • mroggi
    mroggi over 3 years ago in reply to javagoza

    Thank you. I will give it a try and report back

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to mroggi

    I made a mistake and accidentally shorted it and it started to smell like burnt. I already gave up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mroggi
    mroggi over 3 years ago

    Hi, any update on the proprietary interface of the Brother-CE550? I would be very interested to learn if you have been able to connect to the interface in any way. Thanks, Matthias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Nice find! 

    I believe a lot of office machines were really well made, they were pricey and often with rental or maintenance contracts, so calling out a repair guy was undesirable!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago

    The IF-60 interface appears to have been used on at least two other typewriter models, the Brother Pro 440 and the the Brother AX-20. 

    If you can find documentation for either of these models then it could help.

    Here is a video of the IF-60 in use with the Pro 440:

    Brother Pro 440 Typewriter and IF-60 PC
    https://www.youtube.com/watch?v=IJFxAhEMkHQ

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>