The Electronics Inside
  • Challenges & Projects
  • element14 presents
  • The Electronics Inside
  • More
  • Cancel
The Electronics Inside
Forum Winner Announcement: Win a Xbox One S All-Digital Edition!!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Electronics Inside to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 61 replies
  • Subscribers 71 subscribers
  • Views 8989 views
  • Users 0 members are here
  • e14 community
  • e14presents
  • giveaway
  • past_contest
Related

Winner Announcement: Win a Xbox One S All-Digital Edition!!

rjena
rjena over 7 years ago

Meet David Edwards from the e14 presents show The Electronics Inside: a show where David tears down toys, tools, and electronic appliances just to find out what’s inside.

 

image

 

Watch our very first episode where David tears down Xbox One S All-Digital Edition.

 

You must wonder what happens to these devices after they are torn down. Well, if David manages to put it back together (and get it working) then we GIVEAWAY the device.

 

 

This month we are spicing things up by giving away David's torn down and rebuilt  XBOX one S All-Digital Edition to one lucky community member!

 

 

image

 

Rules to enter:

 

Step 1:  Log in or register on element14, it's easy and free.

 

Step 2: In the comments below, post a picture of a game, game controller, handheld or console that you have modified in any way(The project should be yours, not someone else's) AND tell us what would you do with the new Xbox one S all digital. The entry with the best combination of past achievement and future aspiration will win.

 

Step 3: You can enter this contest until midnight UTC 13th September 2019. Winners will be announced on 30th September 2019. If you need something to do between now and then make sure to check out all the great electronics videos at element14 presents

 

Follow these pages for more information:

  • The Electronics Inside
  • Xbox One S All Digital Teardown
  • Project Videos
  • Become a Video Content Producer for element14[VCP Program]
Attachments:
imagexbox_giveaway_TermsandConditions (1).pdf
  • Sign in to reply
  • Cancel

Top Replies

  • kellyhensen
    kellyhensen over 7 years ago +6
    players.brightcove.net/.../index.html The winner of the Xbox One S is gingerofoz !!!
  • dougw
    dougw over 7 years ago +5
    This is the very first PCB I designed for my own personal use. It was laid out using translucent red and blue tape plus black tape and via donuts - at 2X scale, then photographically reduced through colored…
  • memelord69
    memelord69 over 7 years ago +4
    Here is the Gameboy Color that I customised for my son. Nothing too drastic just a new glass screen and backlight. He mainly uses it to Play Pokemon Blu. I'd love to win the Xbox so that we can both play…
Parents
  • dougw
    dougw over 7 years ago

    This is the very first PCB I designed for my own personal use. It was laid out using translucent red and blue tape plus black tape and via donuts - at 2X scale, then photographically reduced through colored filters to obtain 1:1 PCB artwork layers for the print shop. The high cost of making mistakes with this method is probably why I am still so meticulous about getting my PCB layouts to work on the first attempt.

    The function of this circuit is to fit in-line with any joystick of the day (Atari, Sega, Colecovision, Commodore, etc.), which used DB9 connectors, and turn the trigger function into a rapid fire (machine gun) trigger.

    At the time all the action games and shoot-em-ups required the trigger button to be rapidly cycled to have any success. This often led to a sore trigger finger.

    The circuit still allowed single shots by "blipping" the trigger, but if the trigger was held down it would cycle the output at an optimal speed for hardware of the day.

    This little circuit led to many high scores without damage to my trigger finger.

    image

    I had visions of turning this circuit into a product, but eventually expensive joysticks came out with this feature built-in.

    At least that proved it was a good product idea.

    It would be interesting to see how the latest generation of kids (grandkids) fares with modern X-Box technology.

    There always seemed to be a gender bias in the types of games kids played and preferred. I am curious if this trend still persists. I am sure my granddaughter and grandson wouldn't "mind" the experiment.

    I "might" even have a go at it myself to see how the technology and game-play has improved. I am already putting together a retro PiCade so there would be something to compare it with even if I can't get my old hardware platforms functioning.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    This is the very first PCB I designed for my own personal use. It was laid out using translucent red and blue tape plus black tape and via donuts - at 2X scale, then photographically reduced through colored filters to obtain 1:1 PCB artwork layers for the print shop. The high cost of making mistakes with this method is probably why I am still so meticulous about getting my PCB layouts to work on the first attempt.

    The function of this circuit is to fit in-line with any joystick of the day (Atari, Sega, Colecovision, Commodore, etc.), which used DB9 connectors, and turn the trigger function into a rapid fire (machine gun) trigger.

    At the time all the action games and shoot-em-ups required the trigger button to be rapidly cycled to have any success. This often led to a sore trigger finger.

    The circuit still allowed single shots by "blipping" the trigger, but if the trigger was held down it would cycle the output at an optimal speed for hardware of the day.

    This little circuit led to many high scores without damage to my trigger finger.

    image

    I had visions of turning this circuit into a product, but eventually expensive joysticks came out with this feature built-in.

    At least that proved it was a good product idea.

    It would be interesting to see how the latest generation of kids (grandkids) fares with modern X-Box technology.

    There always seemed to be a gender bias in the types of games kids played and preferred. I am curious if this trend still persists. I am sure my granddaughter and grandson wouldn't "mind" the experiment.

    I "might" even have a go at it myself to see how the technology and game-play has improved. I am already putting together a retro PiCade so there would be something to compare it with even if I can't get my old hardware platforms functioning.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • a531016
    a531016 over 7 years ago in reply to dougw

    I can remember when consoles like the MegaDrive (Genesis) started having "turbo" buttons with just this functionality. Building your own with discreet hardware and etched PCB is a great mod though!

     

    Good Luck!