The Electronics Inside
  • Challenges & Projects
  • element14 presents
  • The Electronics Inside
  • More
  • Cancel
The Electronics Inside
Documents Classic Polaroid Instant Camera vs Instax -- The EIectronics Inside 21
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Electronics Inside to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 12 May 2020 6:13 PM Date Created
  • Last Updated Last Updated: 1 Apr 2020 7:24 AM
  • Views 2041 views
  • Likes 5 likes
  • Comments 3 comments
Related
Recommended

Classic Polaroid Instant Camera vs Instax -- The EIectronics Inside 21

element14 presents

element14 Presents  |  About David   |  Project Videos  |  The Electronics Inside

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Instant cameras have been around for a long time, but what has changed in 40 years of electronics to keep them going?

  • vintage tech
  • instax
  • instant camera
  • old electronics
  • polaroid
  • e14presents_davidedwards
  • the electronics inside
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +3
    I can remember the polaroid camera when it first came out. I never owned one but I did see it used and possibly, if my memory is correct, I might even have had my picture taken with it - but that could…
  • beacon_dave
    beacon_dave over 6 years ago +2
    There is a date reference to the 5000 SE as being a 1978 model: SX 70 Camera Museum, Netherlands The SE may stand for 'special edition' as opposed to 'second edition' ? I seem to recall that the shaking…
Parents
  • dubbie
    dubbie over 6 years ago

    I can remember the polaroid camera when it first came out. I never owned one but I did see it used and possibly, if my memory is correct, I might even have had my picture taken with it - but that could be wishful thinking. When they came out they were expensive which is probably the main reason I did not own one.

     

    But, what I did use is the ultrasonic rangefinder which you could purchase as a separate item. They were the rangefinder of choice for robotics in the 1980s and I had several on my first mobile robot, well , maybe just one. They were just fantastic, bearing in mind that there were no SRF04/08 modules in those days. I think they had a large range, probably over 8 feet (were we decimal/metric in 1980?) and because they has such a large transmitter/receiver they were very sensitive. I think they are effectively electrostatic speakers used to generate the ultrasonic chirrup - which did cause some problems when using them as they required a big current pulse to generate the ultrasonic burst, which would screw up all the other electronics so they needed careful handling. The board has a non-linear amplifier that increases the gain as time passes, probably proportionally with the dissipation of the ultrasonic burst power, which I think is what all the TI chips are for. I think it cost about £18 in 1980 - very expensive, but there was nothing to touch it. It even had an analogue output where you could see the analogue voltage from the receiver, which enabled some clever things to be done with signal processing. If you look at mobile robots and possibly other types of robots from that time, they will all (well mostly all) have Polaroid ultrasonic rangefinders and/or cameras .

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    I can remember the polaroid camera when it first came out. I never owned one but I did see it used and possibly, if my memory is correct, I might even have had my picture taken with it - but that could be wishful thinking. When they came out they were expensive which is probably the main reason I did not own one.

     

    But, what I did use is the ultrasonic rangefinder which you could purchase as a separate item. They were the rangefinder of choice for robotics in the 1980s and I had several on my first mobile robot, well , maybe just one. They were just fantastic, bearing in mind that there were no SRF04/08 modules in those days. I think they had a large range, probably over 8 feet (were we decimal/metric in 1980?) and because they has such a large transmitter/receiver they were very sensitive. I think they are effectively electrostatic speakers used to generate the ultrasonic chirrup - which did cause some problems when using them as they required a big current pulse to generate the ultrasonic burst, which would screw up all the other electronics so they needed careful handling. The board has a non-linear amplifier that increases the gain as time passes, probably proportionally with the dissipation of the ultrasonic burst power, which I think is what all the TI chips are for. I think it cost about £18 in 1980 - very expensive, but there was nothing to touch it. It even had an analogue output where you could see the analogue voltage from the receiver, which enabled some clever things to be done with signal processing. If you look at mobile robots and possibly other types of robots from that time, they will all (well mostly all) have Polaroid ultrasonic rangefinders and/or cameras .

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down