The Electronics Inside
  • Challenges & Projects
  • element14 presents
  • The Electronics Inside
  • More
  • Cancel
The Electronics Inside
Documents 1980's Cathode Ray Oscilloscope -- The EIectronics Inside 34
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Electronics Inside to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 26 Jan 2021 4:50 PM Date Created
  • Last Updated Last Updated: 28 Oct 2020 8:24 AM
  • Views 5880 views
  • Likes 7 likes
  • Comments 21 comments
Related
Recommended

1980's Cathode Ray Oscilloscope -- The EIectronics Inside 34

element14 presents

element14 Presents  |  About David   |  Project Videos  |  The Electronics Inside

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Most people will know an old tube TV, some will know tube oscilloscopes. But how many have seen the insides of a late 80s high quality scope? Will there be any surprises in this broken model?

  • tei
  • lab tech
  • scope
  • tektronix
  • cro
  • osciloscope
  • e14presents_davidedwards
  • the electronics inside
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 5 years ago +2
    Thanks for that. I've got a 2215, which is in the same series but has the addition of a B-sweep and B-trigger to the horizontal timebase, so it was interesting for me to see what's inside. Although everyone…
  • a531016
    a531016 over 5 years ago in reply to macona +1
    I'm sorry you are disapointed - I try and be knowledgeable as much as I can about a wide range of subjects - naturally this means that I can't be an expert on every topic and product. Thanks for the catch…
  • a531016
    a531016 over 5 years ago in reply to jc2048 +1
    Amazing - Thank you Jon! I have to admit, I love an old hand drawn drawing. I was looking at a building layout from 1978 a few weeks back, and it was revision P. I had to feel for the poor draftsman that…
Parents
  • jc2048
    jc2048 over 5 years ago

    Thanks for that. I've got a 2215, which is in the same series but has the addition of a B-sweep and B-trigger to the horizontal timebase, so it was interesting for me to see what's inside.

     

    Although everyone is saying the tube shield is mu-metal, in this case it's just steel. At least, that's what the service manual for mine says, and I'd imagine Tektronix knew what they made it out of.

     

    This service manual [so not necessarily the same as your 2213] says the delay down the delay line is 100ns. It doesn't seem to mention the differential characteristic impedance, but the series termination at the driver end is 73.2R and the parallel termination at the receiving end is 78.7R, so that gives us some idea [this is all so critical that it looks like those have been modified to take into account the additional effects of the transistors at each end].

     

    This is the symbol for the delay line. [The drawings were done by hand and are a work of art.]

     

     

    image

     

    At the receiving end, the circuit is like this. Look at all the compensation to get the response level.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • macona
    macona over 5 years ago in reply to jc2048

    Tek is pretty well know for using mu-metal in their scopes. The problem with a steel shield would be that it can retain a magnetic field and mess things up by itself. And generally steel is not a great magnetic shield. Its not like the part was something that was ever going to be replaced.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to macona

    Like you, I would have assumed it was mu-metal. I'm just reporting here what the service manual says. Perhaps I'm misunderstanding it or it was wrong.

     

    image

     

    image

     

    I think I've read somewhere that once you get up to about 100kHz, mu-metal is no more efficient at magnetic shielding than steel, so perhaps it's down to having a SMPS rather than the mains transformer. We might also indirectly be explaining why they had the mechanical linkage for the mains switch, rather than just running a mains cable to the front. Another possible factor is that this is very much a portable, service instrument, rather than one that would sit on a bench or ride around on a scope trolly, so degradation of the mu-metal from banging it around might have been a potential problem and could have spurred the development of an instrument that didn't need that level of shielding. As you say, though, that still leaves the problem of the steel magnetizing.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago in reply to macona

    Like you, I would have assumed it was mu-metal. I'm just reporting here what the service manual says. Perhaps I'm misunderstanding it or it was wrong.

     

    image

     

    image

     

    I think I've read somewhere that once you get up to about 100kHz, mu-metal is no more efficient at magnetic shielding than steel, so perhaps it's down to having a SMPS rather than the mains transformer. We might also indirectly be explaining why they had the mechanical linkage for the mains switch, rather than just running a mains cable to the front. Another possible factor is that this is very much a portable, service instrument, rather than one that would sit on a bench or ride around on a scope trolly, so degradation of the mu-metal from banging it around might have been a potential problem and could have spurred the development of an instrument that didn't need that level of shielding. As you say, though, that still leaves the problem of the steel magnetizing.