The Electronics Inside
  • Challenges & Projects
  • element14 presents
  • The Electronics Inside
  • More
  • Cancel
The Electronics Inside
Documents 1980's Cathode Ray Oscilloscope -- The EIectronics Inside 34
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Electronics Inside to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 26 Jan 2021 4:50 PM Date Created
  • Last Updated Last Updated: 28 Oct 2020 8:24 AM
  • Views 5893 views
  • Likes 7 likes
  • Comments 21 comments
Related
Recommended

1980's Cathode Ray Oscilloscope -- The EIectronics Inside 34

element14 presents

element14 Presents  |  About David   |  Project Videos  |  The Electronics Inside

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Most people will know an old tube TV, some will know tube oscilloscopes. But how many have seen the insides of a late 80s high quality scope? Will there be any surprises in this broken model?

  • tei
  • lab tech
  • scope
  • tektronix
  • cro
  • osciloscope
  • e14presents_davidedwards
  • the electronics inside
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 5 years ago +2
    Thanks for that. I've got a 2215, which is in the same series but has the addition of a B-sweep and B-trigger to the horizontal timebase, so it was interesting for me to see what's inside. Although everyone…
  • a531016
    a531016 over 5 years ago in reply to macona +1
    I'm sorry you are disapointed - I try and be knowledgeable as much as I can about a wide range of subjects - naturally this means that I can't be an expert on every topic and product. Thanks for the catch…
  • a531016
    a531016 over 5 years ago in reply to jc2048 +1
    Amazing - Thank you Jon! I have to admit, I love an old hand drawn drawing. I was looking at a building layout from 1978 a few weeks back, and it was revision P. I had to feel for the poor draftsman that…
  • jc2048
    jc2048 over 5 years ago

    Thanks for that. I've got a 2215, which is in the same series but has the addition of a B-sweep and B-trigger to the horizontal timebase, so it was interesting for me to see what's inside.

     

    Although everyone is saying the tube shield is mu-metal, in this case it's just steel. At least, that's what the service manual for mine says, and I'd imagine Tektronix knew what they made it out of.

     

    This service manual [so not necessarily the same as your 2213] says the delay down the delay line is 100ns. It doesn't seem to mention the differential characteristic impedance, but the series termination at the driver end is 73.2R and the parallel termination at the receiving end is 78.7R, so that gives us some idea [this is all so critical that it looks like those have been modified to take into account the additional effects of the transistors at each end].

     

    This is the symbol for the delay line. [The drawings were done by hand and are a work of art.]

     

     

    image

     

    At the receiving end, the circuit is like this. Look at all the compensation to get the response level.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • a531016
    a531016 over 5 years ago in reply to macona

    I'm sorry you are disapointed - I try and be knowledgeable as much as I can about a wide range of subjects - naturally this means that I can't be an expert on every topic and product.

     

    Thanks for the catch on the drum switch - although I would argue that the complexity and nature of these drum switch puts them firmly in a "grey" area (if you'll excuse the pun)?

     

    I often find that the discussions (and yes, ocassional corrections) that happen in the comments from these videos are some of the best parts. I have on multiple occasions had people that worked on the original product join and add amazing informaiton to the content. Please feel free to keep this going and educate me and others who may not have the existing knowledge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • macona
    macona over 5 years ago in reply to cavemanndave

    Yep, delay line, the Tek 519, which was the first 1hgz scope, used a massive delay line that took up almost half the width of the case, 125 ohm impedance input on this one. These were used to capture data during nuke testing.

    You can see the delay line in a photo on this page.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • macona
    macona over 5 years ago

    O-scope CRTs are electrostatically deflected, not magnetic. The metal tube around the CRT is mu-metal which helps stop external magnetic sources from messing with the electron beam.  

     

    Not rotary encoders, drum switches.

     

    It would be nice if they had someone that knew something about what they were talking about like on EEVblog or the SignalPath. There is just no educational value to this since he hardly understands what he is looking at.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • macona
    macona over 5 years ago in reply to DAB

    X-rays and gammas are the same thing, its just their source. X-rays are "man-made" gammas come from natural sources like decay of elements. There are usually differences in photon energy too, but its still just very energetic photons.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • a531016
    a531016 over 5 years ago in reply to DAB

    Thanks DAB - So much to talk about on this one, I couldn't possibly have fitted it all into one video!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • a531016
    a531016 over 5 years ago in reply to cavemanndave

    You are absolutely right - it is indeed a delay line, and I think DAB below was rigth, the position is mostly a convinience.

     

    An engineer that worked for Tecktronics in the 80s indeed confirmed in the comments over on youtube!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • a531016
    a531016 over 5 years ago in reply to navadeepganeshu

    It did loook a little like the Degauss line on the iMac G3, but that was around the screen, as opposed to the gun at the back? I think the answer is below:

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Great tear down.

     

    Yes, the old Tektronix scopes were built to work in all kinds of environments.

     

    FYI, all CRT's emit a wide range of photons up to and including X-rays, some levels of gamma rays over a very wide spectrum.

     

    My first thought on the coil was a delay line. It was probably put around the CRT neck just for convenience.

     

    The encoder switches were cool to see. Hopefully you also noted the gold plated contacts for reliable contact.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cavemanndave
    cavemanndave over 5 years ago

    Howdy!:

     

    The ”mystery cable coil" is a balanced, controlled impedance (I think its around 130 Ohms Zo) dual-core coaxial transmission line, with a precisely known propagation velocity that serves as a delay line AFTER the trigger pickoff and BEFORE the final Vertical Amplifier.

    It's purpose is to allow the Sweep to get started and the beam unblanked BEFORE the triggering event is displayed in the Vertical axis.

     

    It would have been fun to watch you troubleshoot and attempt repair, too.

     

    Cheers,

    Dave

     

     

    ETA:  The reason for the dual cores is that all the later amplification stages are fully differential to achieve maximum fidelity in the trace at the full bandwidth. CMD

     

    ETA 2: Check out schematics @ https://w140.com/tekwiki/wiki/Main_Page

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>