The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents DIY Desktop Fume Fan -- The Learning Circuit 18
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Aug 2018 2:45 PM Date Created
  • Last Updated Last Updated: 8 Aug 2018 7:24 AM
  • Views 3738 views
  • Likes 14 likes
  • Comments 6 comments
Related
Recommended

DIY Desktop Fume Fan -- The Learning Circuit 18

image

element14 Presents

Learn basic electronics, explore STEM subjects, get what you need to know to get started on electronics projects, and more.

Back to element14 Presents homepage image

The Learning Circuit
sudo Sergeant
The Ben Heck Show

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Solder fumes can be harmful to your health.  Luckily, Karen has a solution.  Build a desktop fan that keeps solder fumes away. You can salvage any old fan, as long as it’s DC, for this to work. To build this circuit, you’ll also need a nine volt battery or a twelve volt power supply, a power switch, an LED, and a resistor. You’ll need the resistor to power the LED, which means you’ll need to know the resistance value.  Karen goes over calculating the resistance value to use either the 9 volt or the 12 volt power supply.

 

Karen's Toolkit:

 

Product NamePart Link

PC fan, 12V DC 80mmx25mm

Buy NowBuy Now

Perfboard

Buy NowBuy Now

Board-To-Board Connector, 2.54 mm, 2 Contacts, Receptacle, 2212S Series, Through Hole, 1 Rows

Buy NowBuy Now

2x1 male header

Buy NowBuy Now

Toggle Switch, DPDT, Non Illuminated, On-On, Panel, 5 A

Buy NowBuy Now

LED, Red, Through Hole, 4mm, 20 mA, 2.1 V

Buy NowBuy Now

Rotary Potentiometer, 1 kohm, 200 mW, ± 20%

Buy NowBuy Now

2.1mm DC Power Connector, Jack

Buy NowBuy Now

AC/DC Power Supply, 12 V, 1 A

Buy NowBuy Now
Through Hole Resistor, 499 ohm, 250 mW, ± 1%Buy NowBuy Now

 

 

 

The resistor will go in line with the LED. Since this fan is rated for a voltage equal to or higher than the supply voltage, I don’t need to add any more resistance. I also want to be able to control the speed of my fan. This would normally be done using a 555 timer or another chip using PWM. To keep the circuit simple, we’re going to use just a potentiometer instead. It’s not the most efficient way to build this circuit, but it works. Potentiometers are variable resistors. If put in line between the battery and the fan, by adjusting the resistance, we also adjust the amount of voltage supplied to the fan, making it go slower or faster. If we put the LED indicator in series with the motor and potentiometer, it would also be supplied a varying voltage, which would cause it to burn out. We don’t want that, so here’s what we’re going to do.We’ll use a DPDT switch which will put the fan and the LED in parallel. The switch will be supplied the 9 or 12V on both poles. The resistor and LED are in one circuit while the potentiometer and motor are in another, both placed after the switch. This way, when the switch is turned on, both circuits are supplied the 9 or 12V.

 

 

 

9V Battery Circuit Diagram12V Battery Circuit Diagram
imageimage

 

 

 

 

 

9V Battery Wiring Diagram12V AC-DC Power Supply Wiring Diagram
imageimage

 

 

 

 

 

 

  • stem_projects
  • tlc
  • potentiometer
  • dc fan
  • e14presents_makerkaren
  • resistor project
  • fume extractor
  • fume away
  • fume extraction
  • solder fumes
  • thelearningcircuit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • makerkaren
    makerkaren over 8 years ago +5
    Hey folks! Since this is The Learning Circuit, I want to encourage learning. Is there anything you think I did WRONG in my circuit? What WOULD make it more efficient? How would you have built this fan…
  • snidhi
    snidhi over 8 years ago +2
    Funny one Karen I also need to make one these Cheers
  • snidhi
    snidhi over 8 years ago in reply to airbornesurfer +2
    or smells just like morning bacon....
Parents
  • 14rhb
    14rhb over 8 years ago

    Without any form of extraction or draft, solder fumes always seem to migrate towards the solderer's face.

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 8 years ago

    Without any form of extraction or draft, solder fumes always seem to migrate towards the solderer's face.

     

    Rod