The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents Types of Diodes -- The Learning Circuit 25
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 8 Oct 2018 8:10 PM Date Created
  • Last Updated Last Updated: 10 Oct 2018 7:24 AM
  • Views 4530 views
  • Likes 11 likes
  • Comments 9 comments
Related
Recommended

Types of Diodes -- The Learning Circuit 25

image

element14 Presents

Learn basic electronics, explore STEM subjects, get what you need to know to get started on electronics projects, and more.

Back to element14 Presents homepage image

The Learning Circuit
sudo Sergeant
The Ben Heck Show

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Diodes are semiconductor components that allow electric current to flow in one direction but not the other. In this episode, Karen reviews p-in junctions and talks about how they differ from other types of common diodes, such as schottky diodes, zener diodes,  LEDs (light emitting diodes), laser diodes, and photodiodes.

 

P-N junctions are considered your typical didoes. They have a p-n junction with a threshold voltage that has to be reached before current will flow through them. In silicon diodes, this is 0.7V. Once this is reached, the current will continue flowing. When hooked up backwards, in reverse bias, these diodes do not allow current to flow. If a diode is reverse bias, and it’s supplied with too much voltage, more than it’s breakdown voltage, it’ll “break-down” and current will flow through it in the wrong direction. Schottky diodes often look like typical diodes. But unlike p-n junction diodes, Schottky diodes have a metal-semiconductor junction. Silicon diodes require time for their depletion zone to grow and shrink when switching from allowing forward current to blocking reverse current. There’s a recovery time. Schottky junctions have no depletion zone. Because of their metal-semiconductor junction, Schottky diodes require virtually no recovery time and therefore have much faster switching speeds. This means they can handle switching current better and faster, which makes them useful in high frequency applications.They also have a lower forward voltage drop. Silicon diodes have a voltage drop of around 0.7V, but the voltage drop of Schottky diodes is between 0.15 V and 0.46 V. This means they lose less energy to heat, making them more efficient. Schottky diodes are not useful for all applications, as they can leak a small amount of current backwards. This could be problematic for certain circuits.

 

While Schottky diodes can let some voltage leak through backwards, zener diodes are designed to allow current to flow in both directions. The p-n junction of zener diodes is heavily doped, only a specific voltage, the Zener voltage (Vz) can pass through without damaging the diode. In reverse bias, current will not flow through until the zener voltage is reached, but the voltage will be limited to the zener voltage.  For example, a 3.3V zener diode will not allow current to flow until the supply voltage reaches 3.3V.  If it’s supplied with 2V, no current flows. However, this diode could be supplied with 5, 6, 9, 12 Volts and it will regulate the voltage output to 3.3V. Zeners can have zener breakdown voltages of anywhere from 1.8V all the way up to 200V.

 

imageimage

 

LEDs, light emitting diodes, use energy from the particles moving through the p-n junction to create light. They can do this because they are made with gallium arsenide. Unlike silicon diodes, diodes made with gallium arsenide release energy in the form of light or photons. Like other diodes, they typically have 2 leads, though these can vary in length depending on the manufacturer. LEDs come in a wide variety of packages. Through-hole LEDs can be 3mm, 5mm, 10mm. They can have round and square lenses. Lenses can be clear or colored. 5mm round ones are the most common through-hole LEDs.  Surface mount LEDs come in a variety of sizes as well. When choosing an LED, one of the first things you’ll look for is color, or wavelength. (Chart-VO) Here’s a chart of the color spectrum. Another choice you’ll have is beam angle or viewing angle. Beam angle is the amount of degrees where the light is visible. Depending on your application, you may want a narrow beam angle, like 10deg or a wide beam angle, like 120deg. Where common light bulbs are measured in watts or lumens, the brightness of LEDs is its luminous intensity and it is measured in millicandelas or mcd.  The higher the number, the brighter the light. A standard LED could have a luminous intensity of 7mcd, whereas a super bright LED could be 120mcd. LEDs can have a range of voltage and current ratings. They have both a minimum current and voltage required to function properly, or even at all, as well as a maximum voltage and current, that if surpassed, can shorten the life of the LED or burn it out completely.

 

imageimage

 

 

While LEDs emit incoherent light, laser diodes emit high-intensity, coherent light. They do this by having a P-I-N, or pin junction rather than the standard p-n junction. The PIN junction has the standard P-type and N-type regions we’re familiar with. But between them there is an area of undoped, or intrinsic, semiconductor. At the junction, in that intrinsic layer is where all the magic happens. When current flows through the diode, energy is released in the form of photons or light into that intrinsic layer. But it doesn’t stop there. In a laser diode, the p and n-type regions have polished, reflective ends, which causes the photons to reflect back and forth, hundreds of times, in that intrinsic layer. The photons eventually escape in the form of a laser beam. You can usually see where a laser hits a surface, but you can’t always see the laser beam itself. If you can see the laser beam, be extra careful. A high powered laser has the potential of causing permanent damage to your eyes.

 

imageimage

While LEDs and lasers emit light, Photodiodes sense light. Light contains energy particles known as photons. When light strikes the PN junction of a photodiode, the energy from the photons is transferred to the diode and creates free electron and hole pairs. Remember what happens when a diode is in reverse bias mode. The charges in the junction repel the holes towards the anode and the electrons towards the cathode. This usually restricts the flow of current. Energy is being introduced by way of the photons, so a current is created in reverse bias mode. This is called the photoelectric effect and the photodiode is considered to be in photoconductive mode. Photodiodes can also be used in zero bias or photovoltaic mode. This is where current is restricted, so the electron-hole pairs, and therefore the voltage builds up.  A photodiode’s response time gets slower the larger the photodiode gets.

  • logic
  • pin junction
  • photodiodes
  • light emitting diodes
  • stem_projects
  • p-i-n junction
  • tlc
  • purple led
  • e14presents_makerkaren
  • switches
  • circuit
  • laser diodes
  • p-n junction
  • battery
  • schottky diodes
  • zener voltage
  • zeners
  • green led
  • blue led
  • gallium arsenide
  • diodes
  • p-n junction diodes
  • silicon diodes
  • white led
  • thelearningcircuit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 8 years ago +6
    Nice summary. In case anyone's interested, there are even more types of diodes out there, but normally used in more specialist settings. One example is the PIN diode, which is useful in RF switching /…
  • makerkaren
    makerkaren over 8 years ago in reply to jw0752 +6
    You are correct. Sometimes I miss little details and sometimes I have to cut them for time. Last week I was working on a capacitor video script and spent an entire day rewriting sections to try to make…
  • shabaz
    shabaz over 8 years ago in reply to makerkaren +6
    I have to say, the animations are awesome. This is something not possible with old textbooks, and it was really cool seeing how the depletion zone varied in size in the diode animations in this video.…
  • inghernandez
    inghernandez over 7 years ago

    I really love it.
    !!Good job.!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 7 years ago in reply to auggie56

    I hadn't heard them called that before, but that's another name for Schottky diodes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • auggie56
    auggie56 over 7 years ago

    What is a hot carrier diode?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 8 years ago

    I love this explanation! Super thorough, but approachable! Thanks, Karen!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to makerkaren

    I have to say, the animations are awesome. This is something not possible with old textbooks, and it was really cool seeing how the depletion zone varied in size in the diode animations in this video.

    It actually helps understand other diode technologies too - e.g. varicap diodes, where that is a clue to why the capacitance changes.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to jw0752

    You are correct.  Sometimes I miss little details and sometimes I have to cut them for time. Last week I was working on a capacitor video script and spent an entire day rewriting sections to try to make sure they were concise, but clear and accurate as opposed to slipping into the, "well technically that's correct".
    Max and I create the graphics together, though he does all the animations right now. Sometimes we just run out of time to make everything exactly perfect, so we have to settle for close enough. Thanks for mentioning it in the comments, though! Always great to get more information and clarifications.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago

    Hi Karen,

    In your explanation of the zener diode you had a circuit with a Vin, a resistor., a 3.3 zener to ground and a Vout =Vz. Your explanation seemed to indicate that there would be no voltage at the output until the voltage at the input equaled or exceeded the zener voltage. Actually the Vout would follow the Vin up until the zener voltage is reached and then it would be clamped at that voltage by the current through the zener,  up to the breakdown current of the zener. What you actually said in the presentation was not wrong but it assumes that there is no load on Vout and your animation did not show Vout = Vin for voltages < Vz. Your presentations are fun to watch and very informative. Keep up the great work. I am enjoying learning things I didn't know from the great details that you are including.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to Gough Lui

    Thanks for the extra info! There's always so much more than what I can cover in a 10 minute video. It's great to have others contribute so that everyone has more opportunities to learn.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 8 years ago

    Nice summary. In case anyone's interested, there are even more types of diodes out there, but normally used in more specialist settings. One example is the PIN diode, which is useful in RF switching / attenuating : https://en.m.wikipedia.org/wiki/PIN_diode

     

    Diodes can also come in different semiconductor materials depending on application - for LEDs, this controls the band gap, forward voltage and wavelength. But even for rectification diodes, there are silicon and germanium (lower voltage drop, often used for signals).

    • Cancel
    • Vote Up +6 Vote Down