The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents How 555 Timers Work -- The Learning Circuit 62
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 11 Nov 2019 9:37 PM Date Created
  • Last Updated Last Updated: 6 Oct 2021 7:24 AM
  • Views 9070 views
  • Likes 7 likes
  • Comments 12 comments
Related
Recommended

How 555 Timers Work -- The Learning Circuit 62

image
The Learning Circuit: 62: How 555 Timers Work

The Learning Circuit | element14 presents |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The 555 timer is probably the most common and popular IC to be used in hobby circuits. There are A LOT of projects out there using the 555 in various ways and it’s easy to find schematics to make a project that has already been proven. But rather than just taking plug and playing circuits with the 555 timer, Karen wants to give you the chance to understand the why of what’s happening when you use the 555 timer. In this episode, Karen breaks down what is happening inside the 555 that makes it function. Learn how the inputs interact with the supply voltage to trigger and reset the output high and low. Find out which pins can be used to adjust the threshold at which that change happens. And see which familiar components can be found within the 555.

 

Covering what happens in the 555 timer, Karen walks through connecting the IC to voltage and ground, following the path through the voltage divider to the 2 comparators, which in turn set and reset the flip-flop, that controls the 555’s output signal. She also reviews the basic function of the control voltage, reset, and discharge pins.

 

 

image

  • threshold
  • capacitor
  • reset
  • e14presents_karencorbeill
  • voltage divider
  • trigger
  • oscillator
  • vcc
  • 555 timer
  • comparator
  • inverter
  • discharge
  • flip-flop
  • supply voltage
  • set
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +3
    Thanks Karen, A very nice look inside the functioning of the 555. John
  • neilk
    neilk over 6 years ago +3
    Thank you Karen for a very nicely presented description of the inner workings. I've used a few 555s, copying and modifying other folks' circuits, but never bothered to look inside the "black box"! Nei…
  • beacon_dave
    beacon_dave over 6 years ago +3
    For those wanting to get deeper inside the 555 timer, then there is always this discrete 555 timer kit: https://shop.evilmadscientist.com/productsmenu/652
Parents
  • beacon_dave
    beacon_dave over 6 years ago

    The Learning Circuit continues to go from strength to strength.  image

     

    Regarding the section on the reset pin 4 (at 6:20 into the video) though, am I missing something or is the on/off operation of the PNP transistor illustrated here as being the wrong way around ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 6 years ago in reply to beacon_dave

    Do you mean the emitter and collector are flipped?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to makerkaren

    Hi makerkaren - I was referring to the bit where you say "...if pin 4 is ever grounded, going low, the transistor is turned off..." and vice versa.

     

    However with a PNP type transistor if the base is made more negative than the emitter, it turns on. In the diagram the emitter is tied to +Vcc so pulling pin 4 to ground would presumably turn it on ?

     

    Pin 4 needs to be pulled high for the 555 to function (reset is active low), however by doing this it presumably turns the transistor off ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 6 years ago in reply to beacon_dave

    It's very possible I got them flipped. I didn't compare my diagram with the in depth schematic that shows all the transistors. I was focused more on the transistor's role in the 555 than ensuring I had the pins laid out correctly. Pobody's nerfect? image

    If my diagram is wrong, I would be happy to be corrected. It's all part of the learning process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 6 years ago in reply to beacon_dave

    It's very possible I got them flipped. I didn't compare my diagram with the in depth schematic that shows all the transistors. I was focused more on the transistor's role in the 555 than ensuring I had the pins laid out correctly. Pobody's nerfect? image

    If my diagram is wrong, I would be happy to be corrected. It's all part of the learning process.