The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents How to Make Chase Lights with a Decade Counter -- The Learning Circuit 74
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 23 Jun 2020 5:30 PM Date Created
  • Last Updated Last Updated: 25 Mar 2020 8:24 AM
  • Views 5578 views
  • Likes 4 likes
  • Comments 10 comments
Related
Recommended

How to Make Chase Lights with a Decade Counter -- The Learning Circuit 74

image
How to Make Chase Lights with a Decade Counter

The Learning Circuit | element14 presents |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Karen is making a robot with lots of flashing lights. But the Arduino she’s using to control the circuit has limited I/O. After learning about 555 timers and decade counters, Karen discovered that she can combine them to animate the lights in her robot reducing the outputs needed on the Arduino from ten, down to one. Decade Counters use a clock signal to cascade a high output signal across 10 outputs. Karen shows how to make an astable oscillator circuit with a 555 timer to create the clock signal needed for the decade counter. Then shows how to set up a circuit with 10 LEDs, one for each output. She also shows how to use transistors and relays for applications that require a higher current draw.

 

 

Bill of Material:

 

 

Product NameManufacturerQuantityBuy KitBuy Kit
74HC4017E -Decade Counter / Divider, 2 V to 6 V, DIP-16TEXAS INSTRUMENTS1Buy NowBuy Now
CD4026BE -Decade Counter / Divider, 16 MHz, 3 V to 18 V, DIP-16TEXAS INSTRUMENTS1Buy NowBuy Now
CD74HC4017E -Decade Counter / Divider, HC Family, 60 MHz, 2 V to 6 V, DIP-16TEXAS INSTRUMENTS1Buy NowBuy Now
CD4022BE -Decade Counter / Divider, 11 MHz, 3 V to 18 V, DIP-16TEXAS INSTRUMENTS1Buy NowBuy Now
CD74HCT390ECD74HCT390E - Decade Ripple Counter, HCT Family, 27 MHz, 4 Circuits, 4.5 V to 5.5 V, DIP-16TEXAS INSTRUMENTS1Buy NowBuy Now

  • clock signal
  • e14presents_makerkaren
  • clock pulse
  • oscillator
  • the learning circuit
  • 555 timer
  • astable
  • decade counter
  • timer circuit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • duckiethedragon
    duckiethedragon over 6 years ago +1
    Hi! Could you instead connect the LED anodes to the output pins of the 4017 and connect all the cathodes to ground through a single resistor? It seems to have the same effect and takes up less space, but…
  • makerkaren
    makerkaren over 6 years ago +1
    Here's the breadboard layout with 10 LEDs for anyone that would like it. (The resistor values may not be accurate.)
  • makerkaren
    makerkaren over 6 years ago in reply to periodic +1
    That's awesome! Thanks for taking the time to figure that out and for sharing it.
Parents
  • duckiethedragon
    duckiethedragon over 6 years ago

    Hi! Could  you instead connect the LED anodes to the output pins of the 4017 and connect all the cathodes to ground through a single resistor? It seems to have the same effect  and takes up less space, but are there drawbacks to doing it this way? This is for the single LED per pin.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • duckiethedragon
    duckiethedragon over 6 years ago

    Hi! Could  you instead connect the LED anodes to the output pins of the 4017 and connect all the cathodes to ground through a single resistor? It seems to have the same effect  and takes up less space, but are there drawbacks to doing it this way? This is for the single LED per pin.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • makerkaren
    makerkaren over 6 years ago in reply to duckiethedragon

    Since, in theory, only one output pin would send a high voltage at any time, I believe you could use only one resistor.