The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents How to Make a 4-bit Shift Register Circuit -- The Learning Circuit 76
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 28 Jul 2020 5:41 PM Date Created
  • Last Updated Last Updated: 6 May 2020 7:24 AM
  • Views 6841 views
  • Likes 6 likes
  • Comments 4 comments
Related
Recommended

How to Make a 4-bit Shift Register Circuit -- The Learning Circuit 76

element14 presents
How to Make a 4-bit Shift Register Circuit

The Learning Circuit | element14 presents |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

After learning about shift registers, Karen shows how to use one in a circuit. Shift registers can take data from a single input and transfer it to multiple outputs or take data from multiple inputs and transfer it to a single output. In this video, Karen shows how to use a 4-bit, bidirectional shift register in a circuit. This shift register has 4 parallel inputs and outputs where data can be transferred. It also has two serial inputs, that can be used to shift data left or right across the 4 outputs. After seeing how the circuit is made, can you think of a way to use this universal shift register in a project? Post your ideas in the comments below or find Karen and tell her about it on the element14 Community!

 

 

Bill of Materials

 

Product NameManufacturerQuantityBuy KitBuy Kit
Breadboard, MCM 60 rows, ABS, 8.5mm, 165mm x 56mmMulticomp1Buy NowBuy Now
Small Breadboard w/ Power Rails, 30 rows, ABS, 8.3mm, 54.5mm x 83.5mmMulticomp1Buy NowBuy Now
Electrolytic Capacitor, Miniature, 10 µF, 25 V, 515D Series, ± 20%, Radial Leaded, 5 mmVishay1Buy NowBuy Now
Ceramic Disc Capacitor, 0.01 µF, 100 V, ± 20%, 5 mmVishay1Buy NowBuy Now
LM555CN - Timer, Oscillator & Pulse Generator IC, TTL Compatible, Astable, Monostable, 4.5 V to 16 V, DIP-8On Semiconductor1Buy NowBuy Now
Through Hole Resistor, 220 ohm, 400 mW, ± 1%Vishay4Buy NowBuy Now
Through Hole Resistor, 10 kohm, 250 mW, ± 1%TE Connectivity12Buy NowBuy Now
Through Hole Resistor, 1 kohm, 500 mW, ± 1%TT ELECTRONICS / WELWYN1Buy NowBuy Now
3306P-1-1043306P-1-104 - Trimpot, Single Turn, Cermet, Top Adjust, 100 kohm, Through Hole, 1 TurnsBourns1Buy NowBuy Now
Tactile Switch, 12mm, Red, 12 VDC, 50mAMulticomp2Buy NowBuy Now
Tactile Switch, 12mm, Blue, Top Actuated, Through Hole, Round Button, 24 VDC, 50mAOmron2Buy NowBuy Now
Red LED, Through Hole, 5mm, 20 mA, 2.1 VLED TECHNOLOGY4Buy NowBuy Now
Slide Switch, SPDT, On-On, 2.54mm, Through HoleAPEM4Buy NowBuy Now
140 Pc. Jumper Wire Kit, 22 AWG, Solid, Assorted Lengths and ColorsTwin Industries1Buy NowBuy Now
  • series
  • shift
  • e14presents_karencorbeill
  • bi-directional
  • storage
  • serial
  • 4-bit
  • parallel
  • left shift
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Very good explanation. Uses for the 194 chip were many. I have seen them used to take parallel data and then use the serial output to send the data over long distances and then use them to read out the…
  • jw0752
    jw0752 over 6 years ago +1
    Hi Karen, This looks like a fun circuit to play with. Thanks for the nice demonstration. John
  • lawangen007
    lawangen007 over 5 years ago

    how to made a 16 bit PIPO shift register

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago

    Hi Karen,

     

    This looks like a fun circuit to play with. Thanks for the nice demonstration.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 6 years ago in reply to DAB

    Oh, that's a really cool application. Thanks for sharing!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    Very good explanation.

     

    Uses for the 194 chip were many.

    I have seen them used to take parallel data and then use the serial output to send the data over long distances and then use them to read out the parallel data at a remote site. We did this when internet and ethernet were still in development.

     

    One very important use for this chip is to introduce a chirp signal for things like range finders. You enter the chirp code you want and then transmit the chirp out using the serial sequence for timing. The receiver picks up the returning signal and cycles the bits through until you match the chirp, signifying an accurate signal return. Quick, simple and easy to use, especially in noisy environments.

     

    DAB