The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents DIY Motion Activated Snow Globe -- The Learning Circuit 82
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 18 Nov 2020 9:43 PM Date Created
  • Last Updated Last Updated: 26 Aug 2020 7:24 AM
  • Views 2595 views
  • Likes 5 likes
  • Comments 3 comments
Related
Recommended

DIY Motion Activated Snow Globe -- The Learning Circuit 82

element14 presents
DIY Motion Activated Snow Globe

The Learning Circuit | element14 presents |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

As the usual follow up to the previous PIR lesson video, Karen shows how to use a PIR sensor in a project. This circuit uses a one-shot 555 timer to control a relay to turn on lights and fans to make a motion-activated snow globe. When motion is detected, the fans will blow snow around the light up tree inside the globe and then automatically shut off.

 

Bill of Materials

 

Product NameManufacturerQuantityBuy KitBuy Kit
LM555CN - 555 Timer, Oscillator & Pulse Generator IC, TTL Compatible, Astable, Monostable, 4.5 V to 16 V, DIP-8ON SEMICONDUCTOR1Buy NowBuy Now
Through Hole Resistor, 10 kohm, 250 mW, ± 1%TE Connectivity2Buy NowBuy Now
Ceramic Disc Capacitor, 0.01 µF, 100 V, ± 20%, 5 mmVishay1Buy NowBuy Now
Electrolytic Capacitor, 100 µF, 25 V, M Series, ± 20%, Radial Leaded, 6.3 mmVishay/Panasonic1Buy NowBuy Now
Trimpot, Single Turn, Cermet, Top Adjust, 100 kohm, Through Hole, 1 Turns, 3306P-1-1043306P-1-104Bourns1Buy NowBuy Now
2N4401, BJT, NPN, 40 V, 250 MHz, 625 mW, 600 mA, 300 hFEMULTICOMP PRO1Buy NowBuy Now
Tactile Switch, 6mm, Black, Tall, Top Actuated, Through Hole, Round Button, 12 VDC, 50mAE-switch1Buy NowBuy Now
G5V-1-DC5G5V-1-DC5 Signal Relay, 5 VDC, SPDT, 1 A, G5V-1 Series, Through Hole, Non LatchingOMRON1Buy NowBuy Now
287-18001 PIR Sensor, 7 m, 5 V, 20 V, 120 °, 300 sMCM1Buy NowBuy Now
RADIAL FAN, 60MM, 5VDC, 78L/MIN, 28DBA, HY_60Q05APSEPA2Buy NowBuy Now
Addressable RGB LEDs, Clear, 5mm, 5pkMCM1Buy NowBuy Now
Through Hole Resistor, 220 ohm, 400 mW, ± 1%Vishay1Buy NowBuy Now
DC Power Connector, Jack, 5 A, 2.1 mm, Through Hole Mount, Through Hole, FC68148CLIFF ELECTRONIC COMPONENTS1Buy NowBuy Now
Wire-To-Board Terminal Block, 5.08 mm, 2 Positions, 24 AWG, 14 AWG, 1.5 mm², ScrewWEIDMULLER4Buy NowBuy Now
Prototype Board, Phenolic, 30 x 25 grid, 1.6 mm, 94 mm, 71 mmMulticomp1Buy NowBuy Now
AC/DC Power Supply, ITE, 1 Output, 10 W, 5 V, 2 A, 28-19317PRO ELEC1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 4 Contacts, Male Header, 1 RowsMulticomp1Buy NowBuy Now

 

Additional Parts:

 

Product Name

4.5VDC LED product (White RGB LED tree from Dollar Tree)

Clear tube or globe with large opening

small styrofoam "snow" balls

Wire mesh (mine was made from a kitchen pan splatter screen)

 



  • monostable
  • one-shot timer
  • snow globe
  • 555 timer
  • motion sensor
  • motion activated
  • christmas
  • pir sensor
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • makerkaren
    makerkaren over 5 years ago in reply to hifromkatie

    You'll probably need a bigger fan. I used a splatter screen for my mesh to keep the snow out of the fan, but you could probably just use mesh for a screen door if you need something bigger. I can't think of any other large, clear, cylindrical objects so yeah, a water bottle would probably be your best bet unless you make one from scratch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 5 years ago

    I love this so much.

    Really want to super size it for our living room window, trying to find a 3 gallon water dispenser bottle to build it in but no one on freecycle seems to have one to give!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Nice seasonal project.

     

    DAB