• Products and Partners
    Products and Partners
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
element14 presents
  • Challenges & Projects
  • More
element14 presents
Documents Build Inside The Box - Brainstorming Call!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 28 Apr 2021 2:07 PM Date Created
  • Last Updated Last Updated: 11 Jun 2021 4:30 PM
  • Views 3400 views
  • Likes 8 likes
  • Comments 14 comments
Related
Recommended

Build Inside The Box - Brainstorming Call!

element14 presents
Build Inside The Box

About the Challenge | Contestants | The Prizes | element14 Vault Giveaway | The Box | Terms & Conditions

 

Click on the banner below to register for the upcoming live stream to see which of your favorite vcp project has won:

image

 

Our Build Inside The Box challenge was designed to celebrate our 500th episode of element14 presents.  We chose three of our video hosts to go head to head in the competition to build the best the project that must use ALL of the products in The Box.

 

The challengers (James, Katie and Clem) met virtually to discuss the parts and their initial ideas on building a working project that uses ALL of the parts in The Box.

Unsupported video URL format.

 

If you're looking for the product links, you need to see What's in The Box !

 

  • Which part is the one that the project will be built around?
  • Which part is the hardest to integrate into a working project?
  • How does that temperature sensor actually work?
  • What coding language best fits the desired functionality?

 

These and other exciting questions are discussed in this video.

 

Join the conversation by posting your ideas and commenting below!

 

You still have time to participate in the Build Inside The Box Challenge - your project blogs for the member contest are due Tuesday, 7th May 2021 5pm CDT.

  • build inside the box
  • bitb
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 5 years ago +3
    it is so hard to get all the components into a single project. I just hope to make a project practical enough to justify not using all the parts to the full extent. I'm so courious about what all the people…
  • kellyhensen
    kellyhensen over 5 years ago +3
    Sharing some links to brainstorming other members are doing as they "Build Inside the Box" What's in the box! Don't look in the box! easyejl Build Inside the Box - James O'G - Build log -Update Sunday…
  • aspork42
    aspork42 over 5 years ago +2
    Awesome video - I have had the same 'roller coaster' experience with all the components. Some I've got 100% locked in, and others it took a lot of pondering to decide and figure out. James - you noted…
Parents
  • kmikemoo
    kmikemoo over 5 years ago

    When James said two OLEDs, I just assumed that he meant 2 TOF sensors - especially given the 180 degree viewing angle that he was talking about.  I'm only planning on using one TOF to start.  I'm trying to keep the project creep in check.

     

    My box didn't contain a SD card, but that's fine.  It would have been used as a data logger.  The second iteration would have been to store audio clips and play "HEY!  HEY!  Pay attention to me!" or something similar as an alarm.  I'll save that for another day.

     

    I was tempted to use the original box as the project box but decided that others would be doing that so I moved on.  Clem just verified my assumption.  image

     

    I am SHOCKED at how much I've forgotten about Arduino programming.  I'll blame COVID brain, but WOW!  I'm also surprised by how finicky the MKRZERO is.  Depending on the sketch I load in, it just won't upload without a RESET double tap.

    I also regret not bench testing better.  Now that my stuff is installed and I'm live testing it, I'm getting a different response.  It still works, but I've got to adjust the response values in code rather than what the bench tests showed.

     

    All in, this has been amazing.  There's so much that I want to redo already...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kmikemoo
    kmikemoo over 5 years ago

    When James said two OLEDs, I just assumed that he meant 2 TOF sensors - especially given the 180 degree viewing angle that he was talking about.  I'm only planning on using one TOF to start.  I'm trying to keep the project creep in check.

     

    My box didn't contain a SD card, but that's fine.  It would have been used as a data logger.  The second iteration would have been to store audio clips and play "HEY!  HEY!  Pay attention to me!" or something similar as an alarm.  I'll save that for another day.

     

    I was tempted to use the original box as the project box but decided that others would be doing that so I moved on.  Clem just verified my assumption.  image

     

    I am SHOCKED at how much I've forgotten about Arduino programming.  I'll blame COVID brain, but WOW!  I'm also surprised by how finicky the MKRZERO is.  Depending on the sketch I load in, it just won't upload without a RESET double tap.

    I also regret not bench testing better.  Now that my stuff is installed and I'm live testing it, I'm getting a different response.  It still works, but I've got to adjust the response values in code rather than what the bench tests showed.

     

    All in, this has been amazing.  There's so much that I want to redo already...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • cstanton
    cstanton over 5 years ago in reply to kmikemoo

    > Depending on the sketch I load in, it just won't upload without a RESET double tap.

     

    I remember the Arduino Leonardo being this awkward in Windows initially as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to kmikemoo

    kmikemoo  wrote:

    I'm also surprised by how finicky the MKRZERO is.  Depending on the sketch I load in, it just won't upload without a RESET double tap.

    Based on the hundreds of times I've had to reset, I am starting to get used to it.

     

    Here's what I've come to realize about the SAMD21 / MKRZERO

     

    1. There is some background interrupt that services CDC communication. If that can't run, the COM port drops and you can't reprogram without going into bootloader mode.

    2. If the CDC communication isn't serviced and the serial monitor is open in the IDE, it can cause the entire IDE to lock up. (However, double-tapping into bootloader mode "fixes" that.)

    3. Any time your code misbehaves, it is possible for you to lose communication. In one program, a while(1) caused mine to require the double-tap.

    4. If programming appears to stall, a double-tap into bootloader mode will sometimes finish the process.

     

    Once I started to notice the patterns, it was less finicky (and less frustrating) to work with. My only concern at this point is that once I button up my enclosure, no more double taps for me...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 5 years ago in reply to baldengineer

    I suspect this is a windows communication issue (dropping com ports is typical for it)
    Under Linux I never had that experience, I can even keep the Serial port open while programming without any issues.