Table of contents
Abstract
A cursed stone gargoyle for the front door that asks trick-or-treaters a riddle, listens to the answer and pays a right one (or a loud scream) with a wrapped sweet. Four Edge Impulse models run fully offline on one Arduino UNO Q.
Project
The finished statue: a riddle answered out loud, and a sweet down the tongue.
![]()
In one line: a cursed stone gargoyle for the front door that asks trick-or-treaters a riddle out loud, listens to their answer, and pays a right answer (or a loud enough scream) with one wrapped sweet down its tongue. Everything runs offline on one Arduino UNO Q: four Edge Impulse models, a voice rendered on the board, and a microcontroller that drives the lights, the candy servo and the mist with a watchdog that fails safe.
Code, CAD and schematic (MIT): https://github.com/Abhinavkrishna3211/Feed-the-Gargoyle
The Imp on the Doorstep
Nobody remembers who carved the imp.
The story goes like this. Long ago, a small stone-born trickster spent one Halloween too many robbing sweets off other people's doorsteps. The carver who caught it did not smash it. He bound it into a block of stone with one curse: guard a bowl of sweets for as long as the stone stands, and never take one.
The curse says the imp may never hand out sweets for free. It never said anything about handing them out for a good answer. So the imp found its loophole: you pay the toll with your wits.
"I follow you everywhere, copy every move, and never once say thank you."
"Light me and I work hard. The harder I work, the shorter I get."
(Answers at the end.)
Why it is a Halloween project
Riddling gatekeepers go back to the Sphinx. Real gargoyles are rain spouts, and the word comes from the old French gargouille, the throat. And long before trick-or-treat, people went guising: you sang or performed at the door, and you got fed. The gargoyle puts those together. A greedy little guardian, a riddle at the door, and a fair trade for a treat.
Every Halloween our sweet bowl is either empty in ten minutes or ignored. I wanted something at the door that makes people stop, think, laugh and earn their sweet, without a phone in sight.
What It Does
the idea, explained as a stick figure animation.
- You walk up. After about a second it notices you, and its eyes open.
- It greets you. If it is sure about your costume, it teases the costume (never the person in it).
- It picks its toll at random: a riddle to answer out loud, or a scream loud enough to light every plate on its spine.
- The eight glowing plates on its spine count down while it waits, or fill up as you scream.
- Right answer or big enough scream: green eyes, a puff of mist and one wrapped sweet down the tongue. Wrong answer: a cackle, a hint and one more go.
- It says goodbye and goes back to sleep.

See it play. The right answer is at the top. Here are the other ways a visit can go, all on the finished statue:
A wrong answer gets a cackle and a hint.
The riddle timer runs out while the spine counts down.
A scream loud enough to light every plate on the spine wins the sweet.
A scream that is too quiet does not fill the spine. No sweet this time.
Before the stone body existed, the same UNO Q ran the whole game in a cardboard prototype:
What is new here
- A four-model cascade on one board, fully offline. A small visitor gate runs all the time. The costume, props and keyword models only wake when there is someone to look at or listen to. Only one heavy model runs at a time.
- An LLM where it actually fits. Gemma 3 1B runs on the UNO Q, but with the camera and audio models running it writes about 2.2 to 2.6 tokens per second (4 GB UNO Q, 3 threads, 30 minute soak). A child will not wait 20 seconds for a reply. So the language model drafted lines while the board was idle, and Piper turned the checked lines into speech on the board ahead of time. During play it only picks a line.
- A scream judged by loudness, not by a classifier. A calibrated loudness meter on the spine was fairer and easier to understand for a seven-year-old: fill the spine, win the sweet.
- Two brains with a safety net. The Linux side sends a heartbeat every half second. If the microcontroller hears nothing for one second, it parks the servo, stops the mist and dims the lights by itself.
- Every number measured on the board. Every figure says which board, which settings and how it was measured. The raw logs are in the repo.
Results at a glance
| What | Result | How it was measured |
|---|---|---|
| Notices a visitor | about 1 s | visitor score above 0.5 on every frame for 1 s, camera at 10 fps, 4 GB UNO Q |
| False wake-ups | 60 down to 4 in 206 s, no visitor missed | door video replayed at 10 fps on my PC, with and without the 1 s rule |
| Hears the riddle answer | 29.6 ms per window, 90.5 % on 569 clips | median on the 4 GB UNO Q; test clips from speakers not in training |
| Confirms the sweet fell | 1.2 to 1.5 s after the command | IR sensor, real sketch, bench rig, 4 GB UNO Q |
| Fails safe | within about 1 s | board USB-C pulled with the app running, 4 GB UNO Q |
| Voice clarity | 8 % average word error, median 0 | every bank line transcribed with Whisper on my PC |
| Board headroom | 2.5 GB of 3.7 GB free, no restart in 30 min | all models loaded, camera at 10 fps, 4 GB UNO Q |
The build at a glance
| Part | Steps | Time | You end up with |
|---|---|---|---|
| Brain and software | 1 to 4 | about 3 hours | a UNO Q that speaks and runs all four models |
| Body | 5 to 9 | 4 to 5 days, mostly printing and drying | a printed, glued, stone-coated statue with a tested dispenser |
| Electronics | 10 to 12 | about 5 hours | lights, servo, sensor, mist, camera and mics wired and calibrated |
| Life | 13 to 14 | an evening | a gargoyle at the door, tested |
No 3D modelling is needed: every part is ready to print. You need basic soldering, and you should be comfortable copying commands into a terminal. Step 2 is optional.
How It Works

One board, two brains. The Arduino UNO Q has a Linux computer (Qualcomm QRB2210) and a microcontroller (STM32U585) on the same board.
- Linux side: camera, microphones, the four models, the game and the voice.
- Microcontroller: the eye rings, the 24 spine LEDs, the candy servo, the IR drop sensor and the mist maker.
They talk over Arduino's Bridge. Linux sends "show the listening colours", "spine to 60 percent", "drop one sweet". The microcontroller answers "a sweet fell" or "nothing fell, it is jammed".

The models (all trained in Edge Impulse, all float32 on the board):
| Model | Job | Result |
|---|---|---|
| Visitor gate | Is someone in front of me? | 91.8 % on 475 test images (Edge Impulse, float32) |
| Keyword spotter | Which of the six riddle answers was said? | 90.5 % on 569 test clips, same answers on the UNO Q, 29.6 ms per window (median, 4 GB UNO Q) |
| Costume | Which costume is that? | 91.0 % on 155 test images (Edge Impulse, float32) |
| Props | No clear costume? Hat, glasses, crown, eye mask or scarf? | mAP@50 0.82 on 1,153 test crops; 825 ms per check on the board (median of 10, app running) |
Bill of Materials

The brain
- Arduino UNO Q, 4 GB version. The 2 GB board cannot hold all the models at once.
- USB-C hub with power-delivery (PD) pass-through. The UNO Q has one USB-C port, so power, camera, mic and sound card share the hub.
- USB-C PD charger, 45 W. A weak phone charger made my board restart in a loop.
Senses and voice
- Arducam B0490 USB camera (IMX462, M12 3.9 mm lens). It becomes the third eye.
- USB sound card with a headphone output, a Boya BY-M1 lavalier mic (it hears both the riddle answers and the scream) and two small speakers.
Lights, candy and mist
- 2 x WS2812 round boards with 7 LEDs each, for the eyes.
- 24 x single WS2812 LED boards for the spine (8 plates of 3).
- 74AHCT125 level shifter, a 1000 uF capacitor (6.3 V or more), two 330 to 470 ohm resistors.
- SG90 micro servo, 180 degree (buy a spare).
- LM393 IR reflective sensor module (often sold as FC-51).
- 5 V ultrasonic mist maker board with a 20 mm disc, a cotton wick, a small cup and a drip tray.
- IRLZ44N MOSFET, a 100 ohm and a 10 k resistor.
Power
- 5 V 4 A supply for the LEDs, servo and mist, separate from the board's charger.
- Inline fuse holder with a 2.5 A fast-blow fuse, and a small kill switch.
- USB-C panel-mount extension, about 30 cm. Red, black and blue hookup wire, perfboard, heat-shrink.
Body
- Grey PLA+ (about 2 spools), clear PLA+ (1 spool) for the eyes and spine plates.
- 4 x M3 heat-set inserts and 4 x M3 x 16 screws, 3 x M3 x 10 screws, 8 x 6 x 2 mm disc magnets, 1.75 mm filament offcuts for pins.
- CA glue, five-minute epoxy, masking tape, putty, grey epoxy primer, fine cement, waterproof PVA glue, matte clear sealer, acrylic paints (black, two greys, green, brown).
- A small cauldron-style bowl and individually wrapped soft toffees, all one type.
Tools: 3D printer with a 256 x 256 mm bed (I used a Bambu Lab P2S with an AMS), soldering iron with an insert tip, multimeter, calipers, wire strippers, flush cutters, a long 2.5 mm ball-end hex key, hot glue gun, gloves, dust mask and safety glasses.
Software (all free): Arduino App Lab and an Edge Impulse account.
Step 1: Set Up the UNO Q
Time: 30 minutes. You need: UNO Q, hub, 45 W charger, a USB-C cable, a computer.
Make sure the board works before any wiring. It is much easier to fix things now than inside a statue.

- Download Arduino App Lab (Arduino's program for writing and running apps on the UNO Q) from https://www.arduino.cc/en/software/ and install it. On Windows, pick the MSI installer. (Version 0.10.0 was current when I built this.)

- Plug the 45 W charger into the hub's PD input, and the hub's USB-C lead into the UNO Q.
- Plug the hub into your computer and open App Lab.
- You should see: your UNO Q found as a new board. If App Lab offers an update, accept it and do not unplug the board until it finishes.

- Open the Examples tab, pick Blink LED and press Run.
- You should see: the example running on the board within about a minute.

- Connect the board to your Wi-Fi when App Lab asks, and note its IP address. Every command below uses it as
<board-ip>. - On your computer, get the project files:
git clone https://github.com/Abhinavkrishna3211/Feed-the-Gargoyle.git
cd Feed-the-Gargoyle
- Copy the app to the board:
scp -r app arduino@<board-ip>:/home/arduino/ArduinoApps/gargoyle
Not working?
| Problem | Fix |
|---|---|
| Board keeps restarting | The charger is too weak. Use the 45 W PD charger through the hub's PD port. |
| App Lab does not find the board | Try another USB-C cable. Some cables only charge and carry no data. |
| Update fails halfway | Leave it plugged in and run the update again. |
Step 2: Find the Language Model's Limit (Optional)
Time: 1 hour. You need: the board on your network, about 700 MB free disk.
The gargoyle does not need this at the door. Do it to see what a language model can and cannot do on a board this size, and why the voice is pre-rendered.
- Open a terminal on the board:
ssh arduino@<board-ip> - Install Gemma 3 1B with App Lab's own tool. It took about 2 minutes on my board and used 705 MB of disk.
arduino-app-cli model install llamacpp:gemma-3-1b-it-Q4_0
- On your computer, copy the test scripts to the board:
scp scripts/llm_bench.py scripts/line_bank.py scripts/gemma_jobs.py arduino@<board-ip>:~/
- On the board, run the speed test at 3 threads. It starts llama.cpp with
-t 3 -c 2048 --cache-reuse 256and asks for a short gargoyle line five times.
python3 llm_bench.py 3 bench-t3.jsonl --runs 5
- You should see: about 4.4 tokens per second. Mine gave 4.36 (median of 4 runs, 4 GB UNO Q, nothing else running).
- Try prompt caching. This puts a fixed 168-token block of rules in front of the prompt and lets the server keep it.
python3 llm_bench.py 3 cache.jsonl --cache --prefix 8 --runs 6
- You should see: the first request is slow, then every later one reads the prompt in under a second.

- Let it draft lines. The script checks each one: 14 words or fewer, ends with
.,!or?, nothing about face, body, age or size, no riddle answers.
python3 line_bank.py drafts.jsonl --per 5
- You should see: roughly one draft in three or four passes. Read the passing ones too: some are good, many only look right.

What I found. With the camera and audio models running, Gemma dropped to 2.58 tokens per second at 3 threads and 2.38 at 4, so a fourth thread bought nothing and 3 leaves a core free. A reply under that load took about 13 s. Most failed drafts broke character. So the final 164 lines are hand-written, with Gemma's drafts as a starting point, and every line passed the same checker.
Not working?
| Problem | Fix |
|---|---|
model install fails |
Check the board has internet and at least 1 GB free (df -h). |
| Server never answers | An old container holds the port. Run docker ps, then docker rm -f gbench. |
| Much slower than 4 tokens per second | Something else is running. Stop the app with arduino-app-cli app stop. |
Aside: my favourite rejected line was "Stuck! Wait, a chilling request." I still do not know what it means, and neither does the gargoyle.
Step 3: Give It a Voice
Time: 1 hour, or a weekend if you write your own lines. You need: the board, the repo, Python on your computer.
The gargoyle speaks from a bank of short lines, one list per situation: greetings, costume teases, riddles, hints, wins, too quiet, wrong answer, goodbye and a polite apology if the dispenser jams. A few of mine: - "Who comes knocking at a hungry stone's door? Speak, sweet seeker." - "Louder! A mouse sat in your voice and kept it tiny."
- Install Piper on the board and download the en_GB-alan-medium voice, following the Piper README (link in References).
- Write your lines as a JSON file: each key is a situation, each value a list of lines. Keep every line to 14 words or fewer and never mention a face, body, age or size.
- On your computer, set
GARGOYLE_SSHto the helper that reaches your board (see the top ofscripts/gargoyle_speak.py), then render:
python scripts/render_bank.py line-bank.json bank/
It speaks each line one sentence at a time, slightly slow (--length_scale 1.1), then adds the stone effect from scripts/gargoyle_fx.py: pitch down and a touch of echo. If it stops, run it again; it skips files it already made.
- You should see: a list of file names scroll past, about 8 seconds per line on my board.

- Copy the rendered lines into the app on the board:
scp bank/*.wav arduino@<board-ip>:/home/arduino/ArduinoApps/gargoyle/python/bank/
- You should see: files named like
greet_0.wavandwin_3.wavin the bank folder.

I checked every line by transcribing it with Whisper and comparing it with the written text: average word error 8 percent, median 0. Any garbled line was reworded and rendered again.
Not working?
| Problem | Fix |
|---|---|
| Voice sounds rushed | Check --length_scale 1.1 in scripts/gargoyle_speak.py. |
| A word comes out garbled | Reword the line. Piper struggles with rare names and stacked consonants. |
| Script cannot reach the board | Check GARGOYLE_SSH and that ssh arduino@<board-ip> works on its own. |
Step 4: Get the Four Models
Time: 30 minutes on the easy route. You need: a free Edge Impulse account, the board on your network.
Edge Impulse Studio is a free website where you upload examples, train a model and download it for your board. My four projects there are public. Cloning copies the data, the settings and the trained model into your own account.
| Model | Public project | File name on the board |
|---|---|---|
| Visitor gate | https://studio.edgeimpulse.com/public/1153004/live | visitor.eim |
| Keywords | https://studio.edgeimpulse.com/public/1153006/live | keywords.eim |
| Costume | https://studio.edgeimpulse.com/public/1153007/live | costume.eim |
| Props | https://studio.edgeimpulse.com/public/1160020/live | props.eim |
For each project:
- Open the link and click Clone this project at the top right. Give it a name and wait a few minutes.
- In your copy, open Deployment in the left menu.
- Click the Deployment target box (it says C++ library at first), search for Linux (AARCH64) and select it.
- Under Model optimizations, select Unoptimized (float32). The page picks int8 by default.
- Click Build. A
.eimfile downloads: the trained model packed as one file the UNO Q can run. Rename it to the name in the table.

Why float32. On my board the int8 build of the keyword model crashed, and the int8 props model scored 0.00 in Studio and was slower (Studio estimate 917 ms against 508 ms per frame). float32 is the safe choice on this board.
Install them on the board:
- Copy the visitor and keyword models to the folder the App Lab bricks read from (bricks are App Lab's ready-made blocks, here the camera and microphone classifiers):
scp visitor.eim keywords.eim arduino@<board-ip>:/home/arduino/.arduino-bricks/ei-models/
- Copy the costume and props models next to the app:
scp costume.eim props.eim arduino@<board-ip>:/home/arduino/ArduinoApps/gargoyle/python/models/
- Make them runnable:
ssh arduino@<board-ip> "chmod +x /home/arduino/.arduino-bricks/ei-models/*.eim /home/arduino/ArduinoApps/gargoyle/python/models/*.eim"
- You should see: four
.eimfiles, andyunet.onnxnext tocostume.eimandprops.eim. The props model uses YuNet to find the face it crops around.

Full route: train them yourself
Each public project holds the full recipe. Here are the settings that mattered, with the screen to check against.
Visitor gate. 160 x 160 images, Squash, an Image block (RGB) and Transfer Learning with MobileNetV2 160x160 0.5, 16 neurons, dropout 0.1, 12 cycles, learning rate 0.0005, data augmentation on. Use a separate test set, not the automatic split. The game also asks for a visitor score above 0.6 on 10 checks in a row, about 1.2 s on the board. On door video replayed at 10 fps on my PC, an earlier 1 s version of this rule cut false wake-ups from 60 to 4 in 206 s and missed no visitor.

Cleaning the labels mattered more than any setting: my audit found 15 percent of the test visitor labels wrong, and adding the pictures the model got wrong took it from 90.3 to 91.8 percent.
Keyword spotter. One-second clips at 16 kHz in eight labels: the six answers (shadow, pumpkin, mirror, candle, spider, scarecrow), unknown and noise. Test clips come from different speakers than the training clips. Window 1000 ms, increase 500 ms, MFCC with 13 coefficients, frame length 0.02, stride 0.01, 32 filters, FFT 256, low frequency 300.

The classifier is a small 1D conv network in expert mode that hides short slices of time and pitch while training and weights rare words more. The game fires only when 3 of 4 windows in a row agree: on long test recordings played every 100 ms on my PC, that caught 90.7 percent of answers with about 44 false alarms per hour, against 160 per hour for single windows.

Costume. 12 classes (11 costumes plus empty), adults only, every photo checked by eye. The standard blocks topped out around 75 percent. EfficientNetV2B0 at 224 x 224 in expert mode, with 5 percent validation, took the same photos to 91.0 percent (141 of 155). A costume line plays only at a score of 0.6 or more.

Props. An object detector on a head crop: YuNet finds the face and the app cuts a square 3.2 face heights wide, face centre 42 percent down. YOLO-Pro small, 224 x 224, 100 cycles, learning rate 0.001, GPU. 6,648 crops split by photographer. YOLO-Pro needs a GPU training job; if yours is refused, clone my project.


Not working?
| Problem | Fix |
|---|---|
| Board crashes when a model loads | You built int8. Rebuild with Unoptimized (float32) for Linux (AARCH64). |
| Every props score is 0.00 in Studio | Model version is set to Quantized (int8). Switch to float32. |
| Visitor gate wakes for posters or TVs | Add posters, screens and statues to empty and retrain. |
| Props found in Studio but not at the door | Check yunet.onnx sits next to props.eim. The crop must match training. |
Step 5: Look Inside the 3D Model
Time: 20 minutes. You need: a computer.
You need no 3D modelling skills. Every part is in the repo under hardware/print/, ready to print, with PRINT_PLAN.md and ASSEMBLY.md next to them. This step shows what is inside, so the next steps make sense.

- Size. The statue is 1.18 times the original sculpt, the smallest size that fits the dispenser under the spine.
- Eyes. Only the visible front of each eye is clear: a thin dome with a dark slit printed through it. The lids around it are thick grey, so only the iris glows.
- Third eye. The camera hides in the middle of the forehead spiral. Its 13.9 mm lens slides into a 14.2 mm hole and holds the camera by itself.

- Spine. Each plate is a thin clear shell with a peg underneath that presses into a socket in the back, with a hole through for the LEDs.
- Candy path. The dispenser sits in the head under the spine, so no plate is covered. The chute runs down the throat and out over the tongue. The mouth is fixed open: no moving jaw near small hands.
- Refill lid. A lid in the top of the head lifts off. Its edge follows a carved crack, and magnets hold it shut.
- Plinth. Holds the electronics, two speakers behind small worn-looking holes, a service door and a USB-C socket.


Step 6: Test Print the Eye and a Spine Plate
Time: about 3 hours of printing, 1 hour of testing. You need: grey and clear PLA+, one eye board, 3 single LED boards, a breadboard, the 74AHCT125, the resistor and capacitor, the UNO Q.
The eyes print into the head, one of the longest prints in this build. If an eye glows wrong, you lose the whole print. So test the risky parts small first.
- Print one eye test piece with exactly the settings you will use for the head: 0.2 mm layers, the same grey and clear spools, clear only on the visible front of the eye. Clear filaments glow very differently, so test the spool you will really use.
- You should see: a smooth clear dome, a crisp dark slit, and no grey streaks in the clear part.

- Print one spine plate in clear and its patch of back in any spare colour.
- Press the plate into the socket.
- You should see: the plate sits down on its ledge all the way round, no gap and no rocking. It needs a firm push, not a hammer.


Build a test light on the breadboard. This is the same circuit as the final build, so it is good practice.
- Push the 74AHCT125 across the middle gap of the breadboard. Pin 1 is next to the small dot or notch.
- Wire the chip:
- pin 14 to 5V on the UNO Q, pin 7 to GND;
- pin 1 to GND (this switches channel 1 on);
- pins 4, 10 and 13 to 5V (this switches the unused channels off);
- pin 2 to D5 on the UNO Q;
- pin 3 through the 330 to 470 ohm resistor to the eye board's DIN.
- Wire the eye board's 5V and GND. Put the 1000 uF capacitor across 5V and GND next to it, striped leg to GND.
- Wire 3 single LED boards after the eye: eye DOUT to the first board's DIN, then DOUT to DIN along the three. Thread them up through the socket hole so they sit under the plate.
- In App Lab, make a new app, paste this into its sketch and press Run:
#include <Adafruit_NeoPixel.h>
// Test light: D5 > 74AHCT125 > 330 ohm > eye DIN, eye DOUT > 3 spine LEDs (one plate).
Adafruit_NeoPixel px(10, 5, NEO_GRB + NEO_KHZ800);
// {eye, spine} colours for idle, listen, win, fail, the same as the game sketch
const uint8_t COL[4][2][3] = {
{{255, 140, 0}, {120, 0, 255}},
{{160, 255, 210}, {255, 110, 0}},
{{0, 255, 0}, {0, 255, 0}},
{{255, 0, 0}, {255, 0, 0}},
};
void setup() { px.begin(); }
void loop() {
for (int m = 0; m < 4; m++) {
for (int pct = 10; pct <= 60; pct += 10) { // six brightness steps, 3 s each
for (int i = 0; i < 10; i++) {
const uint8_t *c = COL[m][i < 7 ? 0 : 1];
px.setPixelColor(i, c[0] * pct / 100, c[1] * pct / 100, c[2] * pct / 100);
}
px.show();
delay(3000);
}
}
px.clear();
px.show();
delay(2000);
}
- You should see: amber, mint, green, then red in the eye, each getting brighter in six steps. The plate glows purple, orange, green, then red.
Safety: this test runs from the UNO Q's own 5V pin, which is fine for one eye and one plate at these levels. Never run the full chain, the servo or the mist from it.
- Push the eye board into the pocket behind the eye. Switch off the room lights and look from 1 m away, straight on, from the side and from a child's height.
- You should see: only the iris glows, the slit stays dark, and you cannot count the seven LED dots. At the second step (20 percent, the cap in the game) it glows clearly in a dim doorway without glaring.
The eye test piece lit.
The spine test plate lit in its socket.
- Leave both on the brightest step for 10 minutes, then touch them.
- You should see: barely warm.
Not working?
| Problem | Fix |
|---|---|
| Light leaks through the lids | The grey around the eye must be at least 2 mm thick. Paint the inside of the pocket black. |
| You can count seven dots | Move the board 5 to 10 mm further back from the dome. |
| Nothing lights | Check the DIN arrow, chip pin 1 to GND, and D5 to pin 2. |
| Grey streaks in the clear | Raise the purge (flush) volume for the colour change in your slicer. |
| Plate too tight | Sand the peg lightly with 240 grit. |
Step 7: Build and Test the Candy Dispenser
Time: about 5 hours of printing, 1 hour of testing. You need: PLA+, an SG90 servo, the IR module, calipers, 10 toffees.
One servo turns a one-pocket rotor under a tube of sweets. Each turn lets exactly one sweet fall down the chute, past an IR sensor that confirms the drop.
- Measure one sweet with calipers. Mine (a wrapped eclair toffee) is 31 mm long, 13.2 mm thick and 53 mm long over the wrapper twists.
- If your sweet is a different size, open
hardware/cad/dispenser/dispenser.py, changeSW_L,SW_WandSW_Hnear the top, and rebuild the parts with free Blender:
blender -b --factory-startup -P dispenser.py -- stl --test
- Print the fit coupons in
hardware/cad/dispenser/stl/test/fit/first. Each prints in minutes and tests one fit:fit_tubeintofit_socket: slides in with a light push, no wobble (FIT, 0.2 mm per side);fit_collarontofit_boss: pushes on and stays on (COLLAR_FIT, 0.1 mm per side);fit_servo: the SG90 drops in gear end first;fit_rotoronto the servo horn: presses on with no play (HORN_FIT).
- If a coupon is wrong, change its setting by 0.05 mm, rebuild and print that coupon again.
- Print the test rig from
hardware/cad/dispenser/stl/test/: housing, rotor, servo plate, shelf, tube and long chute. The shelf tilts it 20 degrees, as in the statue.

- Push the servo into the servo plate and fix it with the screws that came with it. Push the rotor onto the horn, but do not fit the horn screw yet (Step 11 sets the angle).
- Drop one sweet into the tube and turn the rotor slowly by hand, from the load side, over the top, to the chute side and back. Repeat with 10 sweets, then with a full tube.
- You should see: exactly one sweet per turn, sliding out of the chute by itself.
- Print the statue dispenser from plate
04_plate_13_dispenser_grey.3mfinhardware/print/. It is the same mechanism with a short chute; the throat and tongue carry the sweet the rest of the way. - Paint the inside wall of the chute opposite the side window matte black, so the IR sensor sees only the sweet. Fit the IR module at the window.


The final dispenser dropping sweets on command from the UNO Q.
What the first rig taught me. The sweet hung in the pocket and the outlet. Every part on the sweet path got 3 mm more room (RELAX in the script), and the chute went from 35 to 45 degrees: at 35 the sweet rolled slowly, at 45 it slides. My first design used a stepper and a pocket wheel; one servo does the same job with fewer parts.
Safety: once the servo is powered, keep fingers out of the rotor. It is small, but it pinches.
Not working?
| Problem | Fix |
|---|---|
| Two sweets come out at once | Your sweet is shorter than mine. Set its size in dispenser.py and rebuild. |
| Sweet turns sideways and sticks | Too much width. Lower CLR a little. |
| Sweet stops in the chute | Sand the chute floor smooth and check the shelf sits flat. |
| Rotor catches the next sweet | Raise RAMP, the chamfer on the back edge of the pocket. |
Step 8: Print and Assemble the Statue
Time: 4 to 5 days of printing, 2 hours of work plus glue curing. You need: grey and clear PLA+, filament offcuts, CA glue, five-minute epoxy, masking tape, soldering iron with an insert tip, 4 heat-set inserts.

- Open the plates in
hardware/print/in Bambu Studio (or your slicer) in the order ofPRINT_PLAN.md: head, face, dispenser and spine first, then body, wings and plinth. - Print plate 01, the head, as one two-colour print: grey for the head, clear only for the eye fronts, exactly as in your eye test.

- Print plate 05, the eight spine plates, in clear.

- Print the remaining plates in grey. Any colour works for body and plinth parts because the primer and cement cover it, but keep everything around the eyes and LED pockets opaque.
- Cut 1.75 mm filament into 12 mm pins. Push one into each hole on one side of every cut face.
- Dry fit the whole statue with no glue, following
hardware/print/ASSEMBLY.md.- You should see: every joint sits flat, no rocking, no gap. If a pin is tight, twist a 2 mm drill bit in the hole by hand.
- Glue the joints in the same order: CA glue for short joints, epoxy for long ones. Mix epoxy for one joint at a time, tape each joint closed and let it cure.

- Do not glue the refill lid, the spine plates or the statue to the plinth. They come apart for service.
- Turn the statue over and press the four heat-set inserts into the base with the iron at about 220 C, straight down, until flush.
Safety: the iron and insert are hot enough to burn badly. Work on a heat-proof mat.
Not working?
| Problem | Fix |
|---|---|
| Piece lifts at the corners | Wash the plate with soap and water and add a brim. |
| Joint has a gap | Fill it with putty in Step 9. Gaps under 1 mm vanish under the cement. |
| Insert went in crooked | Press it straight with the iron while still warm. |
Step 9: Turn Plastic into Stone
Time: 2 hours of work over 2 to 3 days of drying. You need: putty, sandpaper (120 and 240), masking tape, foam plugs, grey epoxy primer, fine cement, waterproof PVA glue, a flat brush, a sponge, matte clear sealer, acrylic paints, gloves, dust mask and safety glasses.
Paint alone always looks like plastic. A thin coat of real cement gives the grain, weight and cold feel of stone.
- Fill every seam with putty, let it dry, and sand with 120 then 240 grit.
- Take the lid off. Mask the clear eye fronts, every spine socket and ledge, the mouth, throat and tongue, and plug the camera, ear and speaker holes and the insert holes.
- Brush on a thin coat of grey epoxy primer. Let it dry, then add a second coat.
- You should see: one even grey, no filament colour showing.

Safety: primer fumes are strong. Work outdoors or with good airflow, and wear a mask. Wet cement is caustic and the dry powder is harmful to breathe: wear gloves, glasses and a dust mask, and wash any splash off with plenty of water.
- Mix fine cement with waterproof PVA and a little water to thick-paint consistency, about 2 parts cement to 1 part PVA. Mix only what you can use in 20 minutes.
- Brush on a thin coat, about 1 mm, one section at a time, and dab it with the brush or sponge for a rough grain. Keep it extra thin in carved details.
- Let it cure for 24 hours out of direct sun. Lightly sand the sharpest high points so nothing snags a hand.
- Peel the tape and pull the plugs.
- You should see: a spine plate still seats, the lid still drops in, and the camera and ear holes are clear.
- Spray two light coats of matte clear sealer.
- Weather it: a runny black wash wiped off the high points, a dry-brushed light grey on raised details, green and brown dabbed into the low spots. Keep every mark uneven, never the same on both sides. Seal again.
- You should see: from 1 m away, no seams and no plastic shine.
Not working?
| Problem | Fix |
|---|---|
| Cement cracks or flakes | Too thick or too little PVA. Sand off the loose bits, recoat thinner with more PVA. |
| Details blurred | Pick the cement out with a toothpick while soft. Thin the mix next time. |
| Lid no longer fits | Sand the cement off the lid edge and the head edge. |
Aside: the first time I touched the cured statue in the dark, I took my hand away rather quickly.
Step 10: Wire Power, Servo, Sensor, Lights and Mist
Time: about 3 hours. You need: the 5 V 4 A supply, kill switch, fuse holder and 2.5 A fuse, perfboard, red, black and blue wire, multimeter, the 74AHCT125 and parts from Step 6, the 24 LED boards, the eye boards, the servo, IR module, mist board and MOSFET parts.
Keep the schematic and pin map open while you wire. The full KiCad schematic is in hardware/kicad/ in the repo.

10a. The power rail
The gargoyle has two supplies that share only a ground wire. The board runs from the 45 W charger through the hub. The LEDs, servo and mist run from a separate 5 V rail. Servos and LEDs pull sudden bursts of current; on the board's supply those bursts made my board restart.

Safety: keep both supplies unplugged while you wire. Plug in only when a step says so.
- Wire the kill switch into the 5 V supply's positive lead, then the fuse holder after it. Fit the 2.5 A fuse.
- On perfboard, make two bus strips, +5 V and GND. Solder the fused positive to +5 V and the supply's negative to GND.
- Add one black wire from the GND bus to a GND pin on the UNO Q. Without the shared ground, the signals will not work.
- Set the multimeter to continuity and touch +5 V and GND.
- You should see: no beep.
- Plug in the supply, switch on, and measure +5 V to GND.
- You should see: 4.9 to 5.1 V. Switch off and unplug.
10b. Servo and drop sensor

| UNO Q pin | Goes to |
|---|---|
| D2 | IR module OUT |
| D4 | Mist MOSFET gate (through 100 ohm) |
| D5 | Eye LED data, through the 74AHCT125 (channel 1) and a 330 to 470 ohm resistor |
| D6 | Spine LED data, through the 74AHCT125 (channel 2) and a second 330 to 470 ohm resistor |
| D9 | Servo signal |
| GND | GND bus of the 5 V rail |
- Servo: brown to GND bus, red to +5 V bus, orange to D9.
- IR module: VCC to +5 V bus, GND to GND bus, OUT to D2.
- Power the rail and hold a sweet in front of the IR module.
- You should see: the module's small LED on with the sweet there, off when it is gone. If not, turn its trimmer screw slowly until it reacts only to the sweet.
10c. Eyes and spine
The 38 LEDs run as two chains: the eyes on D5 (left eye 7, then right eye 7) and the spine on D6 (8 plates of 3, tail plate first). Data goes in at DIN and out at DOUT, board to board.

- ort the 24 boards into eight groups of three, one per plate.
- Within each group, solder short loops: 5 V to 5 V, GND to GND, DOUT to the next DIN. Use red for 5 V, black for GND and blue for data so you can check it at a glance.
- Join the groups with longer wires, last DOUT of one group to first DIN of the next, with enough slack to reach the next plate opening.

- Lay the chain inside the back shell with group 1 at the tail and group 8 at the head. Cover each group with a small paper square and fix it with hot glue, so it can come out again.


- Seat each eye board in its pocket behind the eye with a dab of hot glue. Chain them: left eye DOUT to right eye DIN.

- Move the 74AHCT125 circuit from Step 6 onto perfboard, powered from the +5 V and GND bus (not the UNO Q's 5V pin). Channel 1 (pin 3) goes through a resistor to the left eye's DIN, as before.
- Switch on channel 2 for the spine: move chip pin 4 from 5V to GND, wire pin 5 to D6 on the UNO Q, and pin 6 through the second resistor to the tail group's first DIN. Leave right eye DOUT unconnected.
- Solder the 1000 uF capacitor across +5 V and GND where power enters the chains, striped leg to GND. Feed 5 V and GND from the bus to both ends of the chain.
- Open
app/sketch/sketch.inoand setPLATE_PX = 3, for three LEDs under each plate.
Why the brightness is capped and the redraw is slow. The sketch caps the eyes at about 20 percent and the spine at about 70 percent: it looks better on stone, draws less current and keeps the plastic cool. With the spine at full brightness, the USB camera dropped off the bus on my 4 GB UNO Q during a full run, so leave the cap in place. On an earlier UNO Q build, redrawing an LED ring every 40 ms made every Bridge message time out; redrawing only on a change brought them back to 6 to 8 ms. Here the sketch only sends pixels when one changes, at most every 200 ms, and every colour change is slew-limited: no sudden flashes.
10d. Mouth mist
- Hold the IRLZ44N with the writing facing you. The legs, left to right, are Gate, Drain, Source.
- Solder the 100 ohm resistor from D4 to the Gate, and the 10 k from the Gate to GND. The 10 k keeps the mist off while the board starts.
- Connect Source to GND. Connect the mist board's + to the +5 V bus and its - to the Drain.
- Put the disc on a wet wick in the water cup (damp, not under water), and the cup in the drip tray under the mouth, away from the boards, the mic and the sweets.
Safety: never let the disc run dry and never let water reach the electronics. Empty the cup after every night.
The sketch protects the mist: one puff lasts 3 s at most, then it rests 6 s, it never runs while the gargoyle is listening, and the safety net turns it off. On the bench (4 GB UNO Q, real sketch) a second request 3 s after a puff was refused and a 3.5 s request was cut to 3 s.
Not working?
| Problem | Fix |
|---|---|
| Board restarts when the servo moves | The servo is on the board's power. Move it to the 5 V rail and check the shared GND. |
| IR LED always on | It sees the chute wall. Paint the wall matte black and turn the trimmer down. |
| LEDs show random colours | Check the DIN arrows, the level shifter and the shared GND. |
| Only some spine plates light | Check PLATE_PX = 3 and the DOUT to DIN joints between groups. |
| Eyes light but the spine stays dark | Check chip pin 4 is on GND, pin 5 goes to D6 and pin 6 to the tail group's DIN. |
| Mist never starts | Check the MOSFET legs (G, D, S) and that the disc is damp. |
Step 11: Load the Sketch, Set the Rotor, Test the Safety Net
Time: 1 hour. You need: everything wired, the dispenser on its rig shelf, 10 toffees.
The sketch is the Arduino program that runs on the microcontroller. Every value marked CAL at the top of app/sketch/sketch.ino is one you may tune for your build.
- Copy the edited sketch to the board:
scp app/sketch/sketch.ino arduino@<board-ip>:/home/arduino/ArduinoApps/gargoyle/sketch/
- Start the app. In App Lab, open it and press Run, or from the board:
arduino-app-cli app start /home/arduino/ArduinoApps/gargoyle
- The first start compiles the sketch and loads it onto the microcontroller. It takes a few minutes.
- You should see: slowly breathing amber eyes and a soft glow on the spine. With no models found, the app runs a practice mode with a pretend visitor, so you can check lights and voice first.
Both eyes wired in the head, breathing slowly through ember, amber, gold and red.
The finished spine lighting plate by plate based on scream intensity.
The finished spine, as a timer for the riddle.
The finished spine,as a timer for riddle(If you fail to answer in time or if your answer is wrong ).
- Set the rotor. With the app running, the servo holds the load angle (170 degrees). Pull the rotor off the horn, push it back on with the pocket facing straight up the tube, and now fit the horn screw.
- Run the drop test. Stop the app and create the test switch:
touch /home/arduino/ArduinoApps/gargoyle/python/dispense.on
- Load 10 toffees and start the app again. It drops one sweet every 4 seconds, up to 50, and stops if it jams.
- You should see: each sweet out of the chute and
drop_confirmedcounting in the log. On my bench the drop was confirmed 1.2 to 1.5 s after each command.
- You should see: each sweet out of the chute and
- Delete the switch when you are done:
rm /home/arduino/ArduinoApps/gargoyle/python/dispense.on - Test the safety net. With the app running, pull out the board's USB-C.
- You should see: within about a second, the rotor returns to load, the mist stays off and the lights go to idle.
Not working?
| Problem | Fix |
|---|---|
| Rotor turns the wrong way | Swap the PADDLE_LOAD and PADDLE_DUMP values. |
| Sweet gets flung out | Raise SWEEP_MS (3 ms per degree by default) so the rotor moves slower. |
Sweet drops but no drop_confirmed |
Adjust the IR trimmer and check OUT goes to D2. |
| Two misses, then everything stops | That is the jam protection. Clear the jam and restart the app. |
Step 12: Fit the Dispenser, Camera, Mic and Speakers
Time: 2 hours. You need: the tested dispenser, 3 x M3 x 10 screws, 8 magnets, camera, mic, sound card, speakers, rubber grommet, cable ties.
Dispenser and lid
- Route the servo and IR cables down through the neck first.
- Lower the dispenser onto the locating pin and three posts inside the head, and screw it down with the three M3 screws.
- You should see: it sits level with the chute lined up with the throat.
- Stack all eight magnets and mark the top face of the stack. Glue four into the lid with the marked face up and four into the head tabs with the marked face down.
- You should see: the lid snaps into place and lifts off with a fingertip. The head holds 5 sweets: one in the pocket, four in the tube.
Camera, the third eye
- From inside the head, push the lens into the forehead hole until the case rests on the ledge.
- You should see: from the front, only a dark dot in the middle of the spiral.

Microphone and speakers
- Fit the lavalier mic in the ear cavity with its foam windscreen, held by a rubber grommet, not glue, so servo buzz does not travel into it. Plug it into the USB sound card, and the sound card into the hub.
- Glue each speaker on its tray in the plinth, facing the small worn holes. Connect them to the sound card output, left channel on the visitor's left.
Fix the mic levels once, then never touch them
The ear mic hears riddle answers. The camera's built-in mic measures the scream: side by side, it gave the steadier level (26.5 to 32.4 dB above its silence floor, four screams at 1 m, 4 GB UNO Q).
- On the board, run
alsamixer. Press F6, pick the USB sound card and set its mic capture to the maximum (28 on mine). - Press F6 again, pick the camera, and set Mic capture to the maximum (256).
- Press Esc and save the levels so they survive a reboot:
sudo alsactl store
Calibrate the scream meter
The spine reads the camera mic every 0.2 s and maps the level to 0 to 100 between FLOOR_DB (empty spine) and TOP_DB (full spine) in app/python/sensors.py. A scream wins when it reaches the top plate on 2 readings in a row.

- On the board, make a tiny level script:
cat > level.py << 'EOF'
import sys, wave, array, math, statistics
a = array.array("h", wave.open(sys.argv[1]).readframes(10**9))
n = 3200 # 0.2 s at 16 kHz
db = [20 * math.log10(max(1, math.sqrt(sum(x * x for x in a[i:i + n]) / n)) / 32768)
for i in range(0, len(a) - n, n)]
print("quietest %.1f median %.1f loudest %.1f dBFS" % (min(db), statistics.median(db), max(db)))
EOF
- With the gargoyle where it will stand and nobody talking, record 5 s of the room:
arecord -D plughw:CARD=Camera,DEV=0 -f S16_LE -r 16000 -c 1 -d 5 quiet.wav && python3 level.py quiet.wav
- Stand 1 m in front and scream as loud as you comfortably can for the whole 5 s:
arecord -D plughw:CARD=Camera,DEV=0 -f S16_LE -r 16000 -c 1 -d 5 scream.wav && python3 level.py scream.wav
- You should see: the scream's loudest reading well above the room's median.
- In
app/python/sensors.py, setFLOOR_DBto the room's median plus 2 dB andTOP_DBto the scream's loudest reading. - Delete the recordings:
rm quiet.wav scream.wav
Not working?
| Problem | Fix |
|---|---|
| Wrong mic records | Card numbers swap between boots, so the app opens them by name: CARD=Camera for the scream, CARD=Device for the ear mic. arecord -l lists the names. |
| Talking fills the spine | Raise FLOOR_DB a few dB. |
| No scream ever wins | Lower TOP_DB a few dB. |
| No sound from the speakers | Run aplay -l and check the sound card is listed. |
Step 13: Bring It to Life
Time: 30 minutes. You need: the board with the models (Step 4) and the voice (Step 3).
- Switch the app from practice mode to the real models:
touch /home/arduino/ArduinoApps/gargoyle/python/sensors.on
- Start the app:
arduino-app-cli app start /home/arduino/ArduinoApps/gargoyle
- You should see: in the log, the camera starting, the keyword runner found, the visitor model loaded, then the game going idle.

- Stand in front of the camera, one to two metres away.
- You should see: after about a second, mint eyes, a greeting and a challenge.
- Do what it asks: answer the riddle clearly, or scream.
- You should see: on a win, green eyes, a puff of mist and a sweet down the tongue.
- Walk away.
- You should see: a goodbye, a 10 second rest, then sleepy amber eyes.
What it costs the board (4 GB UNO Q, all models loaded, camera at 10 fps, nobody in front, measured once about a minute after start): the camera model uses about one of the four cores, the app about half a core, the audio models a quarter of a core, and 2.5 GB of 3.7 GB memory is still free. In a 30 minute run with the camera, audio and language models all busy, the board never restarted.
For the curious: the game is a plain state machine in app/python/game.py with no hardware calls. Run python app/python/game.py on your computer and its self-checks run.
Not working?
| Problem | Fix |
|---|---|
| "Failed to enumerate audio devices" | The mic must be named directly, as hw:CARD=Device,DEV=0. Check names with arecord -l and see app/python/main.py. |
| No greeting, eyes stay amber | Check the camera is in the hub and visitor.eim is installed and runnable. |
| Greets but never hears you | Check the mic level (Step 12) and that keywords.eim is installed. |
| Still in practice mode | Check sensors.on is in app/python/ on the board. |
Step 14: Close It Up and Test Before the Night
Time: 1 hour, then an evening of testing. You need: 4 x M3 x 16 screws, the long hex key, cable ties, friends in costumes.
- Mount the USB-C panel extension in the back of the plinth and plug its inside end into the hub.
- Tie every cable away from the servo and the mist cup.
- Lift the statue onto the plinth, line up its four inserts with the holes, and drive the M3 x 16 screws up from inside with the long hex key. One speaker covers a screw path: lift it out first.
- You should see: the statue does not move when you push the top of its head gently.
- Run this checklist before the big night:
- 50 visits in a row with no restart, counting wins, losses, wrong costume lines and missed visitors;
- an empty doorway for an hour, counting false wake-ups;
- music and chatter nearby, counting false riddle answers;
- pull the plug in the middle of a drop: the rotor must park;
- play with an empty tube: it must apologise for a jam, not grind away;
- two hours non-stop: the board must not be too hot to touch.
In a short live test with only a fan running, I got two false "pumpkin" detections in 191 s, both on loud bangs, none from the fan.
On the night: put the gargoyle where the forehead looks at adult chest height, the cauldron under the tip of the tongue, up to 5 toffees in the lid, the mist cup filled. Switch on the 5 V rail first, then plug in the board.
Safety: wrapped sweets only. Keep the back door and cables out of reach of small children. Keep it out of direct sun: PLA+ softens at around 55 to 60 C. Empty the mist cup at the end of the night.
Privacy and Safety
- Camera frames and sound stay in memory only long enough to be checked. Nothing is stored or sent anywhere, and it needs no network at the door.
- It never comments on a face or body. Costume lines play only when the model is confident.
- No moving jaw near small hands: the mouth is fixed open and the tongue is the slide.
- Wrapped sweets only.
- If Linux crashes, the microcontroller parks the servo, stops the mist and dims the lights within one second.
- No flashing lights: every LED change is slew-limited.
What Went Wrong
- Stepper and pocket wheel: worked, but needed a driver and step counting. One servo does the same job.
- A moving jaw: a pinch point near a child's hand. Removed.
- A weak charger: boot loops once the camera was plugged in. Fixed with a PD supply and a separate 5 V rail.
- LEDs redrawn every loop: jammed the Bridge. Redraw on change only.
- Mic at full gain on the wrong mic: clipped screams. Fix the gain first, then collect data.
- int8 models: crashed or scored zero on this board. float32 works.
- The language model could not hold the character. So it drafts, rules filter, and the board speaks only checked lines.
- More photos of the same costumes stopped helping at about 75 percent. A bigger network in expert mode took the same photos to 91.
Where it stands. The statue is printed, stone-coated, wired and playing every outcome on the finished body: right answer, wrong answer, timer out, a winning scream and a scream too quiet (the clips at the top).
Files and Credits
- Code, CAD, print plates, schematic and every measurement: https://github.com/Abhinavkrishna3211/Feed-the-Gargoyle
- Public Edge Impulse projects: visitor gate https://studio.edgeimpulse.com/public/1153004/live, keywords https://studio.edgeimpulse.com/public/1153006/live, costume https://studio.edgeimpulse.com/public/1153007/live, props https://studio.edgeimpulse.com/public/1160020/live
- Edge Impulse Studio, Arduino App Lab and the UNO Q bricks. Gemma 3 1B by Google with llama.cpp. Piper TTS with the en_GB-alan-medium voice. YuNet from OpenCV Zoo. Public datasets listed in the repo.
If you build one, post a photo in the comments. I want to hear what yours says to people.
Riddle answers: a shadow, and a candle.
References
- Edge Impulse, "Arduino UNO Q" board docs. https://docs.edgeimpulse.com/hardware/boards/arduino-uno-q
- Edge Impulse, "Run models in Arduino App Lab". https://docs.edgeimpulse.com/hardware/deployments/run-arduino-app-lab
- M. Pous, OCR cascade on the UNO Q (detector then recogniser). https://github.com/mpous/ocr-linux-arduino-uno-q
- S. Githu, vision model and small language model cascade on the UNO Q. https://docs.edgeimpulse.com/projects/expert-network/behavioural-coach-vision-model-cascade-slm-arduino-unoq
- Clawrophyll, continuous keyword spotting on the UNO Q. https://docs.edgeimpulse.com/projects/expert-network/clawrophyll-on-device-wake-word-detection-using-keyword-spotting-arduino-unoq
- Edge Impulse Linux Python SDK. https://github.com/edgeimpulse/linux-sdk-python
- Arduino App Lab bricks (microphone, audio classifier, language model), read at source level. https://github.com/arduino/app-bricks-py
- Gemma 3 1B open weights by Google, run with llama.cpp. https://github.com/ggml-org/llama.cpp
- Piper text to speech. https://github.com/rhasspy/piper
- YuNet face detector, OpenCV Zoo. https://github.com/opencv/opencv_zoo
- COCO 2017 dataset (visitor gate images). https://cocodataset.org
- My earlier UNO Q projects, where the server settings, line checking loop and microphone gain checks came from: https://github.com/Abhinavkrishna3211/Daybreak and https://github.com/Abhinavkrishna3211/jarvis-lab-assistant
- Arduino UNO Q user manual. https://docs.arduino.cc/tutorials/uno-q/user-manual/
Top Comments