• Products and Partners
    Products and Partners
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
555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Blog Class D Amplifier TLC555 Timer Based PWM Audio Amp
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AE7HD
  • Date Created: 18 Oct 2022 3:03 PM Date Created
  • Views 3881 views
  • Likes 8 likes
  • Comments 2 comments
  • timer
  • 555 timer
  • tlc555
  • 555timermadnessch
  • class d amplifier
Related
Recommended

Class D Amplifier TLC555 Timer Based PWM Audio Amp

AE7HD
AE7HD
18 Oct 2022

Recreating a 555 timer based Class D PWM amplifier I first built in the '80s.

Using the TLC555, a CMOS based timer that is faster than the NE555 TTL based timer.

This takes advantage of the comparators in the 555 timer and uses a constant current device called a current mirror to create a linear sawtooth needed to generate a linear PWM.

The parts count over a more conventional Class D amplifier of the time is greatly reduced.

image

IC1 is an astable, constant period clock. The Off time is very short as required by the next stage. The period is about 20uS or about 50kHz so as to be well above the Nyquist limit of 2f of the highest frequency. I will be adding a lowpass filter to the input.

IC2 is wired as a monostable that is triggered by a Low on pin 2. The output at pin 3 goes High until the capacitor, C2, reaches the setpoint voltage on pin 5 of IC2. IC2 acts as both a sawtooth generator and comparator.

A current mirror formed by Q1 and Q2 provide a constant charging current. This causes the charging voltage on C2 to be a linear ramp.

The control voltage, CV, on pin 5 of IC2 is normally biased at 2/3 of Vcc by internal resistors. The Op Amp IC3 biases this at 1/2 of Vcc with no signal present. IC3 is wired as an inverting amplifier with a gain Av of -10 for a 5V system, or -22 for a 12V system.

With CV at 1/2 Vcc, by design the charge time is 1/2 of the clock period. So the PWM output is 50%. When the Op Amp raises CV, the charge time increases as a linear function of the change. So if it raise CV to 3/4 of Vcc, the output PWM is 75%. If CV is lowered to 1/4 of Vcc, the output PWM becomes 25%.

L1 and C4 form a lowpass filter on the output with a corner -3dB point of approximately 20kHz. I have given values for both an 8 ohm and a 4 ohm speaker.

I will be improving on this circuit. I no longer have all of my notebooks from the '70s and '80s, so I must recreate this from memory.

  • Sign in to reply

Top Comments

  • Sudeep AJ
    Sudeep AJ over 3 years ago +1
    Amazing! sounds interesting to build!
  • dougw
    dougw over 3 years ago +1
    Old memories are sometimes the best ones.
Parents
  • dougw
    dougw over 3 years ago

    Old memories are sometimes the best ones.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 3 years ago

    Old memories are sometimes the best ones.