• Products and Partners
    Products and Partners
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
555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Blog Lead battery regenerator using 555
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: JWx
  • Date Created: 18 Oct 2022 12:19 PM Date Created
  • Views 27916 views
  • Likes 11 likes
  • Comments 11 comments
  • 555timermadnessch
Related
Recommended

Lead battery regenerator using 555

JWx
JWx
18 Oct 2022

When trying to revive degraded lead-acid battery (that were left without charging for too long and entered deep undercharge condition) old wisdom (from the times when buying new car battery was near impossible so people have gone great lengths to restore even worst cases) suggests using charge cycles interrupted by discharging. Using that principle chargers of old were using unfiltered rectified current and some load connected parallel to charged battery - in that config every cycle cell was charged (when input voltage exceeded cell voltage) and discharged into load (when rectified voltage  was below cell's voltage).

Modern chargers are working different way - usually as constant current source with voltage limit.

As I have decided to try to revive some old standby battery (left in unpowered equipment for several years) I have learned limits of this method - battery charged somewhat and then stopped. To my surprise, discharging battery using old lamp as load enabled it to consume more energy during next charging cycle - and this experience have led to creation of this circuit. Schematics is very simple and standard:

schematics

Every minute or so (555 frequency of 13mHz with duty cycle of 95%) generator disconnects battery from charger and discharges it for several seconds through small car lamp. D2 prevents reverse current flow when charger is disconnected.

It seems that after every discharging event charging current increases a bit - maybe (let's hope) because internal resistance of battery lowers?

Described experiment goes on for some time without dramatic improvements but it is only an experiment - "what happens to  otherwise dead battery when treated this way?"

Below some photos of this module connected to DYI (LM317 based) battery charger and proof-of-work movie:

imageimageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
Parents
  • robogary
    robogary over 3 years ago

    Nice project idea to help restore the cell plates.

    In the ancient days of unsealed lead acid car batteries, batteries would be visually checked for suffient electrolyte solution in the cells. Often they just needed distilled water added. Hygrometers can also check specific gravity in case the battery needs some acid added. 

    In old batteries the plates may just be worn out from a life of charge/discharge cycles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 3 years ago

    Nice project idea to help restore the cell plates.

    In the ancient days of unsealed lead acid car batteries, batteries would be visually checked for suffient electrolyte solution in the cells. Often they just needed distilled water added. Hygrometers can also check specific gravity in case the battery needs some acid added. 

    In old batteries the plates may just be worn out from a life of charge/discharge cycles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • JWx
    JWx over 3 years ago in reply to robogary

    I really like procedure that goes  something like this:

    - remove electrolyte

    - fill with water

    - charge (or maybe charge/discharge?)

    - replace with fresh water

    - charge

    - replace water with fresh electrolyte

    And how to execute it when battery is sealed, maybe filled with gel or electrolyte stored in glass mat layers... And properly disposing of used electrolyte involves trip through the city to find institution that is recycling that sort of chemicals...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to robogary

    The sealed batteries appear to be little different. Once you pop the cover plate off, instead of the old screw caps you tend to find rubber caps. If the battery has been venting gas you often find that the top of the rubber caps are sucked in due to a vacuum having formed inside the cell. Inside you tend to find a rather dry looking cell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 3 years ago in reply to beacon_dave

    Interesting observation - thanks! I wonder if there is any mean to refill with water when cell dries out without destroying one-way valve... Maybe using syringe with needle would do the trick? But how to monitor electrolyte level during the process... Gotta check when I encounter one in really bad state...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to JWx

    The one-way valve is often just a rubber cap.

    Remove the cap and you can access to the cell just like an older unsealed battery.