555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Blog Ludicrous 555
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 9 Oct 2022 1:09 AM Date Created
  • Views 14449 views
  • Likes 15 likes
  • Comments 18 comments
  • mic1555
  • ittybitty
  • astable mode
  • 555 timer
  • 555timermadnessch
  • 555 Timer Madness
  • frequency
Related
Recommended

Ludicrous 555

wolfgangfriedrich
wolfgangfriedrich
9 Oct 2022

So, the humble 555 timer started its live as a bipolar IC. Technology progressed and CMOS type 555 timer chips are available now.
The fastest one I could find is the Microchip “IttyBitty” MIC1555.

My quest is to find out how fast it can really go.
The MIC1555 can be used in astable oscillator configuration and the datasheet specifies a maximum frequency of 5 MHz with a 1 KOhm resistor and 47 pF capacitor.
image

I built up the circuit on a tiny breadboard to minimize those pesky parasitic capacitances (not that I think it really made a difference).

image

With 1 KOhm and 47 pF I did a voltage sweep in the recommended operation range from 2.7 V to 18 V and beyond the the absolute maximum rating of 22 V. Turns out I already get 8.43 MHz at 6 V as a maximum frequency. Successively reducing the resistor and capacitor values to 0 Ohm and open circuit instead of a capacitor increased the frequency further to 9.75 MHz at about 6V. Interesting side note, that the frequency reaches a minimum at the specified max operation frequency of 18 V and increases again when going higher than that inside the absolute maximum range.

image

I also recorded the current draw and duty cycle for all test setups. No surprises there, the current increases with the voltage and the duty cycle decreases.

image
image

And for everybody's enjoyment, here is a full voltage sweep captured on video.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Now I am trying to push the limits even further. Overclocking often needs better cooling and increasing the operation voltage.
The coldest temperature I can easily get to in my house is the freezer with -16 °C. Sticking the circuit in there and doing the voltage sweep again brought some improvement to 9.98 MHz at 5V and fine-tuned to 5.3 V got me to 10.01 MHz; above the desired 10 MHz margin twice the specified value in the datasheet.

image

I saved the overvoltage experiment for last as it might turn out fatal for the tiny little fellow. In fact I was determined to crank up the voltage until certain death. Sorry 555.

It did not take much. Back on the bench at room temperature the MIC1555 burnt out above 24V, but with encouraging results of 8.24 MHz sharply increased from the value at 23 V. So with a proper heat sink at low temperatures, it might survive longer at even higher voltages. At 24V it was drawing 35 mA and dissipating a whopping 0.84 W. I was recording the high voltage test live on video and I could argue that it did die ozcillating at 10.6 MHz, if the fequency measurement is assumed to still be correct from the the previous frame on the screen.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


image
image

Conclusion:
The 555 works well beyond the specified values and I had fun doing the measurements.

  • Sign in to reply

Top Comments

  • scottiebabe
    scottiebabe over 4 years ago +1
    Not a fair race, but with a 74 Advanced CMOS Schmidt trigger (74AHC1G14) I got 156 MHz using only a 1 kOhm feedback resistor in a relaxation oscillator configuration. No capacitor was added only the…
  • DAB
    DAB over 4 years ago +1
    The old 555 continues to amaze me even after all these years.
  • baldengineer
    baldengineer over 3 years ago in reply to dougw +1
    CMOS versions of the 555 don't always use 5Kohm for their resistor divider. For example, the ICM7555 from Renesas uses ~140k for its resistors.
Parents
  • scottiebabe
    scottiebabe over 4 years ago

    Not a fair race, but with a 74 Advanced CMOS Schmidt trigger (74AHC1G14) I got 156 MHz using only a 1 kOhm feedback resistor in a relaxation oscillator configuration. 

    image

    No capacitor was added only the effective input capacitance of the inverter.

    image

    image

    Regardless, I loved your blog and experiments! You really squeezed every last Hz out of your 555 oscillator.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago in reply to scottiebabe

    This is a wild build, I love it. And the result is rather impressive. This might be a way to measure the input capacitance of the IC. 

    I would like to know what bandwidth your scope probe has (my guess would be ~12pF for a 200 MHz probe) and what the supply voltage is? With the beautiful sine wave, would we see a square wave with a faster scope and yours is just cutting off the higher harmonics? Good results always lead to more questions Wink

    Thanks for sharing!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago in reply to scottiebabe

    This is a wild build, I love it. And the result is rather impressive. This might be a way to measure the input capacitance of the IC. 

    I would like to know what bandwidth your scope probe has (my guess would be ~12pF for a 200 MHz probe) and what the supply voltage is? With the beautiful sine wave, would we see a square wave with a faster scope and yours is just cutting off the higher harmonics? Good results always lead to more questions Wink

    Thanks for sharing!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • scottiebabe
    scottiebabe over 4 years ago in reply to wolfgangfriedrich

    Thank you for the kind words :) I wasn't expecting it to be that fast. With that scope shot I was using the 10 cm ground clip, so that was likely the bandwidth limiter. Being a rigol is hard to say what the actual bandwidth is but somewhere between 100 and 150 MHz.

    With enough measurement bandwidth I would suspect the output may look more like a triangle wave, with the output slewing up and down.

    With a 10x probe on the input (red) and probing the output with a probe with a ground spring:

    image

    I have some Advanced cmos inverters in a DIP package and they are definitely too fast for their own good. You can see up to 1V of ground bounce from the the DIP's lead frame inductance when one inverter switches....