555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Blog Pulse Reverse Electroplating/Electroetching Using 555 Timers
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AE7HD
  • Date Created: 18 Oct 2022 2:58 PM Date Created
  • Views 1767 views
  • Likes 6 likes
  • Comments 2 comments
  • electroplating
  • etching
  • ne555
  • 555 timer
  • tlc555
  • 555timermadnessch
Related
Recommended

Pulse Reverse Electroplating/Electroetching Using 555 Timers

AE7HD
AE7HD
18 Oct 2022

A simple pulse reverse electroplating/electroetching controller using the 555 timer. The Arduino of its day.

Two 555 timers with control over forward pulse, reverse pulse, and zero current rest time by the artful use of steering diodes and potentiometers. Wired in such a way that the H bridge can never turn on two transistors on the same side of the arm.

image

Drawn in KiCAD.

The first 555 timer is run as an astable with a steering diode, so charge and discharge times have minimal interaction. A 1M ohm potentiometer and a 470k resistor set the forward current timing from 33 to 103ms.
Tfwd = 0.7 x 470k x 0.1u = 32.9e-3 minimum Fwd current time 
Tfwd = 0.7 x 1470k x 0.1u = 102.9e-3 maximu Fwd current time 

On the discharge time, a 1k resistor sets minimum reverse current time to about 0.1ms. Section A of a dual 50k potentiometer causes the discharge time to track the reverse timing set on the other 555 timer. A single section 50k potentiometer allows setting an additional discharge time as a rest time with no current.
Toff = 0.7 x 1k x 0.1u = 0.07e-3 minimum time that Fwd current is off
Toff = 0.7 x 51k x 0.1u = 3.57e-3
Toff = 0.7 x 101k x 0.1u = 7.07e-3

The lower 555 timer is run as a monostable. Because charge/discharge of an astable is 0.7RC for each cycle, but for a monostable charge is 1.1RC, the timing capacitor should be 0.64 of the first 555 timing capacitor. 0.062uF is the closest standard value. The second section of the dual 50k potentiometer and a 1k resistor controls reverse current time from about 0.1ms to about 3.5ms.
Trvs = 1.1 x 1k x 0.062u = .0682e-3 
Trvs = 1.1 x 51k x 0.062u = 3.48e-3

With the optoisolators wired as they are, there can never exist a condition where too many power transistors are on.

The resistor and capacitor between pin 3 of U1 and pin 2 of U2 is a differentiator. So when the output of U1 is going from High to Low, a very short low pulse appears on pin 2 of U2, triggering the monostable. The diode is there so that when pin 3 of U1 goes from Off to On, it dumps the capacitor into Vcc rather than putting a 10V pulse into U2.

  • Sign in to reply
  • AE7HD
    AE7HD over 4 years ago in reply to dougw

    Yes, for our makerspace to use for etching and electroplating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago

    Interesting application. Did you have a use for this?