555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Forum Stayin Alive with the 555
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 36 subscribers
  • Views 5318 views
  • Users 0 members are here
Related

Stayin Alive with the 555

scottiebabe
scottiebabe over 4 years ago

Many individuals have created a version of this circuit before. So, I take no credit.

Most USB power banks have an auto shutoff feature that is triggered when the output current drops below a threshold value. I am guessing whatever value that is, will vary greatly from unit to unit so you may need to adjust the load resistors.

image

This circuit kept my dollar store power bank from going into auto shutdown.

The oscillation frequency was approximately 1/7 Hz.

So every 7 seconds a ~100mA load is applied for ~100 ms.

image

The advantage of a pulse load circuit like this is that the average load current can be kept low, instead of say a static 100 mA load on your power bank.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 4 years ago +5
    Its the circuit has kept a small amber LED running at 2 mA for some time now!
  • javagoza
    javagoza over 4 years ago in reply to scottiebabe +4
    Two more days adding hardware and you already have a monster for the Halloween competition
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to javagoza +4
    The LED is pumpkin-coloured
Parents
  • scottiebabe
    0 scottiebabe over 4 years ago

    The control IC in my USB power bank is a TP4333:

    image

    On my powerbank the SWT pin left NC (there is no button or flashlight). 

    Unfortunately there are no detailed specifications on the auto shutdown feature:

      image

    https://www.skytech.ir/DownLoad/File/1167_ETP4333.pdf 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scottiebabe
    0 scottiebabe over 4 years ago

    The control IC in my USB power bank is a TP4333:

    image

    On my powerbank the SWT pin left NC (there is no button or flashlight). 

    Unfortunately there are no detailed specifications on the auto shutdown feature:

      image

    https://www.skytech.ir/DownLoad/File/1167_ETP4333.pdf