555 Timer Madness
  • Challenges & Projects
  • Project14
  • 555 Timer Madness
  • More
  • Cancel
555 Timer Madness
Forum Stayin Alive with the 555
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timer Madness to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 36 subscribers
  • Views 5074 views
  • Users 0 members are here
Related

Stayin Alive with the 555

scottiebabe
scottiebabe over 3 years ago

Many individuals have created a version of this circuit before. So, I take no credit.

Most USB power banks have an auto shutoff feature that is triggered when the output current drops below a threshold value. I am guessing whatever value that is, will vary greatly from unit to unit so you may need to adjust the load resistors.

image

This circuit kept my dollar store power bank from going into auto shutdown.

The oscillation frequency was approximately 1/7 Hz.

So every 7 seconds a ~100mA load is applied for ~100 ms.

image

The advantage of a pulse load circuit like this is that the average load current can be kept low, instead of say a static 100 mA load on your power bank.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +5
    Its the circuit has kept a small amber LED running at 2 mA for some time now!
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe +4
    Two more days adding hardware and you already have a monster for the Halloween competition
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to javagoza +4
    The LED is pumpkin-coloured
Parents
  • scottiebabe
    0 scottiebabe over 3 years ago

    Another power bank I have is based on the IP5305 and the datasheet would suggest my original circuit should work:

    image

    https://aitendo3.sakura.ne.jp/aitendo_data/product_img/ic/charger/IP5305/IP5305-Injoinic.pdf

    However no luck. I needed both a larger amplitude and duration to keep this power bank alive.

    image

    The morale of the story is that, some breadboard experimentation is required to see what your power bank needs to see to stay alive...

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • scottiebabe
    0 scottiebabe over 3 years ago

    Another power bank I have is based on the IP5305 and the datasheet would suggest my original circuit should work:

    image

    https://aitendo3.sakura.ne.jp/aitendo_data/product_img/ic/charger/IP5305/IP5305-Injoinic.pdf

    However no luck. I needed both a larger amplitude and duration to keep this power bank alive.

    image

    The morale of the story is that, some breadboard experimentation is required to see what your power bank needs to see to stay alive...

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rsjawale24
    0 rsjawale24 over 3 years ago in reply to scottiebabe

    umm I guess you need to take care about the loading effect when connection the 555 with the power bank IC. Maybe due to the impedance differences there is a drop in the amplitude. I'm not very sure though.