7-Segment Display
  • Challenges & Projects
  • Project14
  • 7-Segment Display
  • More
  • Cancel
7-Segment Display
Blog Electronic Die
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
  • Author Author: scottiebabe
  • Date Created: 8 May 2022 1:51 AM Date Created
  • Views 12730 views
  • Likes 15 likes
  • Comments 23 comments
  • 7segmentdisplaysch
Related
Recommended

Electronic Die

scottiebabe
scottiebabe
8 May 2022

I can remember building an electronic die soldering kit as a child. I haven't seen that kit in ages, I assume its gone for good. But I can try to build a new one with a RPI Pico...

If you look at the dot pattern on the faces of a six sided die, you will notice there are a few common pairs of dots:

image

Take for example the dots on the 2 side, neither of those dots are every displayed individually, so we can group them together as one segment. Similarly, we can group the other 2 opposing corner dots as a segment. Here is how I wired up 7 LEDs to represent the six faces of the die:

image

I soldered the LEDs to a small piece of perfboard and connected it to a RPI Pico in a solderless breadboard:

image

Here is the micropython code I put together:

from rp2 import PIO, StateMachine, asm_pio
from machine import Pin
import time
import rp2
import random

pb = Pin(22,Pin.IN,Pin.PULL_UP)

@rp2.asm_pio(out_shiftdir=PIO.SHIFT_RIGHT,sideset_init=[],out_init=([PIO.OUT_LOW]*4),fifo_join=PIO.JOIN_TX)
def PIOLED():
    # Actual program body follows
    wrap_target()
    pull(block)                  [0]
    out(pins,4)                  [0] 
    wrap()
        
sm = rp2.StateMachine(0, PIOLED, freq=2000000, out_base=Pin(16))
sm.active(1)

ledLUT = {1:0x01,2:0x04,3:0x05,4:0x0C,5:0x0D,6:0x0E }

while True:
    if pb.value() == 0:
        # display a die rolling
        for i in range(12):
            sm.put(ledLUT[i%6+1])
            time.sleep(0.4)
            
        sm.put(ledLUT[random.randint(1,6)])

I am not sure how easy or difficult this code would be for a beginner. The use of a RP2040 state machine makes writing a bitfield across a few gpio pins easy. 

It definitely took me longer to solder the LEDs, resistors, and wires than to write the code. The pico is pretty neat.

image

In the second third version, I will try using an old pic microcontroller to display the numeric value of a die on a 7-segment display.

7-Segment Display with Pi Pico

Just like in the first example of where I created an electronic die face, with a 7-segment display there exists a mapping between the visible numeric value and active display segments. I resued the existing 7-segment code table on wikipedia, but it is easy enough to work out for yourself. The 7-degment display I used in this example has the segments arranged in a common-anode configuration. So the common pin is tied to VDD. A segment is illumined by sinking current out of the segment pin, this is done by driving a gpio pin low with a series ballast resistor. Here is the schematic I used:

image

The code:

from machine import Pin, mem32
import time
import random

# Configure GP26 as input with internal pull-up
pb = Pin(26,Pin.IN,Pin.PULL_UP)

# Configure GP14 - GP21 as outputs
PinBus = [ Pin(x,Pin.OUT) for x in range(14,22) ]

def BusWrite( pbus, v ):
    for i in range(len(pbus)):
        pbus[i].value( v & (1<<i))
           
# Seven segment LUT table for numerical readout
# bit0 - segA, bit1 - segB,... bit7 - segDP
SGLUT = [ ~x for x in [0x3f,0x06,0x5b,0x4f,0x66,0x6d,0x7d,0x07,0x7f,0x6f,0x77,0x7c,0x39,0x5e,0x79,0x71]]

def displaySevenSeg(v):
    BusWrite(PinBus,SGLUT[v])#14,21,SGLUT[v])

BusWrite(PinBus,0xff)
while True:
    if pb.value() == 0:
        # display a die rolling
        for i in range(30):
            BusWrite(PinBus,~(1 << (i%6)))
            time.sleep(0.035)
        displaySevenSeg(random.randint(1,6))

The electronic die in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Thanks for reading :) 

  • Sign in to reply
Parents
  • Andrew J
    Andrew J over 4 years ago

    I remember doing this with purely analog components - I have a post on E14 showing it as a jokey post about breadboarding.

    Breadboarding a must

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to Andrew J

    That is extra fancy!!!

     image

    Did you ever sketch out a schematic of the build?

    That is one of the major downsides of breadboarding I have come to learn. If you don't transfer the project to a pcb/perfboard eventually is gone forever :( 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 4 years ago in reply to Andrew J

    That is extra fancy!!!

     image

    Did you ever sketch out a schematic of the build?

    That is one of the major downsides of breadboarding I have come to learn. If you don't transfer the project to a pcb/perfboard eventually is gone forever :( 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Andrew J
    Andrew J over 4 years ago in reply to scottiebabe

    I didn't but I wish I had.  I guess if I put my mind to it I could re-create it.  The core of it, 'randomising' a dice, actually came from Make: Electronics by Charles Platt so I wouldn't want to post the whole lot anyway.  I extended it quite a bit to duplicate the circuit to provide a two player set up for snap.  Press your button if the die faces match and it locks out your opponent and increases your score, on the 7-segment display, IF you were correct.  All logic chips: I even used a XNOR gate!