7-Segment Display
  • Challenges & Projects
  • Project14
  • 7-Segment Display
  • More
  • Cancel
7-Segment Display
Blog Simple clock with common cathode display
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
  • Author Author: me_Cris
  • Date Created: 4 Jun 2022 2:15 PM Date Created
  • Views 1563 views
  • Likes 11 likes
  • Comments 4 comments
  • 7-segment display
  • display
Related
Recommended

Simple clock with common cathode display

me_Cris
me_Cris
4 Jun 2022

Greetings !

I present another project in which I used a 4-digit 7-segment display, but this time it is a common cathode with 12 pins, red color.
It is a settable clock, but the idea is more about the pleasure of making a PCB, so you can share your opinion.
Using the same technique, with a multimeter and an internet search, I discovered the functionalities of the pins of this display, which one is a digit and which is a segment. It is a homemade PCB, designed in KiCAD, made in two layers, for which I used only THD components. Luckily with my friend, he has an ultraviolet device and copper vias that I plant with a manual press, so I was able to make this circuit in two layers, it was a bit difficult in one layer because it came out a bit tangled and had larger dimensions. As can be seen in the diagram below, the display is connected to uC via a 4.7kohm resistive network, without the help of any transistor, the control is performed only by the microcontroller. The numbers are formed by turning off the segments, so not turning them on. By using two push-buttons we can adjust the clock.

/resized-image/__size/1280x720/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-68/circuit.png

/resized-image/__size/1280x720/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-68/AT89C2051_5F00_CLock.png

/resized-image/__size/1280x720/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-68/AT89C2051_5F00_CLock_5F00_.png

Real Circuit

/resized-image/__size/1280x720/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-68/2.jpeg

/resized-image/__size/1280x720/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-68/3.jpeg

/cfs-file/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-68/Demo.mp4

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 4 years ago +1
    Nice project. Will you post the code for the processor ? MK
  • scottiebabe
    scottiebabe over 4 years ago +1
    Wonderful use of the SIL resistor pack! I assume you are driving the segment pins open collector? Great project!
  • DAB
    DAB over 4 years ago +1
    Very good project.
Parents
  • michaelkellett
    michaelkellett over 4 years ago

    Nice project.

    Will you post the code for the processor ?

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • me_Cris
    me_Cris over 4 years ago in reply to michaelkellett

    https://github.com/ruthsarian/at89c2051_clock

    You can find it at that link.

    P.S. I am not the author of it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • me_Cris
    me_Cris over 4 years ago in reply to michaelkellett

    https://github.com/ruthsarian/at89c2051_clock

    You can find it at that link.

    P.S. I am not the author of it.