Acoustics
  • Challenges & Projects
  • Project14
  • Acoustics
  • More
  • Cancel
Acoustics
Blog Nexgen: FAA Nav Aid Station Slant Range Math
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Acoustics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 3 Feb 2020 9:33 PM Date Created
  • Views 4070 views
  • Likes 3 likes
  • Comments 6 comments
  • flight simulator
  • nexgen
  • radio propagation
  • slant range
  • algorithms
  • dme
  • mathematics
  • radar
  • acousticsch
Related
Recommended

Nexgen: FAA Nav Aid Station Slant Range Math

phoenixcomm
phoenixcomm
3 Feb 2020
image

Acoustics

Enter Your Electronics & Design Project for a chance to win an $200 Shopping cart of product!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

image Ok in my last post I made a feeble attempt to write some code. Without the full math understanding. So I will attempt this again but I will add a new image, as seen on the right,  that will help you out.  Where R is the Slant Range, Where H is the Aircraft's altitude from the antenna and ε is the angle between R and Topogar or the distance between the antenna and the aircraft projected on the ground. R, H, and Topogar will always form a right triangle. And simply we must use a Great Circle Calculation to determine Topogar. If the station Slant Range (R) is greater than the line of sight you will not hear the Nav Aid. image image

 

In the NavAids published info Latitude and Longitude the antenna is described as so many feet off the ground we will call it ha. So we must add the antenna height, or ha to get the distance been the antenna and center of the Earth. While re is a vector from the center of the Earth to sea level, and then is extended aircraft's altitude above sea level.

A second way of looking at this is that you have 3 triangles:

  • made of the following sides: R and Topogar and the Altitude of the aircraft to the center of the antenna.
  • made of the following sides: (1) the antenna, latitude, and longitude, and the height of the antenna to the center of the earth. (2) The center of the earth to the surface.  (3) The curved section of the earth.
  • made of the following sides: (1) the antenna, latitude, and longitude and the height of the antenna above sea level. (2) Slant Range a line between the antenna and the aircraft. (3) a line from sea level to the aircraft.

 

Now Back to the math, what I have shown was radar slant range! The formula for computing the DME  slant range is the following:

 

  1.      D  = √((re+ha)2-re2)) + √(re + h)       can now be reformatted as:
  2.      D  = √( ha2+2reha) + √( hs2 + 2)
  3.      ha = 0  Assuming a receiver on the sea surface
  4.      D  ≈ √(2rehs)
SITE: Owen, J. I. R., “Results of an Investigation into the use of 1175 MH and 1202 MHz for GNSS Signals in European Airspace,” Proceedings of the 2002 National Technical Meeting of The Institute of Navigation, SanDiego, CA, January 2002, pp. 742–749
  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Your post takes me back a bunch of decades where I had to deal with line of sight, slant range, beacon visibility, over the horizon detection and other things that will remain nameless. DAB
  • robogary
    robogary over 6 years ago +1
    Become a Flat Earther and the math gets alot easier ! :-)
Parents
  • robogary
    robogary over 6 years ago

    Become a Flat Earther and the math gets alot easier !  :-) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to robogary

    robogary LOLimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to robogary

    robogary LOLimage