Acoustics
  • Challenges & Projects
  • Project14
  • Acoustics
  • More
  • Cancel
Acoustics
Blog Screaming LM386:  An Audio Amplifier with PCB Art
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Acoustics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 11 Feb 2020 7:09 AM Date Created
  • Views 7501 views
  • Likes 19 likes
  • Comments 19 comments
  • audio
  • amplifier
  • lm386
  • p14acousticsch
  • electronicartch
  • acousticsch
  • pcb art
  • lm386 audio amplifier
  • audio test
Related
Recommended

Screaming LM386:  An Audio Amplifier with PCB Art

fmilburn
fmilburn
11 Feb 2020

This is the final post in a three part series on how to create an audio amplifier using the classic TI LM386 which has been further adorned with PCB art.   The method for transferring art work to a PCB was described in the first post.  The LM386 amplifier design was documented in the second post.  In this post a summary of the art transfer process and amplifier design is presented, the PCB  is populated, and the audio amplifier tested.

image

Transferring Art to PCB

 

The PCB art is based on the famous work by Edvard Munch called The Scream.  The method used is based on the work of Andrew Sowa, with the main difference being my workflow uses Photoshop and converts the image to grey scale using the "magic wand" to isolate layers rather than a color conversion using Adobe Illustrator to create the bit map for KiCad as Andrew does.  The modified layers are brought into KiCad and converted into a footprint as shown below.  For additional information on the methods used see my first post here.

 

A palette of colors is created with the bare FR4, copper, solder mask, and silk screen.  The palette resulting from purple OSHPark boards is shown below.

image

 

By converting to a grey scale image in Photoshop and then adjusting by trial and error it is possible to isolate the layers corresponding to the palette above.  The layers below have been shaded with the palette and are the ones used in this project.

{gallery} Photoshop Layers

image

Silk on Copper

image

Copper

image

Bare FR4

image

Solder Mask on Copper

image

Solder Mask on Bare FR4

image

Stacked View in Photoshop

 

Before exiting Photoshop the layers are converted back to a pure black and white image before importing into KiCad.  That process is straight forward although a bit tedious and results in a component footprint as shown in the image below.

image

The resulting render in KiCad looks like this:

image

Amplifier Design

 

The amplifier is based around the LM386 as described in this post.  The design is taken from the LM386 datasheet but includes almost all of the optional bells and whistles.

image

 

When creating the PCB itself it was eventually decided to use the art work as a ground plane on the two layer board as it covered most of the bottom side.  Surface mount components were used for the most part on the front side so as not to unduly deface the art work.

 

The resulting unpopulated PCB as received back from OSHPark is shown in the photo below.

image

I thought the finished product looked great!

 

As noted in the video discussion of the PCB below, the main change I would make would be to increase pad sizes, especially of the trimmer used for gain.  Bringing gain out to a full sized potentiometer and adding a potentiometer for bass boost could also be considered if board size is not a consideration.

 

The final bill of materials is given below.  The small gain trimmer has been updated in this list to show the preferred part.

image

 

Discussion of the PCB

 

The video below gives more discussion on the aesthetics of the board and how the components were soldered to the PCB.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Audio Tests

 

In the video below several tests are done to see how well the amplifier compares to the datasheet.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Summary and Conclusion

 

The artwork turned out much better than expected.  However, I should note that the response I got from most engineers at the local Hardware Happy Hour where I showed it around last week was either a dull stare or ''it looks like a lot of work".  People who don't know much about PCBs don't really get it either.  But there have been enough nerds who showed excitement (and recognized The Scream) to encourage me to try this type thing again.

 

The LM386 performance met the datasheet specifications but newer Class D amplifier designs are available which are more efficient and have additional features.  For testing this design it would have been nice to bring both the Gain and Bass Boost out to full sized potentiometers.

 

Thanks for reading and comments are always welcome.

 

Links

PCB Art:  Screaming LM386

PCB Art:  The Scream

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 6 years ago +4
    Hi Frank, It's the best-looking PCB I've seen : ) The detail is apparent, and in the video, it almost looked like some art on a wall until you picked it up : ) Great, very practical project, and nice to…
  • baldengineer
    baldengineer over 6 years ago +4
    Fantastic job on the artwork side! It looks great. The meta-ness of an amplifier board with The Scream is blowing my mind. Any chance you're willing to use OSHPark's project sharing feature so that someone…
  • fmilburn
    fmilburn over 6 years ago in reply to shabaz +3
    Thank you Shabaz, That is a good idea to design it to fit a container or enclosure. Another idea would be to make a badge or jewelry of some sort as those seem to be popular. If anyone would like to make…
  • fmilburn
    fmilburn over 6 years ago in reply to phoenixcomm

    Thanks Cris!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago

    fmilburn Very Cool Frank!

    ~~Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to hugohu

    Thanks. Many of the Adafruit circuits come pretty much directly from the datasheet as did the circuit for the LM386 project above.  I enjoy putting my own twist on things and the art is one way of doing it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 6 years ago

    I'm too late but this is great!

     

    You could maybe steal borrow the circuits from Adafruit and just design your PCB.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk99
    kk99 over 6 years ago

    Awesome PCB !

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>