• Products and Partners
    Products and Partners
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
Animatronics
  • Challenges & Projects
  • Project14
  • Animatronics
  • More
  • Cancel
Animatronics
Blog Hey Moogle - an animatronic moose assistant
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Animatronics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: easyejl
  • Date Created: 13 Nov 2019 8:31 PM Date Created
  • Views 7822 views
  • Likes 9 likes
  • Comments 52 comments
  • animatronicsch
Related
Recommended

Hey Moogle - an animatronic moose assistant

easyejl
easyejl
13 Nov 2019

My wife and I went to see Evil Dead - The Musical, and I was entranced by the moose puppet on the wall. I thought "Heck, it would be easy enough to make an animatronics moose to have at home", so I set out on this project.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Basic plan steps are

  • Acquire moose head puppet
  • Acquire robotic arm + servos
  • Begin programming pi - Basically can use most of the Google AYO voice pieces, need to add some references to pulse audio to capture the sound as he's speaking, to use to move the mouth
  • Assemble pieces
  • Laugh a lot

 

Steps completed

Moose head puppet on the way from ebay!

image

Robotic arm on order

Google AYO kit reformatted back to original and programming has begun!

  • Sign in to reply

Top Comments

  • easyejl
    easyejl over 6 years ago +4
    Made some modifications to the claw, and have it able to work a puppet mouth now. It's only slow because the pi is underpowered right now, I ran out of outlets. So its being powered by the USB port on…
  • easyejl
    easyejl over 6 years ago +4
    For the claw modifications, I took out the 2 pieces circled, set the other arms to be straight and then fully tightened them. They originally were set as loose, with a locking nut so that they could bend…
  • msebok
    msebok over 6 years ago +4
    really cool progress. I was looking at the google machine and found this link, I was trying to find other methods of articulation etc...I doubt it helps or gives any ideas with your current project, but…
Parents
  • easyejl
    easyejl over 6 years ago

    the arm is almost complete. I had originally going to use the google AYO voice hardware, but was having problems getting it to specifically work with pulseaudio, which I need for reading the output volume/frequency realtime. so I picked up a different audio card. Nice thing about this specific kit is that the controller built in that you can see in the picture allows control by USB. so easy to integrate with the pi, and I don't need a 2nd servo hat on top of the audio.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • easyejl
    easyejl over 6 years ago

    the arm is almost complete. I had originally going to use the google AYO voice hardware, but was having problems getting it to specifically work with pulseaudio, which I need for reading the output volume/frequency realtime. so I picked up a different audio card. Nice thing about this specific kit is that the controller built in that you can see in the picture allows control by USB. so easy to integrate with the pi, and I don't need a 2nd servo hat on top of the audio.