Project14
  • Challenges & Projects
  • More
Project14
Blog 18650 Li ion batteries question
  • Blog
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 9 Nov 2021 4:34 PM Date Created
  • Views 2502 views
  • Likes 2 likes
  • Comments 11 comments
  • 18650_battery
Related
Recommended

18650 Li ion batteries question

dubbie
dubbie
9 Nov 2021

I have been gifted a (broken) child's electric tricycle toy. The main problem is that the 6V 4Ah lead acid battery is defective - a collapsed cell I assume. I would like to replace this battery with Li-Ion batteries, specifically the 18650 type. I am thinking of using two 18650 to get the 6V needed (it will be a bit more at 7.2V but that will just mean the tricycle goes faster - Yeah!). However, I am finding it difficult to find suitable 18650 batteries and associated charger. It is not clear what the capacity of these 18650 batteries is. Do they vary? What is the maximum capacity? I have seen 3300 mAh mentioned but I'm having trouble identifying these batteries. I could create a parallel series arrangement of batteries to get higher currents but then I do not seem to be able to find a charger. I'd like to have separate 18650 batteries so I can use them in other things such as mobile robots.

 

I thought of using a 7.2V battery pack as used in cordless drills, but I cannot find any at 7.2V (or is it 7.4V - but I cannot find any of them either), plus I'm reluctant to spend a fair bit of money without knowing if it would be suitable or not.

 

Any advice or sources of information would be welcome.

 

Dubbie

  • Sign in to reply

Top Comments

  • rsjawale24
    rsjawale24 over 4 years ago +2
    Hi! The battery capacity varies as per manufacturer. Even for the 18650 type, they are available in different capacity. I recommend to buy from a vendor that gives a datasheet along with the battery. Also…
  • jw0752
    jw0752 over 4 years ago +2
    Hi Dubbie, Unless you are paying for a quality brand name battery do not expect to get the mAh that is printed on the battery. I have tested many different East Asian Brands with ratings of 2500 mAh, 4400…
  • ralphjy
    ralphjy over 4 years ago +2
    You also need to be aware that 18650 batteries can vary in physical dimensions - especially length. Flat top batteries are about 65mm, button tops are a bit longer and protected types can be 2-4mm longer…
  • rsjawale24
    rsjawale24 over 4 years ago

    Hi! The battery capacity varies as per manufacturer. Even for the 18650 type, they are available in different capacity.

    I recommend to buy from a vendor that gives a datasheet along with the battery.

    Also, since this is a Li-ion battery, you'll need a specific charger for this. I think a generic Li-ion charger can work fine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<