Project14
  • Challenges & Projects
  • More
Project14
Blog Makevember Project - M5 ESP32Cam
  • Blog
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 5 Nov 2019 7:06 PM Date Created
  • Views 1600 views
  • Likes 8 likes
  • Comments 4 comments
  • makevember 2019
  • makevember
  • m5 esp32cam
Related
Recommended

Makevember Project - M5 ESP32Cam

ralphjy
ralphjy
5 Nov 2019

I'm waiting for my mezzanine kit to arrive today so that I can continue with my PIIP training.  Unfortunately, UPS delivers in the late afternoon - evening so I've got some time to kill.

 

I have an M5 ESP32Cam that I haven't tried yet so I thought I'd do the normal - print a case and do a quick test.  This is a pretty small camera board - 23mm x 50mm.  The board costs less than $10 but you have to add shipping cost.

 

Back in December 2017 I had solar panels installed and the utility company installed a smart meter that is bi-directional (measures what I consume and what I return to the grid).  They read the meter via a 900MHz radio.  I knew they wouldn't allow me to access the meter directly, but I had hoped that they would allow me to access the data on their website so I could track my daily consumption (SMA allows me to track the solar inverter data on their website).  Unfortunately, the utility will only provide me with monthly data (might be possible they only read it monthly?).  I've been getting the daily data the old fashioned way - visually reading the meter.  I'm going to try using the M5 camera via WiFi rather than going outside every morning and I could also automate it to take data always at the same time of the day.  This camera has a LiPo battery interface so I might be able to make it standalone by adding a battery and a small solar panel.

 

Here's a picture of the meter:

image

 

Pictures of the M5 kit:

 

Comes in nice plastic box -seems to be a packaging trend (fewer damaged boards)

image

 

The camera side with the USB C connector on top

image

 

ESP32 side with Grove connector on top, WiFi antenna on bottom, ESP32 is next to the antenna.  The heatsink is for the ESP32 - there is a warning about overheating with continuous operation.

image

 

I bought a 500maH battery that is approximately the same size as the board.

image

 

I 3D printed a two piece case.  It was quick because of the small size.  Looks like I had some contaminant in the filament (discoloration by the lens hole).

image

 

Camera Board in the case

image

 

Battery fits on top (there is no battery connector on the PCB, so I'll need to solder some wires to the provided pads)

image

 

Lens side view

image

 

Connector side view

image

 

Hooked up to battery bank for test.  I may want to disable that bright red LED.

image

 

The M5cam comes pre-flashed with firmware that configures a WiFi access point which allows you to grab images from its webserver.  I connected my iPad to it for a quick test.  You can see the image of the Ultra96 on the iPad screen.  The image is flipped horizontally.  Can't imagine why they set it up that way but I'll need to recompile the program to fix it.

image

 

The other thing that I noticed is that the image stream stutters (pauses periodically).  I'll need to look into that.  Here is a video with an example of the stutter:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I'll probably not get around to completing this setup until next January.  Lots of work left.  Need to figure out how to mount this on the meter and add the solar panel and hook up the battery.  And some software and firmware.  Will need power management and to protect it from rain.

 

Good enough progress for a Makevember project.......

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 6 years ago +3
    This is a nice idea. I'd seen the M5 stack before, but hadn't looked lately all the items they sell. This board is inexpensive from the M5 web site. https://m5stack.com/products/esp32-camera?_pos=5&_sid…
  • dubbie
    dubbie over 6 years ago +2
    I like this. I've just purchased an ESP32 CAM board and this makes it look easy to get started with. Dubbie
  • neilk
    neilk over 6 years ago +1
    Looks fantastic for the price. I've added it to my "to buy and do list"! Neil
Parents
  • skywalker1211
    skywalker1211 over 6 years ago

    interesting project.

    added to my to do list.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • skywalker1211
    skywalker1211 over 6 years ago

    interesting project.

    added to my to do list.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data