PYNQ Workshop
  • Challenges & Projects
  • Project14
  • PYNQ Workshop
  • More
  • Cancel
PYNQ Workshop
Blog PYNQ-Z2 Select Video Source
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PYNQ Workshop to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 7 Jun 2020 12:01 AM Date Created
  • Views 2294 views
  • Likes 3 likes
  • Comments 6 comments
  • pynq-z2
  • pynq workshop
  • pynqhero
  • pynqstarter
Related
Recommended

PYNQ-Z2 Select Video Source

ralphjy
ralphjy
7 Jun 2020

I'm finally getting around to doing my homework from session 3.  I decided to do a simple modification of adding an AXI4-Stream Switch so that I could select between video sources, in this case between the HDMI camera and the TPG (test pattern generator).

 

I started with the overlay from session 3 and added back the TPG and added an AXI4-Stream Switch.  Seems very straightforward but I encountered a problem that I didn't expect.  The TPG apparently only uses a single clock domain for the AXI control and the video generation.  That meant I had clock conflicts with the frontend implementation which was using a separate video clock and AXI control clock.  Luckily there is an AXI4-Stream Clock Converter that provides syncing across clock domains.  So I added one of those.

 

Here's the diagram showing the added parts:

image

I have two slave inputs into the Stream Switch and one master output.  The switch can handle 16 inputs and 16 outputs.

 

The frontend (HDMI camera) is Slave 0 (SI0) and the TPG is Slave 1 (SI1).

 

The register offset for the master 0 output (MI0) is 0x40.  The value in the register selects which input is used.

 

When testing it out I found something I hadn't expected - if I didn't configure the Stream Switch first - the frontend wouldn't start.  Had me baffled for a bit.

 

Here's the Jupyter notebook:

image

image

 

The color space matrix has an error that I corrected. (Should be a diagonal - fixed it for the video).

 

And a short video showing it operating:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 6 years ago +2
    Excellent work ! Looks like your over halfway there to having an automated video production console to help in making Element 14 project videos ! I've still not got the PYNQ-Z2 to recognise the recommended…
  • Fred27
    Fred27 over 6 years ago +2
    I used a Raspberry Pi and camera instead of the recommended one. I have a Zybo Z7 and a Pcam 5C from a previous road test, so I'm currently looking at building PYNQ for that (and disappearing down a rabbit…
  • beacon_dave
    beacon_dave over 6 years ago in reply to ralphjy +2
    "...I’ve been trying to figure out where the hdmi_out_hpd_irq should go for the constraints file..." The TUL pynq-z2_v1.0xdc lists the hot plug detect input as being: #set_property -dict { PACKAGE_PIN…
Parents
  • beacon_dave
    beacon_dave over 6 years ago

    Excellent work !

     

    Looks like your over halfway there to having an automated video production console to help in making Element 14 project videos !  image

     

    I've still not got the PYNQ-Z2 to recognise the recommended Crosstour action cam yet. I ended up having to use a laptop with webcam in order to scan the barcode on a tin of baked beans... (Busy writing up a blog on my adventures with PYNQ & GPIO at the moment.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to beacon_dave

    Someone needs to figure out what’s up with those cameras....

     

    I should have thought about scanning the canned goods image.

     

    I’ll watch for your blog.  Have you figured out where to find the pin assignments for the board?  I’ve been trying to figure out where the hdmi_out_hpd_irq should go for the constraints file.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to ralphjy

    "...I’ve been trying to figure out where the hdmi_out_hpd_irq should go for the constraints file..."

     

    The TUL pynq-z2_v1.0xdc lists the hot plug detect input as being:

     

    #set_property -dict { PACKAGE_PIN R19   IOSTANDARD LVCMOS33 } [get_ports { hdmi_tx_hpdn }]; #IO_0_34 Sch=hdmi_tx_hpdn

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to beacon_dave

    Thanks.  I should RTFM.  I was looking at the constraints file from the PYNQ-Z2 build for the Base overlay.  I've downloaded the file from TUL.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 6 years ago in reply to beacon_dave

    Thanks.  I should RTFM.  I was looking at the constraints file from the PYNQ-Z2 build for the Base overlay.  I've downloaded the file from TUL.