PYNQ Workshop
  • Challenges & Projects
  • Project14
  • PYNQ Workshop
  • More
  • Cancel
PYNQ Workshop

Blog

  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PYNQ Workshop to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • 2020 PYNQ-Z2 Workshop - in 2026: Getting Started/Lab 1

    kmikemoo
    kmikemoo
    I have a little more time on my hands these days and while looking for something (I forget what), I came across the PYNQ-Z2 board that I had won in a Hackster competition.  It was kind of a bucket raffle where you earned points and could "bid" o...
    • 20 Feb 2026
  • PYNQ Overlay creation per Getting up and Running

    grondak
    grondak
    This was a tutorial without feedback. I had NO idea what I did except to click , drag, and connect. I double-checked my connections and the bitstream came out fine.  I wish I would have an understanding of what the IP components do beyond their ...
    • 29 Aug 2020
  • QNNClassifier Fun

    grondak
    grondak
    I used scp to copy images from my host machine into the QNN classifer's directory to see what happened. A pile of cigarette butts was missed-- it got some animal. I threw it an italian spinone dog and it got the following:class: otterhound probabilit...
    • 28 Aug 2020
  • My final creation

    weiwei2
    weiwei2
    first of all, i am truly sorry for delay in posting, as there is some shipment complexity and i only got my PYNQ-Z2 board first week of July. it is somewhat too short time to rush through everythingeventually over the last week , i manage to rush thr...
    • 3 Aug 2020
  • PYNQ Workshop 2

    weiwei2
    weiwei2
    By the time i got my board to test it is early July, so it is kind of latefor the session 2, my original aim is to use does overlay on IO to control on/off of water pump to shoot waterfollowing the lab book 2 (which is also accessible from Github htt...
    • 3 Aug 2020
  • Ping Pong trainer

    yuricts
    yuricts
    Introduction First of all, this is a work in progress. This blog will be updated regularly. I did not post any of this yet since development is going slow. Partly due to the beginning of July being very hectic work-wise...Anyhow, I would like to...
    • 28 Jul 2020
  • Ponq - bringing Pong to life with Pynq

    Fred27
    Fred27
    What's Ponq?A false startI'd been wondering exactly what to so for my PYNQ embedded vision project. I'd started out with an attempt to identify racing kayaks as they crossed the finish line, but I was having a lot of trouble with the OCR ...
    • 7 Jul 2020
  • Install OpenVINO on PYNQ-Z2

    ralphjy
    ralphjy
    I received an Intel NCS 2 from the Hackster Deep Learning Giveaway.  I've used the original NCS on the PYNQ-Z2 and the Ultra96v2 using the NCSDK toolkit and I've just tried the NCS and NCS 2 on a RPi4 using the OpenVINO toolkit. &nb...
    • 13 Jun 2020
  • Using PYNQ as user interface/user experience platform

    riklaunim
    riklaunim
    Using OpenCV to detect a face or other specific object on an image isn't something new or groundbreaking. However many machine vision applications are based on such functionality and the best ones excel because they provide the best UI and user e...
    • 8 Jun 2020
  • PYNQ-Z2 Select Video Source

    ralphjy
    ralphjy
    I'm finally getting around to doing my homework from session 3.  I decided to do a simple modification of adding an AXI4-Stream Switch so that I could select between video sources, in this case between the HDMI camera and the TPG (test patte...
    • 7 Jun 2020
  • PYNQ-Z2 Workshop - Lab 1: Debugging CAN Project with PYNQ

    maxim.yudayev
    maxim.yudayev
    TL;DR: Debugging a CAN board with PYNQ-Z2's logictools and WaveDrom ->              -> A lot faster than debugging Assembly! This blog is long overdue, I hope your tea did not...
    • 5 Jun 2020
  • PYNQ Session 1: pynq starter project with logictools overlay : The missing blog

    ipv1
    ipv1
    The PYNQ is a versatile platform that combines the power of FPGA with the flexibility of software(python on linux). Running atop the Zynq series of SOCs from Xilinx, this platform builds towards rapid prototyping of solutions.   In this blo...
    • 31 May 2020
  • Auxiliary PYNQ-Z2 features - using USB, GPIO and various HDMI setups for handy HDMI processing

    riklaunim
    riklaunim
    The webinar focused on video processing while the PYNQ-Z2 board has additional features that can be used when making an edge-processing prototype.You can use the USB host connector to connect a UART serial/RS232 adapter to then control some electroni...
    • 31 May 2020
  • Pynq-Z2 Getting Up and Running Overlay Modification

    ralphjy
    ralphjy
    I was somewhat inspired by beacon_dave 's post on his overlay modification so I decided to do something very similar.  I'm adding the Button interface to the overlay we created in Session 2 so that I can control the pattern that is displ...
    • 25 May 2020
  • PYNQ-Z2 Getting Up and Running

    ralphjy
    ralphjy
    Another great workshop with Adam Taylor today.  Adam went through creating a new Pynq overlay in Vivado.  The workshop created an overlay with a VDMA element to interface the TPG (test pattern generator) with the Processing system. The...
    • 20 May 2020
  • PYNQ-Z2 workshop -> after the first session

    weiwei2
    weiwei2
    In session #1 of the workshop, i have learned a coupled of new things -the Linux that runs on the PYNQ-Z2 is PetaLinux-we can do RISC-V overlay on it Adam Taylor has provided a concise introduction about PYNQ-Z2 with sufficient information ...
    • 19 May 2020
  • PYNQ pink basics pinking around

    riklaunim
    riklaunim
    There is a lot of electronics or IoT connection points for Python developers or just makers playing with their Micro:Bit, Raspberry Pi or other board powered by Zerynth, TinkerForge, MicroPython, CircuitPython and alike. Among all of those there is n...
    • 11 May 2020
  • The hottest FPGA game of 2020

    chris244
    chris244
    Below is the hottest game of 2020. A £500 reward is given to anyone who is able to win. A light run to the right will indicate a sequence beggining with a length 1 for you to remember, a second light run to the right shows the sequence has finis...
    • 11 May 2020
  • PYNQ-Z2 Getting Started - I2C Trace Analyzer

    ralphjy
    ralphjy
    PYNQ-Z2: Embedded Vision Workshop Series with Adam Taylor Getting Started | Getting Up and Running  | Unlocking Your Inner PYNQ Hero  | Project14 | PYNQ Workshop  Session 1 of the workshop covered two overlays that are included i...
    • 7 May 2020
  • Getting started with PYNQ-Z2

    equaltoall
    equaltoall
    PYNQ-Z2: Embedded Vision Workshop Series with Adam Taylor Getting Started | Getting Up and Running  | Unlocking Your Inner PYNQ Hero  | Project14 | PYNQ Workshop  I've been cutting my teeth with this board since Sunday night....
    • 7 May 2020
  • Taylor waves - WaveDrom demonstration on the PYNQ framework

    yuricts
    yuricts
    PYNQ-Z2: Embedded Vision Workshop Series with Adam Taylor Getting Started | Getting Up and Running  | Unlocking Your Inner PYNQ Hero  | Project14 | PYNQ Workshop  TL;DR - How many waves can you add to WaveDrom? Benchmark it using...
    • 6 May 2020