Project14
  • Challenges & Projects
  • More
Project14
Blog PYNQ-Z2 Select Video Source
  • Blog
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 7 Jun 2020 12:01 AM Date Created
  • Views 2128 views
  • Likes 3 likes
  • Comments 6 comments
  • pynq-z2
  • pynq workshop
  • pynqhero
  • pynqstarter
Related
Recommended

PYNQ-Z2 Select Video Source

ralphjy
ralphjy
7 Jun 2020

I'm finally getting around to doing my homework from session 3.  I decided to do a simple modification of adding an AXI4-Stream Switch so that I could select between video sources, in this case between the HDMI camera and the TPG (test pattern generator).

 

I started with the overlay from session 3 and added back the TPG and added an AXI4-Stream Switch.  Seems very straightforward but I encountered a problem that I didn't expect.  The TPG apparently only uses a single clock domain for the AXI control and the video generation.  That meant I had clock conflicts with the frontend implementation which was using a separate video clock and AXI control clock.  Luckily there is an AXI4-Stream Clock Converter that provides syncing across clock domains.  So I added one of those.

 

Here's the diagram showing the added parts:

image

I have two slave inputs into the Stream Switch and one master output.  The switch can handle 16 inputs and 16 outputs.

 

The frontend (HDMI camera) is Slave 0 (SI0) and the TPG is Slave 1 (SI1).

 

The register offset for the master 0 output (MI0) is 0x40.  The value in the register selects which input is used.

 

When testing it out I found something I hadn't expected - if I didn't configure the Stream Switch first - the frontend wouldn't start.  Had me baffled for a bit.

 

Here's the Jupyter notebook:

image

image

 

The color space matrix has an error that I corrected. (Should be a diagonal - fixed it for the video).

 

And a short video showing it operating:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 5 years ago +2
    Excellent work ! Looks like your over halfway there to having an automated video production console to help in making Element 14 project videos ! I've still not got the PYNQ-Z2 to recognise the recommended…
  • Fred27
    Fred27 over 5 years ago +2
    I used a Raspberry Pi and camera instead of the recommended one. I have a Zybo Z7 and a Pcam 5C from a previous road test, so I'm currently looking at building PYNQ for that (and disappearing down a rabbit…
  • beacon_dave
    beacon_dave over 5 years ago in reply to ralphjy +2
    "...I’ve been trying to figure out where the hdmi_out_hpd_irq should go for the constraints file..." The TUL pynq-z2_v1.0xdc lists the hot plug detect input as being: #set_property -dict { PACKAGE_PIN…
  • beacon_dave
    beacon_dave over 5 years ago

    Excellent work !

     

    Looks like your over halfway there to having an automated video production console to help in making Element 14 project videos !  image

     

    I've still not got the PYNQ-Z2 to recognise the recommended Crosstour action cam yet. I ended up having to use a laptop with webcam in order to scan the barcode on a tin of baked beans... (Busy writing up a blog on my adventures with PYNQ & GPIO at the moment.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<