Project14
  • Challenges & Projects
  • More
Project14
Blog What 2022 Arduino Week Challenge Are You Interested In?
  • Blog
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 2 Mar 2022 4:28 PM Date Created
  • Views 2516 views
  • Likes 11 likes
  • Comments 9 comments
Related
Recommended

What 2022 Arduino Week Challenge Are You Interested In?

tariq.ahmad
tariq.ahmad
2 Mar 2022

Every year on the community we do a special Arduino Day Challenge.  Last year,  we did a Drone Workshop followed by a Drone project competition.   The year before that we did a NanoRama competition which focused on Arduino's Nano product line. The year before that we did an Open Arduino challenge.  This year,  instead of an Arduino Day,   Arduino will be celebrating an Arduino Week from March 21st - March 26th and we need your help finalizing our plans on the community for how we'll celebrate Arduino this year.  We try to do something different every year so this year we'll be holding a Nicla Sense ME workshop with balearicdynamics followed by an Arduino Week Competition that features the Nicla Sense ME board.

image
Buy Now

In preparation for the Arduino Week Workshop we've sent balearicdynamics a Nicla Sense ME board and he's come up with some great ideas around the board and since it features a multifunction sensor, we were thinking of this year could focus on "Environment monitoring" or "One Room Climate Change"?  For example,  a climate change related challenge could focus on the shower, temperature water control, garage state monitoring, etc.  We've also noticed that TinyML and using something like EdgeImpulse to easily add ML to your project has been a very popular subject on the community and want to give members a chance to explore this topic with a proper project competition.   Although Nicla Sense ME is the board we'll be focused on there are already a couple of other really good solutions from Arduino for enabling ML in addition to the Niclas Sense ME board (Nano Sense 33 and the Portenta boards).

If you're not familiar with the Nicla Sense 33 board then here are some details from the Arduino site:

The Nicla Sense ME is a tiny, low-power tool that sets a new standard for intelligent sensing solutions. With the simplicity of integration and scalability of the Arduino ecosystem, the board combines four state-of-the-art sensors from Bosch Sensortec:

  • BHI260AP motion sensor system with integrated AI
  • BMM150 magnetometer
  • BMP390 pressure sensor
  • BME688 4-in-1 gas sensor with AI and integrated high-linearity, as well as high-accuracy pressure, humidity and temperature sensors. 

Designed to easily analyze motion and the surrounding environment – hence the “M” and “E” in the name – it measures rotation, acceleration, pressure, humidity, temperature, air quality and CO2 levels by introducing completely new Bosch Sensortec sensors on the market. Its tiny size and robust design make it suitable for projects that need to combine sensor fusion and AI capabilities on the edge, thanks to a strong computational power and low-consumption combination that can even lead to standalone applications when battery operated. Part of Arduino Pro’s new Nicla family of modular, intelligent products that are easy to use, cost effective, versatile and accessible, the Sense ME has a new, tiny form factor that is also compatible with the Arduino MKR and Portenta ranges.

Key benefits

  • Tiny size, packed with features
  • Low power consumption
  • Add sensing capabilities to existing projects
  • When battery-powered, becomes a complete standalone board
  • Powerful processor, capable of hosting intelligence on the Edge
  • Measures motion and environmental parameters
  • Robust hardware including industrial-grade sensors with embedded AI
  • BLE connectivity maximizes compatibility with professional and consumer equipment
  • 24/7 always-on sensor data processing at ultra-low power consumption

Tech Specs:

MICROCONTROLLER

64 MHz Arm® Cortex M4 (nRF52832)

Nordic Semiconductor nRF52832 Product Brief

SENSORS

BHI260AP - Self-learning AI smart sensor with integrated accelerometer and gyroscope, BMP390 - Digital pressure sensor, BMM150 - Geomagnetic sensor, BME688 - Digital low power gas, pressure, temperature & humidity sensor with AI

Bosch BHI260AP Datasheet

Bosch BMP390 Datasheet

Bosch BMM150 Datasheet

Bosch BME688 Datasheet

I/O Castellated pins with the following features: 1x I2C bus (with ext. ESLOV connector), 1x serial port, 1x SPI, 2x ADC , programmable I/O voltage from 1.8-3.3V
CONNECTIVITY Bluetooth® 4.2
POWER Micro USB (USB-B), Pin Header, 3.7V Li-po battery with Integrated battery charger
MEMORY 512KB Flash / 64KB RAM, 2MB SPI Flash for storage, 2MB QSPI dedicated for BHI260AP
INTERFACE USB interface with debug functionality

image image
Environmental Monitoring One Climate Change
image image
Open ML IoT Remote Sensing Applications

image

  • Sign in to reply

Top Comments

  • tariq.ahmad
    tariq.ahmad over 4 years ago in reply to dubbie +2
    Yes. The project competition will be open ended. You can use any board you like. I'm finalizing things now and will make an announcement on Monday. It will be a make the world better competition and I…
  • javagoza
    javagoza over 4 years ago +1
    Arduino week is an event that spreads happiness but this year is special for everyone, we have gone from being aware of not getting sick from COVID-19 to fearing " war ". As a father of a family there…
Parents
  • genebren
    genebren over 4 years ago

    I think that this would make a great machine controller.  I have a client that builds animatronic displays (Halloween Props).  I am currently working on a project for him to directly control elements of these displays by using realtime motions of an hidden actor(s) as opposed to prerecorded sequences.  I could easily see that the Nicla Sense ME board would make an excellent controller for this application, as well as many other forms of machine (robot) control.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tariq.ahmad
    tariq.ahmad over 4 years ago in reply to genebren

    It does seem like there are some excellent predictive maintenance applications that could be used here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • tariq.ahmad
    tariq.ahmad over 4 years ago in reply to genebren

    It does seem like there are some excellent predictive maintenance applications that could be used here.