Project14
  • Challenges & Projects
  • More
Project14
Makevember! Makevember: Project Revive Bot #2 - X-Y Plotter
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: skywalker1211
  • Date Created: 16 Nov 2019 2:00 PM Date Created
  • Views 2479 views
  • Likes 10 likes
  • Comments 6 comments
  • arduino project
  • makevember 2019
  • makevember
  • grbl
  • laser engraving
Related
Recommended

Makevember: Project Revive Bot #2 - X-Y Plotter

skywalker1211
skywalker1211
16 Nov 2019

i brought back this machine from ex-company 18 months ago. at that time, they allowed us to bring back to-be-disposed item from company.

i found this machine which i believe it was x-y plotter/cutter prototype.

mechanical structure still in good condition.

wiring is a mess. missing motor and motor driver. i dont know if it is functional.

image

 

vertical axis motor missing. looks like a nema17 stepper motor.

image

 

limit sensor still in place

image

 

the machine uses timing belt, not lead screw for x-y motion.

i guess this might be the reason why they threw it.

i feel the machine might suffer from under power motor or low precision problem.

image

 

 

my plan is to revive this bot as a x-y laser plotter machine.

first of all, i am going to test if this machine still functional.

ordered a nema17 motor, arduino cnc v3 shield and few pcs drv8825.

will test once the components arrive.

 

 

Parts arrived,  assembled and install on the machine.

image

 

some wiring job. the wiring still is a mess. got to find some time later to clean it up. my priority still to get the machine run for the first time.

image

 

 

image

 

have a quick setup with grbl. this is my first time on it. i like the simplicity of grbl, hassle free if using arduino uno. the configuration is done later using UI.

ordered a 2500mw laser head, havent received. i test only x-y movement with laserGRBL UI. https://lasergrbl.com/en/.

I have to acknowledge Simen Svale Skogsrud, Sungeun(Sonny) K. Jeon, and arkypita. Their work make my life easier.

 

The machine is well built, movement is smooth.

 

homing.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

dummy drawing without laser head

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

waiting for this laser head. cant wait to have my first laser engraved wood by next week.

image

 

I got the laser head arrive yesterday.

make a not so nice looking bracket to mount it on the machine.

image

 

cant wait to test it out. power is on, connection is on, protection glass is on.

tested my first drawing on an acrylic sheet.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

There are still some issues to solve before I can get my first pretty print.

On the first few minutes, the machine runs without problem. It start jerking afterwards, I guess the driver is too hot and has thermal shutdown.

Laser power is too strong, and it penetrates the sheet. Also, I need to adjust the laser head focal length to get the best resolution.

Protector/Cover for this machine.

I think it is enough to get me busy for another 1 or 2 weeks.

 

finally, i get the printing done.

driver overheat problem - reduce current limit rating to slightly higher than what motor needs.

laser power is not too strong after tested with medium density fibreboard. i should have bought 10w laserhead. can get faster printing speed with that.

still thinking if want to make a cover for it. i am having new idea to repurpose this machine to a flying probe machine.

image

 

printing process, with 20x fast forward

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 6 years ago +2
    Nicely done so far. I look forward to seeing your progress when the laser head arrives. I have to ask - are you adding a safety cover and interlock system as your eyesight and that of other people is very…
  • skywalker1211
    skywalker1211 over 6 years ago in reply to 14rhb +2
    thanks for the suggestion. at this moment i haven't thought of cover and interlock yet. but you are right, proper protection is a must. i will get a cover for it. grbl has a estop input, i can use that…
  • DAB
    DAB over 6 years ago +1
    The plotter looks reasonably well built. You should be able to do a good job in repurposing this device. DAB
Parents
  • dubbie
    dubbie over 6 years ago

    A nice find. I once had a massive X-Y plotter bed, probably 2 x 2 metres which had been used for cutting the masks used in making integrated circuits (a long, long time ago). I was very excited when I first got it, but time passed, other pressures in life and after many years of doing nothing to it it was disposed off. I hope you achieve a better outcome than I did.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    A nice find. I once had a massive X-Y plotter bed, probably 2 x 2 metres which had been used for cutting the masks used in making integrated circuits (a long, long time ago). I was very excited when I first got it, but time passed, other pressures in life and after many years of doing nothing to it it was disposed off. I hope you achieve a better outcome than I did.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • skywalker1211
    skywalker1211 over 6 years ago in reply to dubbie

    2m x 2m. that is a big one.

    back in the day, it is not easy to build circuit/firmware, have to go into bare metal programming for it.

    thanks to arduino and those opensource hardware/library, thing becomes much simpler now.