Build a Present
  • Challenges & Projects
  • Project14
  • Build a Present
  • More
  • Cancel
Build a Present
Blog A customizable light and music box and a gift to the e14 community - Part 1
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
  • Author Author: rsjawale24
  • Date Created: 14 Jan 2022 4:52 AM Date Created
  • Views 1167 views
  • Likes 12 likes
  • Comments 0 comments
  • happyholidays
  • leds
  • project14
  • buildapresentch
  • arduino
Related
Recommended

A customizable light and music box and a gift to the e14 community - Part 1

rsjawale24
rsjawale24
14 Jan 2022

Introduction

My project14 idea for the Build a Present contest is to make a transparent music box made of plexiglass and light it up using RGB LEDs. I'm using plexiglass for two reasons- First because it is transparent in nature. Second, a single LED can be used to light up the entire sheet of plexiglass this will reduce the power requirement and the project can be powered using a battery.

The idea is to use a single SMD RGB LED on one of the edges of the plexiglass sheet and engrave a message on the sheet. The SMD RGB LED is interfaced with an Arduino (Arduino UNO in my case as I don't have a smaller form factor Arduino) so that the R,G,B can be combined to obtain different colors. Also effects such as blink and fading can be added to the LED. I have run some initial tests with the plexiglass sheet and SMD RGB LED from muticomp.

Parts Used

Arduino UNO x 1

Transparent Plexiglass sheets of 2 inch thickness x 4

MP001251 SMD RGB LED x 1

Piezo buzzer x 1 (later part for adding music)

Initial Tests

For the initial tests, I interfaced the RGB LED with Arduino UNO and pasted the LED onto one of the edges of the plexiglass sheet.

The results are shown below

image

In the next blog, I will engrave a message on the plexiglass sheet and add effects to the LEDs along with some holiday music which can played using the piezo buzzer.

EDIT: Some last-minute changes. I won't be engraving the plexiglass sheet. Instead, I'm going to use RGB LEDs. Will post a blog soon with the update.