Build a Present
  • Challenges & Projects
  • Project14
  • Build a Present
  • More
  • Cancel
Build a Present
Blog Arduino UNO Mini Limited Edition comes home.
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
  • Author Author: javagoza
  • Date Created: 7 Feb 2022 8:00 PM Date Created
  • Views 3798 views
  • Likes 15 likes
  • Comments 1 comment
  • buildapresentch
Related
Recommended

Arduino UNO Mini Limited Edition comes home.

javagoza
javagoza
7 Feb 2022
Arduino UNO Mini Limited Edition comes home.

I have been one of the lucky ones who have received an Arduino Mini UNO Gold Limited Edition .

/challenges-projects/project14/buildapresent/b/blog/posts/mini-gold-uno-winners-16-presents-to-celebrate-the-16th-anniversary-of-the-arduino-uno

It comes in a special case. It's a really small, black & gold and fully functional board.

image

As with the UNO the board comes ready to use just like the original Arduino UNO. Just change the USB connector, which in this case is a USB C and the Pin Header Pitch (distance between pin holes) is 0.05", or 1.27 mm. This is half the distance compared to the classic, regular sized UNO (0.1", 2.54mm).

image

After playing with it for a while, it has returned to the box, it will be a nice souvenir of this last year full of projects and surprise boxes from element14.

We'll think of a cool project for it.

  • Sign in to reply
  • rsjawale24
    rsjawale24 over 4 years ago

    Wow! It looks cool!