Circuit Prototype Techniques
  • Challenges & Projects
  • Project14
  • Circuit Prototype Techniques
  • More
  • Cancel
Circuit Prototype Techniques
Blog Proto Board Performance Enhancing Wingdings
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Prototype Techniques to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 21 Feb 2022 12:58 AM Date Created
  • Views 33965 views
  • Likes 18 likes
  • Comments 5 comments
  • breadboard
  • Protyping
  • circuitprototypingch
  • stripboard
Related
Recommended

Proto Board Performance Enhancing Wingdings

kmikemoo
kmikemoo
21 Feb 2022

Many of my projects start out a little half baked so breadboarding them is a must.  One of the things that has bothered me in the past is when I need a common buss and I run out of holes.  Sure I can add a jumper, but that "costs" me two holes.

Need Another Hole   Jumper Installed   I have ten holes but only eight are usable.  Why can't I have it all?

I also breadboard to try to get a vision of what the final circuit layout will look like.  As you can imagine, there is typically more than one iteration and physical placement becomes a consideration.

Most of us have scraps and extras laying about.  I can't be the only one that couldn't resist buying the 100 pack of Arduino headers when it was just a couple of dollars more than the 10 pack.

Scraps and Extras

Well...

Single Buss 1   Single Buss 2   Single Buss 3   Single Buss 4

Now I have 12 holes AND I've recovered a jumper.    Headers soldered onto strip board and cut to size.  Very handy.  I did have to file the sides of the headers to get them to fit flush together.  The pins serve more as anchors but the parallel conductors in the proto board sure can't hurt.

It does not have to stop there.

Triple Buss 1   Triple Buss 2

This is a three buss rail.  I did get lazy and didn't go for the flush mounting, but it's prototyping.  It's also three 24 hole common rails.  Very handy.

Then comes the issue of an Arduino Nano or Raspberry Pi Pico on the proto board.  What if I need more connections - and then want to measure the output of the pin?  No problem.  Header stripboard wings.

Pico Wings 1   Pico Wings 2   Pico Wings 3

During a moment of unusual clarity, I realized that I had proto board and headers that I was saving for... yeah... WHAT?!  A future project?  If you have it, use it.  I made this and used it during Build Inside The Box as a launching point to build my circuit.

Layout Starting Point

There are times that I need to break the project into pieces - so I'll actually build (at least some of) it.  The tiny breadboards help.

Tiny Breadboards   Shout out to Jan Cumps.  You can see I still have A Crystal Clock with 1 Transistor---The Pierce Oscillator assembled.

The female headers will work but on these I revert back to my original solution - extra bits of male headers and strip board.  These don't create busses as much as equipotential zones.  <- There's my powerline grounding training sneaking out.

Electrically Common Zones

I hope folks find these simple, built from scraps solutions as helpful as I did.  I always feel better when I can use the little leftovers.  I'm kind of a cheap guy.

AND it proves that strip board is the best prototyping board ever!  Reference dougw  Strip Board - Is It The Best Prototyping Board.

  • Sign in to reply

Top Comments

  • robogary
    robogary over 4 years ago +2
    Hi Mike - 100% agree ! use them headers. I have used the headers to make sockets for the Arduino Nanos so I can reuse the Nanos in different projects but also get those projects back in service quickly…
  • shabaz
    shabaz over 4 years ago +1
    Hi Mike, Very good idea, for a very frequent problem!
  • kmikemoo
    kmikemoo over 4 years ago in reply to robogary +1
    robogary Nice! I like the modular approach.
  • dubbie
    dubbie over 4 years ago

    An interesting idea. I think I will have to see what I have hidden away to see if I can also make some useful 'expanders' . Or I might just buy bigger protoboards - which is what I currently do. Or build smaller projects.

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 4 years ago in reply to robogary

    robogary  Nice!  I like the modular approach. Thumbsup

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago

    Hi Mike - 100% agree ! use them headers.  I have used the headers to make sockets for the Arduino Nanos so I can reuse the Nanos in different projects but also get those projects back in service quickly by reloading SW and plugging a Nano back in. I also use the headers for some prototyping with level shifters. I can replace the level shifters easily if they fail, and make the connections with the same jumpers as with a solderless breadboard......... without using a solderless breadboard.

    imageimageimage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 4 years ago

    Hi Mike

    Brilliant idea!

    I have a box of odd bits of stripboard and headers!

    neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Hi Mike,

    Very good idea, for a very frequent problem!