Circuit Prototype Techniques
  • Challenges & Projects
  • Project14
  • Circuit Prototype Techniques
  • More
  • Cancel
Circuit Prototype Techniques
Blog Prototyping experiences
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Prototype Techniques to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: strb
  • Date Created: 1 Feb 2022 7:57 PM Date Created
  • Views 1626 views
  • Likes 8 likes
  • Comments 4 comments
  • esc
  • Protyping
  • circuitprototypingch
  • project14
  • circuitprototypetechniques
Related
Recommended

Prototyping experiences

strb
strb
1 Feb 2022

Hi all!

There is no such "superior prototype technique" for circuits. Every project has its unique caracteristics and that imply different prototyping technniques. Down below I will present my experiences, what techniques I use the most, what I don't use that often and what I like the most. Feel free to comment and share your experience!

Pen and paper

No, I'm not suggesting you to grab some conductive ink and connect components by drawing traces on a piece of paper (altough you could do so if you want Slight smile ).  I'm talking about sketches, block diagrams or simply writing down whatever you want to create.
Personally I never skip this step, even for the simpler project. Even a simple drawing on a 5cm by 5cm paper offcut, but I always put on paper what I want to create.
Why is that so important? Conveing ideas into something that is not volatile allow me to better imagine, organize and implement what I'm planning to create. Without that, I would probably need a bigger bucket for failed projects and quite a bit of air freshener to cover the "magic smoke" smell Slight smile.
That is why, for me, planning ahead on a piece of paper is the most valuable tool at my disposal. And it's also cheap!

           image 
30 pages of reasoning and learning just for a single project!

  image

One of many block diagrams.

Breadboards

Another easy way to test a circuit is to built it on a breadboard. It can't be easier than this: just grab components, push them into the breadboard and add connections with a solid core wire.
However, I don't use breadboards very often to build complete circuits for two main reasons:I have only two relatively small breadboards (so I'm space limited) and also connecting a lot of components one to another can become a bit messy if wiring isn't managed correctly. What I actually like to do is to to test, when possible, smaller sub circuits using breadboards. By doing so I can keep complexity low while troubleshooting in a time efficient way any possible problem.
Following the same logic, I've also used them as temporary "mod board": just bring out needed signals from your pcb (or microcontroller evaluation board!) to an external breadboard, add additional circuit and then feed back the signal on the "main" board. If it works on a breadboard, the additional circuitry will work for sure once integrated on a single pcb Wink.

image
This is quite an old photo, but it shows well how I like to use breadboards to test sub circuits in conjunction with other PCBs

Perfboards

Perfboard (perforated boards, prototype board, call them how you prefer Wink) to me are an happy middleground to obtain a working circuit that could be moved, used and carried around without the fear of losing camponents because they unclip from the breadboard (it's rare, but I have some buttons that really like to pop free from my breadboards). It's also a more reliable way to building a circuit if you need any kind of high current capability.
Perfboards exist in many different kinds: you can find ones with array of single pads , with premade connections bars, with the same connection layout of a breadboard and so on. My absolute favourites are boards with pads isolated one to another, simply because to me are the most flexible ones: I can just keep on hand a few of them and I can arrange a circuit as I need without the limitation of pre made connections.

image 

  image

Example of a circuit made using perfboard: pulse generator to measure inductance of a motor

DIY PCBs

One step further from perfboards are actual dyi PCBs. Usually manufacturing can be divided into two categories: mechanical milling and chemical etching. Personally I like (and use) the first option simply because it's less messy and I don't have to manage and properly dispose chemical solutions.
Milling PCBs comes with it's own set of challenges, expecially when done using a self made router, but good results are still achievable. Tracks down to 0.5mm can be done with a bit of patience and machine tuning.
The main downside of this method, compared to a "real" PCB is the absence of plated vias. Trust me, soldering a small piece of wire through all vias to connect traces on opposite sides is quite a tedious task!
On the other side, if you are in a hurry you can built your own PCB in manner of hours and don't wait for manufacturing/shipping times.

Doing PCB from myself also allowed me to appreciate the technology and the work that is usually hidden when ordering PCB from a professional manufacturer. Learning, even at small scale, to deal with process and technology limitations (basically, limitation of my router in my specific case)  to me has been quite beneficial.

      image  

My homemade milling machine to mill PCBs.

   image

Milled PCB example. Soldered resistors are 0402!

Professionally made PCBs

I have to admit that, as hobbist, I've never ordered PCBs, at least yet! My experience here is "limited" to what I've seen/used at work.
Premade PCBs are very handy and easy to handle/assemble compared to all previously mentioned method, no surprise here. At home I start thinking about profesionally made PCBs when my manufacturing capabilities are not up to the requirements. In the end, to me these are just a tool as every other technique described above. I use it if I really need it, and I use the tool that better fit my requirements time to time.

image
PCB work in progress Slight smile

Other experiences

Altough I've not used extensively, in the past I've done a couple of circuits using wire wrap, mainly at school. Probably back then the main prototiping technique in the lab was simply bodging all toghether hoping for the best Slight smile

All these "techniques" into one project

The project I'm working on (BLDC sensorless controller for an RC car) has seen some up and down, but thank to its longevity I've used all described techniques to develop prototypes and to learn along the way.

As a final touch, a video of a drone motor spinning and starting up without hesitations (common in sensorless systems) and another comparison video with my actual RC car (which is not bad at all!).
Final boards hopefully coming soon!

                                                                      

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Video #1: start up procedure on my RC car. The motor (sensorless) has a small hesitation.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


Video #2: motor start up with my prototype.

  • Sign in to reply
  • strb
    strb over 4 years ago in reply to shabaz

    Thank you!

    I have still to completely figure out how to organize all my notes. At the moment I have an envelope were I put just "random stuff" that I've made in the past. With this project, I'm dedicating a plastic envelope to collect all these sheets (which are numbered so I don't mess them up too much).

    At the moment I'm trying different approaches to see what it fit the best for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • strb
    strb over 4 years ago in reply to scottiebabe

    How did I miss that Sweat smile, thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Great blog! 

    I do the same in terms of block diagrams/sketches, I write lots of notes, although untidily, and often in a book if I can, otherwise I lose the notes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago

    Nice work! You may want to add the /tags/circuitprototypingch tag to your blog post so it gets listed on the projects page :)