Project14
  • Challenges & Projects
  • More
Project14
Forum 12VDC UPS Project
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 201 subscribers
  • Views 279 views
  • Users 0 members are here
  • solid state
  • UOS
Related

12VDC UPS Project

Atalantia
Atalantia 3 days ago

Hello People,

I try to outline a 12V UPS for my router. The commercial things I see are either to complicate, means have to much functions or they use a relay. I want to build a solid state switch that is faster than a relay. I have a first sketch. What do you think thats the right direction?

The battery has her own BMS it's not in the circuit here. The comparator is the watchdog who activates the switch in case of a power outage. There are a few diodes to prevent return current. A few resistor to adjust the components margins. R4 is a trimm-pot. Works as a pull-down resistor and adjust the threshold for the comparator.

PS: I know. The input voltage has to be higher than 12V. 

image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 3 days ago +3
    The comparator and switch are not really doing anything useful. Two diodes will do the business quite easily. Both cathodes to the output, one anode to the 12V DC in and one to the battery. It is…
  • geralds
    geralds 3 days ago in reply to Atalantia +3
    Hi look here, an idea: This is a very simple "UPV". The switching time is not the big problem if you make a buffer (Elko-accu) during toggling the relay. It's just an idea.
  • dang74
    dang74 3 days ago +2
    I think you will need second resistor connected to R1 to form a voltage divider. Otherwise I think your comparator will always select the battery. The comparator should also have a bypass capacitor connected…
Parents
  • dang74
    dang74 3 days ago

    I think you will need second resistor connected to R1 to form a voltage divider.  Otherwise I think your comparator will always select the battery.  The comparator should also have a bypass capacitor connected to its supply pin.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dang74
    dang74 3 days ago

    I think you will need second resistor connected to R1 to form a voltage divider.  Otherwise I think your comparator will always select the battery.  The comparator should also have a bypass capacitor connected to its supply pin.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • JWx
    JWx 3 days ago in reply to dang74

    I think there should be also some current limiting during battery charging - now, when battery voltage is < (12V - Vd4), it would be charged through D4 with possibly big current (even creating fire hazard in case of - for example - battery cell shortage and powerful PSU), but maybe BMS would protect against it?