Geeky Gadgets
  • Challenges & Projects
  • Project14
  • Geeky Gadgets
  • More
  • Cancel
Geeky Gadgets
Blog Geeked Out Business Cards
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Geeky Gadgets to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 12 Jun 2017 3:15 AM Date Created
  • Views 2558 views
  • Likes 13 likes
  • Comments 9 comments
  • doug wong
  • geeky gadgets
  • project 14
  • ggadgetsch
Related
Recommended

Geeked Out Business Cards

dougw
dougw
12 Jun 2017

I have made a lot of unique business card holders over the years, but I always wanted to make one that could automatically dispense cards.

It sounds pretty straight forward, but I know that to make a reliable and simple machine that can do this is not an easy task and there are several risks that turn it into more of a research project than a sure-fire design project.

The Project14 Geeky Gadget is a good opportunity to see what can be accomplished, since there are no product sponsors counting on a successful project.

So this project is dramatically different from my usual projects, where I do enough up-front homework to ensure the resulting design will work on the first try.

I expect it will be a meandering narrative of tests and discussion of what works or doesn't work - it might provide insight into the crazy tangents my mind is capable of, but I will probably sensor some of that.

There is a master plan which involves quite a lot of work, but I don't want to build up expectations and pressure to deliver, so the plot will thicken as progress is made.

It is not set up to stick rigidly to the Project14 schedule - that is just an excuse to work on it - if it works by the deadline - great, if it doesn't work by then - still great.

I use low cost components which equals long delivery, so missteps will slow it down significantly (already happening).

This initial part of the blog will cover some of the issues with motorized ejection of cards.

The debate over whether to eject the top card or the bottom card is still not settled.

Ejecting the top card means the stack needs to be spring loaded or motorized which adds to complexity.

Ejecting the bottom card allows gravity feed, but the force will change as the stack shrinks.

In both cases there is a problem of how to eject only one card. Any restraint or pushing lip that acts on the edge of a card needs to be thinner than a card, but cards can easily be bent by much more than one card thickness.

If a friction wheel is used for propulsion, ensuring a constant amount of friction has many problems. Both gravity and springs provide a different force depending on stack size.

There needs to be force on the card to generate enough friction to move it, and the friction with the wheel needs to be greater than the friction between cards.

The wheel cannot be flush with the surface or it won't contact the card, but how to prevent cards from warping around the wheel and still only feed one at a time?

If there is a funnel for the ejecting card to ensure it doesn't get caught on a lip, how to ensure multiple cards don't get jammed in the funnel?

These are the kinds of thoughts and questions I have running around in my head - each one leads to a whole series of tangential possibilities.

I decided to start with a simple gravity feed hopper and single drive motor to see if it would work.

My design calls for a small motor (required by the mysterious master plan), so I ordered a tiny flat motor when Geeky Gadget was announced - it looks like one I've seen in old slot cars. But there were no specs.

When it arrived a week ago, I got to measure it and print off a card-handling hopper.

The following video shows the best results I could get with this prototype.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The simple system worked after a fashion, but I want something much better.

I learned that I wanted slower motors with more torque and the feed system needs a lot of thought to improve its performance, so some really small gearmotors are on order but again - no specs.

I think I will try a 2 stage ejector - the first motor just moves the bottom card into the "breach" where I can control the friction and ejection speed because the second ejection motor only has to deal with one card.

The hopper "nozzle" will be redesigned to only have critical tolerance at one point where card selection will be controlled. Everywhere else the system will use smooth guides. I may be able to prove this concept with another bigger gearmotor I already have.

To be continued......

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago in reply to jw0752 +3
    My lab has only ever been seen by a handful of people in the world - maybe less than 10. And none of the ones who have seen it have a clue what they are looking at, except my brother who has 2 engineering…
  • jw0752
    jw0752 over 9 years ago in reply to dougw +2
    "Well organized" is a very subjective thing. If you can find what you want when you want it then it is organized. I have been told that I border on eccentric in my pursuit of order. Incidentally, I suspect…
  • mcb1
    mcb1 over 9 years ago +2
    Great Geeky Gadget. I wonder if you used the rollers from a commercial printer you might be able to handle the friction and grip a little better (once you gear it down) If I recall some of the paper feeders…
Parents
  • DAB
    DAB over 9 years ago

    Nice build.

     

    Not sure of its use.  I prefer the old fashioned hand off so you can look people in the eyes to assess if they are just going to toss them after you leave.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to DAB

    In some circles formally presenting a business card is mandatory.

    In some it would be considered impolite to flick a business card down a long conference table.

    I figure some would forgive it if was a novelty machine handing out business cards.

    But it is more about breaking the ice - something other than business to kick off a meeting.

    My mini seismometer card holder actually has people wanting to order one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago in reply to dougw

    I agree, sometimes you just need something to break the ice.

     

    Plus watching their jaws drop would bring a smile to my face. image

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago in reply to dougw

    I agree, sometimes you just need something to break the ice.

     

    Plus watching their jaws drop would bring a smile to my face. image

     

    DAB