Geeky Gadgets
  • Challenges & Projects
  • Project14
  • Geeky Gadgets
  • More
  • Cancel
Geeky Gadgets
Blog Geeky Dalek Project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Geeky Gadgets to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lahey
  • Date Created: 19 May 2017 6:23 AM Date Created
  • Views 2467 views
  • Likes 4 likes
  • Comments 12 comments
  • ggadgetsch
Related
Recommended

Geeky Dalek Project

lahey
lahey
19 May 2017

My geeky idea is a Dalek with object recognition and different behaviors based on what it sees. I have recently acquired two 12'' rc daleks, one functioning and one for spares, and the motor section is actually well built. I will use a RPI3 for the image recognition and an Arduino for the movement and obstacle avoidance, so as not to encumber the RPI too much. Trying to find a viable way to turn an optical mouse into an odometer for motion tracking. Any tips VERY welcome.

 

image

  • Sign in to reply

Top Comments

  • lahey
    lahey over 9 years ago in reply to balearicdynamics +3
    Ciao Enrico, The imaging and object recognition will already use up a lot of processor time for the PI, and the camera and head servos will drain a lot of power. I decided to set up an Arduino so it will…
  • lahey
    lahey over 9 years ago +3
    Update: The motor section is taking shape, what's missing is a gyro to calculate rotation and probably a mouse optical sensor to calculate movement. I hope I have enough pins on the Arduino for all these…
  • lahey
    lahey over 9 years ago in reply to DAB +2
    Hi DAB, yes, the speaker is already in place and I have a whole range of phrases the Dalek will say, based on what it "sees" i have managed to get to get my hands on a couple of these sensors. Thy basically…
Parents
  • DAB
    DAB over 9 years ago

    Hi Ian,

     

    Interesting project.

    As I recall, the optical mouse uses a laser diode and a simple imaging sensor.

    If you get one of the laptop mice, you should be able to strip out the sensor and processing chips, remount it in the Dalek base to get X-Y movement info over the USB port.

    A wireless mouse would get you position information directly to the RPi, assuming all of the pieces can fit inside the base.

     

    You do realize that you need to add a speaker so that they can blast out "Terminate" when anyone nears the device.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lahey
    lahey over 9 years ago in reply to DAB

    Hi DAB,

     

    yes, the speaker is already in place and I have a whole range of phrases the Dalek will say, based on what it "sees"

     

    i have managed to get to get my hands on a couple of these sensors. Thy basically are 16X16 monochrome cameras which also output the movement delta.  Working on the wiring.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • lahey
    lahey over 9 years ago in reply to DAB

    Hi DAB,

     

    yes, the speaker is already in place and I have a whole range of phrases the Dalek will say, based on what it "sees"

     

    i have managed to get to get my hands on a couple of these sensors. Thy basically are 16X16 monochrome cameras which also output the movement delta.  Working on the wiring.