Going Green
  • Challenges & Projects
  • Project14
  • Going Green
  • More
  • Cancel
Going Green
Blog Chicken Coop Livestream
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Going Green to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 30 Jul 2017 8:17 PM Date Created
  • Views 4664 views
  • Likes 15 likes
  • Comments 17 comments
  • rpiintermediate
  • going green
  • gogreench
  • iot_projects
  • pi noir
  • solar power
  • chicken coop
  • solarpwrdevicesch
  • pi zero
Related
Recommended

Chicken Coop Livestream

fvan
fvan
30 Jul 2017

I'd hate to let the Going Green  theme go to waste without multiple entries, so I created a (solar powered) video streamer for my chicken coop as a little weekend project image

 

  • Hardware
  • Software
  • Testing
    • Power Saving
    • Infrared

 

Hardware

 

The idea is to use a Pi Zero with Pi NoIR and a set of IR LEDs which can be enabled/disabled on demand. An external wifi dongle ensures better connectivity from the back of the garden. Using a solar panel and battery pack, the circuit can remain powered and automatically charge during the day.

 

The hardware required for this project is:

 

* Solar panel with charging circuit and battery

* Raspberry Pi Zero

* Wifi dongle for extra range

* Raspberry Pi NoIR Camera v2Raspberry Pi NoIR Camera v2

* Official Pi Zero case with camera lid

* Pi-Supply Bright Pi

 

The gallery below serves as a build log for this project image

 

{gallery} My Gallery Title

image

image

image

image

image

image

image

image

image
image

 

Software

 

On the software side of the project, I went for the all-in solution provided by MotionEyeOS, a streaming OS compatible with the Raspberry Pi.

 

After downloading the software image for my device, I flashed it onto an SD card using Etcher. I copied my "wpa_supplicant.conf" file to the SD card, before ejecting and inserting it in the Pi.

Upon first boot, the Pi automatically connected to the wireless network and set up the camera. I honestly didn't expect it to be this easy image

 

Browsing to the web interface, various options are available to configure frame rate, resolution, camera name, etc ...

image

 

MotionEye also allows the creation of "action buttons". Just what I need in order to enable/disable the BrightPi's IR LEDs.

 

In the "/data/etc" folder, I created two files called "light_on_1" and "light_off_1".

 

[root@meye-1d01a2ec etc]# pwd
/data/etc

 

[root@meye-1d01a2ec etc]# ls -l light_o*
-rwxrwxrwx    1 root     root            83 Jul 29 20:02 light_off_1*
-rwxrwxrwx    1 root     root            83 Jul 29 20:02 light_on_1*

 

Inside those files, a short bit of code to control the Bright Pi via I2C.

 

[root@meye-1d01a2ec etc]# cat light_off_1
#!/usr/bin/env python

from os import system

system("i2cset -y 1 0x70 0x00 0x00")

 

[root@meye-1d01a2ec etc]# cat light_on_1
#!/usr/bin/env python

from os import system

system("i2cset -y 1 0x70 0x00 0xa5")

 

MotionEye detects these scripts, and adds the button overlays to the video streams.

image

 

Testing

 

Long duration testing will have to determine if the 10W solar panel is sufficient to keep the battery charged, but some measures to lower the power consumption can already be taken.

 

Power Saving

 

Every bit helps when using battery powered applications. And though the Pi Zero isn't the most efficient choice, some tricks can be applied to lower its power consumption.

 

The first easy change, is to disable the onboard LED by editing the "/boot/config.txt" file and appending the following:

 

# Disable the ACT LED on the Pi Zero.
dtparam=act_led_trigger=none
dtparam=act_led_activelow=on

 

The same can be done for the camera's LED, though that option exists within MotionEye, making it even easier:

image

 

As the Pi is running without monitor attached, the HDMI output can be disabled. This is done by adding a cronjob using "crontab -e" to execute the command upon reboot:

 

# Disable HDMI
@reboot /usr/bin/tvservice -o

 

Disabling any services that are not used may help as well. By default, MotionEye, enables things like Samba and FTP. These can be disabled via the GUI:

image

It's worth going through all options and disabling anything you don't require. The streaming settings can be adapted as well, as the camera doesn't necessarily need to stream all the time, or at full resolution.

 

Infrared

 

I also performed a test in total darkness, with the IR LEDs. They aren't super powerful, but it's enough to keep an eye on the chickens image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • fvan
    fvan over 9 years ago in reply to fvan +2
    I've been working on the maths for this, but could use some assistance with the theoretical side until I get actual measurements. I'm working with the components I have at hand, trying to determine if…
  • e14phil
    e14phil over 9 years ago +1
    fvan , What great timing! I was JUST about to begin build of a solar powered IR motion cam. My parents have a hedgehog house in their back garden and were looking to monitor it. You have done all the leg…
  • DAB
    DAB over 9 years ago +1
    You could use this same setup in a number of nocturnal animal monitoring projects. Well done. DAB
Parents
  • idanre1
    idanre1 over 9 years ago

    Great project!

    I actually Interested doing such a thing in my roof.

    I suffer from pigeons and I want to monitor the roof and using some computer vision - motion detector, know when they party in my roof.

    And when they come - auto open a water hose to scare them out to someplace else.

     

    +1

     

    Idan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago in reply to idanre1

    Hi Idan,

     

    You could implement the Time Of Flight type processing I discussed with the TI PIR sensor.

     

    You should be able to detect movement and possible get a rough count of occupants based upon the frequency components.

     

     

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • idanre1
    idanre1 over 9 years ago in reply to DAB

    Hi DAB

    Could you share some link with more info?

     

    regards

    Idan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • idanre1
    idanre1 over 9 years ago in reply to DAB

    Hi DAB

    Could you share some link with more info?

     

    regards

    Idan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 9 years ago in reply to idanre1

    Hi Idan,

     

    Start with TI document TIDUCV3A dated February 2017 and go from there.

     

    It is an interesting approach for passive sensors.

     

     

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • idanre1
    idanre1 over 9 years ago in reply to DAB

    Hi

    I must say the design in the application note is pretty high quiality.

    The documant explains allot and very inspiring.

     

    I will take it in mind when designing my pegion scarecrow.

     

    Thanks!

    Idan