Hack the Holidays
  • Challenges & Projects
  • Project14
  • Hack the Holidays
  • More
  • Cancel
Hack the Holidays
Hack the Holidays Blog Musical LED Christmas Tree
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hack the Holidays to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 31 Dec 2022 4:23 AM Date Created
  • Views 1922 views
  • Likes 12 likes
  • Comments 3 comments
  • LED Xmas Tree
  • Soldering Kit
  • musical
  • hacktheholidaysch
  • hack the holidays
Related
Recommended

Musical LED Christmas Tree

ntewinkel
ntewinkel
31 Dec 2022
Musical LED Christmas Tree

The holidays are often the only time of year that I have time to work on projects - cold, rainy (or snowy!) weather with long dark nights are perfect for indoor techy projects!

This year was a better in terms of being able to create more projects throughout the year, but the holiday challenge has pretty much become a tradition for me now, so I obviously had to build something festive again this year! Smiley

Several years ago I bought a handful of soldering practice kits - this was back when shipping was super cheap, and the kits were also super cheap. Shipping was still the kind that required patience, so often by the time the kits arrived I'd have forgotten why I bought them ShrugSmile cat
I like these kits - they're a little bit like building a puzzle.

Among those kits were several LED Christmas trees - nice and colourful, and easy to assemble. They're also easy to power - I can light the whole tree with a simple 3v button battery, or with power from a little dev board.

LED xmas tree

I also at one point bought a few kits that flash LEDs when sound is heard. I think I actually bought them because I needed the little connectors for some other project. And then they were the wrong style of connector Laughing 

soldering kit - flash to music

For this one I only soldered on one LED for testing, but later I cut one leg of that LED so that the tree would light more brightly.
For the power connector I just added some patch wires, and in one of the LED positions I added a connector so I could power the tree from it there.

flash to music board

I also had this music box lying around - it plays a little bit of Christmas music that reminds me of when I was little, so I kept it. I think it had chocolates in it at one point, which left a nice big open area in which to place the electronic parts.

music box

At first I had planned to use a Pi Pico to detect sound with an electret mic, or with a piezo buzzer, but I was not able to get that circuit working at all! Luckily I still had that little sound flashing soldering kit that I had randomly bought years ago!

So I soldered things up and connected it to the tree.

musical tree connectedmusical tree parts

And after putting it all together:

musical tree ready

I notice now that things are a little bit crooked there. ah well, I shall once again have to embrace the imperfection Stuck out tongue closed eyes

It turned out kind of cool though:

Tree in the dark

But you need the video to fully appreciate it:
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
Happy Holidays, everyone!

And Happy Hacking the Holidays!

-Nico

  • Sign in to reply
  • ntewinkel
    ntewinkel over 3 years ago in reply to beacon_dave

    That's a good idea. I thought of having it come out through the lid, but couldn't quite visualize a neat way to do it.

    I probably should have assembled one of the other yet-unassembled tree kits and built it without the base, and then hot-glued it to the music box lid, which already has a slot through it for the ribbon where the wires could go through. But I was running out of time, so I decided to finish it imperfectly instead of not finishing it at all Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago

    Works well.

    You could perhaps try 3D printing a new lid for the music box, with slots in the top of it for the PCB trunk of the tree to pass through.

    Perhaps use the general profile of the original lid to keep the original styling and adjust where necessary. Might need to round off the corners of the tree base PCB a little.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DeltaPi
    DeltaPi over 3 years ago

    Looks nice.