Hack the Holidays
  • Challenges & Projects
  • Project14
  • Hack the Holidays
  • More
  • Cancel
Hack the Holidays
Hack the Holidays Forum A simple game on the RPI Pico
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hack the Holidays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 39 subscribers
  • Views 5728 views
  • Users 0 members are here
Related

A simple game on the RPI Pico

scottiebabe
scottiebabe over 3 years ago

Pimoroni have recently included support for basic 8x8 pixel sprites in micropython https://github.com/pimoroni/pimoroni-pico/tree/55821d2896ac12732c4e84142ba1fb76d4382dc5/micropython/modules/picographics#sprites 

So, I would like to try and make a simple holiday game on a RPI Pico.

I am thinking of something along the lines of:

image

Where the objective of the game is to avoid airborne objects while dropping presents into chimneys.

Two buttons for Rudolf up/down. Then a third button for santa to drop a present.

I got this Pimoroni example to run with my Pico Display: https://github.com/pimoroni/pimoroni-pico/blob/main/micropython/examples/tufty2040/awesome_game.py 

So, I can use that as a starting point. I'm still not sure how I will handle a scrolling scene.

I'll post a quick video of the example code running later.

Edit:

The 8-bit color gives such a cool retro vibe, I love it!

image

A *Very* early proof of concept:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Why can't I comment? ... lol

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +6
    What a cute idea! Maybe start with a static screen where Santa goes back and forth dropping presents into a static set of chimneys. The challenge element could be "smoke" coming out of the chimney means…
  • beacon_dave
    beacon_dave over 3 years ago +5
    You could perhaps drop baubles onto the Xmas trees causing them to light up/decorate. Brussel sprouts would make good airborne objects to avoid. Perhaps some carrots for the reindeer to collect and mince…
  • dougw
    dougw over 3 years ago in reply to scottiebabe +5
    irfanview You can select the target number of pixels, edit each pixel, select the color depth, select the file format, etc.
Parents
  • ntewinkel
    ntewinkel over 3 years ago

    That’s really cool!

    This would be a great entry for the Hack The Holidays competition!

    It’s amazing how much power is available on that little board to give you those possibilities.

     There’s a Flappy Bird for the Pico, but it looks like it’s in C. But it might help with the scrolling background part?

    https://github.com/andreban/pico-bird

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to ntewinkel

    Thanks :) I think its a fun festive idea for a hackathon. Hopefully it turns out okay!
    It really blows me away that this is a microcontroller running python!
    Flappy Bird for the Pico, that's amazing!

    Re: background. I still have to decide if I want to draw the background as a small number of "sprites" or a full 240x135 jpeg image.
    Right now, I am using a jpeg image as the background. I am just not sure yet if I can copy x from imgA and y from imgB in a fast way in micropython. I may end up having to write a fast routine in assembly. If microbython had better indexing and slicing that could would work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 3 years ago in reply to ntewinkel

    Thanks :) I think its a fun festive idea for a hackathon. Hopefully it turns out okay!
    It really blows me away that this is a microcontroller running python!
    Flappy Bird for the Pico, that's amazing!

    Re: background. I still have to decide if I want to draw the background as a small number of "sprites" or a full 240x135 jpeg image.
    Right now, I am using a jpeg image as the background. I am just not sure yet if I can copy x from imgA and y from imgB in a fast way in micropython. I may end up having to write a fast routine in assembly. If microbython had better indexing and slicing that could would work.