Hack the Holidays
  • Challenges & Projects
  • Project14
  • Hack the Holidays
  • More
  • Cancel
Hack the Holidays
Hack the Holidays Forum Have you ever made a 9V battery topper circuit?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hack the Holidays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 38 subscribers
  • Views 16043 views
  • Users 0 members are here
Related

Have you ever made a 9V battery topper circuit?

scottiebabe
scottiebabe over 3 years ago

I never have!

I wanted to measure the optical flicker of some new decorative lights that are advertised as being "constant lit".

Naturally, I thought I would just use a reverse biased photodiode and current sense resistor on top of a 9V battery. Then combined with my handheld portable scopemeter I could measure the brightness of these LEDs versus time.

I sacrificed a new 9V battery snap for the endeavor. Perhaps one could salvage the snaps of an expired 9V battery.

image

So far things look okay. Time will tell if I end up breaking the 9V snaps off... lol

My First 9V Topper Circuit

image

If I make a second topper circuit I could make a much more luxurious version of this circuit which includes a dual op-amp in a DIP package.

Testing in the Garden

Finally I get to the point of why I built the circuit in the first place! I was curious to see if these product claims were even remotely true:

image

They claim to be shimmer-free:

image

At first glance there dosen't appear any addition circuitry in the string lights aside from the LEDs themselves. The plugs look ordinary

image

(This isn't a blog post or content for competition so excuse the blurry photos for now :) )

Are the LEDs constant-lit?

image

No, but interestingly they LEDs are active on both halves of a line cycle:

image

I am still think about this one, it isn't obvious there is a bridge rectifier nestled away in the strand or plug. Perhaps each "LED" has two LEDs in opposing polarities?

Old skool LED Christmas lights are only active one half of the 60 Hz line cycle

image

Interesting...

  • Sign in to reply
  • Cancel

Top Replies

  • ralphjy
    ralphjy over 3 years ago +5
    Not sure I've got this right, but if you just want to add contacts to the top of the battery - Digikey sells some contacts mounted to a fibre plate that can be mounted on a PCB or used separately. Comes…
  • scottiebabe
    scottiebabe over 3 years ago +5
    O hello there little bond wire I used a TEFD4300 photodiode because I had them. If you were interested in measuring the flicker of a larger light source like an E26 lamp I think a small solar panel…
  • ralphjy
    ralphjy over 3 years ago +5
    Interesting discovery of "full wave" performance of the string lights.. I think you have inspired me to build some of my own 9V "toppers" using the Digikey contacts and 3D printed housings. Would be…
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago in reply to scottiebabe

    I use them for 5V circuits with rechargeables. But they also come as 6 AA holders.

     image

    PS: How do I insert a nice shopping link, like @dougw is able to do?

    Maybe this?

    6x AA

    Looks different in the editor. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 3 years ago

    Interesting discovery of "full wave" performance of the string lights..

    I think you have inspired me to build some of my own 9V "toppers" using the Digikey contacts and 3D printed housings.  Would be nice to have interchangeable modules for various functions.

    I have a 6 LED 9V flashlight that I use for traveling (has a 2 LED and 6 LED mode).  Getting a little dim, but I realized the expiration date was Mar 2016 Smile.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to ralphjy

    That is a cute topper...Thumbsup tone3

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to ralphjy

    Thanks, I'm still looking into how the full wave magic happens :) 

    This is wonderful! Its a fun low cost (I think I had 99 cents invested) and low time effort project theme. And its always fun to try new things Slight smile.

    That is one fancy topper!

    I might try making a second topper which is a noise generator with an SMA output.

    Not quite a topper but when I was a child I spent way too many hours using one of these:

    image

    For all I know my parents were damaging bulbs as a way to keep me occupied lol

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago

    Very interesting!

    I guess a dual led setup would be a cheap way to reduce flicker from 60hz to 120hz. The spikes make it seem like there’s no buffering.

    I’m curious to see what you find out Smiley 

    Also interesting for me to see how you used an oscilloscope in a direct useful application like this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<