Holiday Special 20
  • Challenges & Projects
  • Project14
  • Holiday Special 20
  • More
  • Cancel
Holiday Special 20
Blog Dog Shaped Arduinos. What could go wrong?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Holiday Special 20 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hugohu
  • Date Created: 10 Jan 2021 7:34 PM Date Created
  • Views 6996 views
  • Likes 19 likes
  • Comments 36 comments
  • holidayspecial20ch
Related
Recommended

Dog Shaped Arduinos. What could go wrong?

hugohu
hugohu
10 Jan 2021

"What brings you joy"


Well, certainly, I'd say dogs, since they're one of my favorite species.

In specific, corgis.

 

image

image

image

image

 

You gotta admit, they have great smiles.

 

image

 

Oh no I published it.

 

*smacks my head*

 

Oh well anyway/

 

"open-ended holiday project competition that challenges you to make a project that reflects what the holidays mean to you"

 

I am, indeed, stretching it with... a bundle of corgi joy.

 

Sorry, Tariq.

 

(Maybe dont disqualify me? Thanks hehe)

 

Well, I designed a small 328P based board, because I was not really happy about 2020 and wanted a furball Arduino that was in 0 ways space efficient.

 

image

 

Well, hehehehehehe

 

It uses a ATmega328P, clocked at 16MHz, onboard USB bridge, yada yada, NANO pinout, yada yada.

 

The point of a project14 is to document your process-

 

Let me do that.

 

I was discussing which arduino they should pick to a beginner, and they were talking about their arduino UNO that just arrived and how their corgi loves to sit on his lap while he works with the UNO.

 

Well, hearing "UNO" and "corgi" gave me the exceptionally bad idea of a corgi-shaped UNO.

 

There's a RX TX LED because it doesn't add much to BOM and I said "why not". It uses a USB-B THT connector, because I actually have a 10% accuracy rate of soldering microUSB.

 

There's a CH340C for USB bridge.

 

I made this design recently(a few weeks ago, early December)

 

I had the PCBs printed and they're coming tomorrow!

 

I'll update with more info... hopefully it works.

 

Oh right. I forgot. "What could go wrong?"
Well, the unique shape makes it... more expensive for manufacturing, remarkably inefficient design. What else could go wrong? My subpar SMD practice. I mean, I did get better at it recently and can go up to 0402?

 

With a SP25?

 

image

 

I would be concerned about signal integrity and that stuff. Wait- did I use 0.5mm for power and 0.3 for signal instead of 0.254 for everything?

 

Here's a bit into an in depth view of the design.

 

Please excuse my ignorance of using EasyEDA, I've just recently begun the transition to KiCAD. image. Libraries are a bit wonky but I'm starting to get the hang of it. Enough of the KiCAD mumbo jumbo.

 

image

 

This is the 328P:

The chip is in TQFP for easy hand soldering(TQFP32 has larger pin pitching too). I've soldered QFN but I'm not the most reliable at such, since it's hand soldering with an iron.

 

As usual, the usual pin net flags, a Reset Button, a 16MHz SMD crystal and it's 22pF capacitors, since I didn't use the packaged ones with 22pF built in.

 

Ground and more netflags-

 

5V LED for power, etc etc etc etc etc etc and a D13 standard LED.

 

Nothing special at all.

 

image

This is the CH340 USB Serial bridge circuit- FTDI is relatively pricey and these are close to 50 cents. I also could have used a Silicon labs CP series chip but its QFN and harder to use, and more expensive. I'm planning to give these as gifts so having a high BOM cost doesn't help.

 

I also chose a CH340C which is more expensive than a G, but has a built in crystal so I do not need an external 12MHz one. Ultimately I screwed up and bought 15 of BOTH CH340C and CH 340G, where I don't need the G. Yeah, five dollars wasted and some chips I don't need. Let me know if you happen to need any CH340G image Shipping included but the crystals are not image

 

image

Following the ICSP and NANO pinout, these are the net flags. Why use NANO? Not so much HATs on them, but it's a relatively compact form factor and I didn't want to do battery charging for Feather pinout.

 

image

This is the part for 7-12V input down to 5V, using an AMS1117, because those are a bit cheaper. Yeah.

 

(If I'm sounding like I'm trying to use a ton of not so great parts to reduce BOM costs, I probably am hehehehe)

 

image

Lastly, this is the USB.

 

Nothing special, just a barrier diode.

 

"Where's 3.3V regulator? No MCP1700 or something?"

Nope... CH340 has 3.3V regs. Fancy, right?

 

image

 

image

 

The power tests look good(I need to clean off the flux a bit)

 

However, I am having some difficulty flashing on the bootloader(as you can see that's what I'm trying to do)

 

I also flipped the ICSP header upsidedown image

 

(The eye is connected to D13)

 

I'll be installing the CH340 driver later today. If that assists with flashing bootloader.

 

A friend informed me I'd need an oscilloscope to probe RX and TX.

 

Ah. I really need to buy one now LOL

 

(or maybe win image, but the chances of that aren't too high. I mean... WOOF)

 

USB WORKS

USB

WORKS

 

You can see my ugly fix in the image below:

image

It consists of a 0.1uF(100nF) cap from 3.3 to GND.

 

Call me stupid, and I am stupid, but I actually forgot.

 

:')

 

But they do work.

 

image

 

image

 

(Also, thanks for tweeting this James image)

Well, it's the 13th, the deadline is the 15th.

 

I managed to get it to work.

 

Hehehehe.

 

Mission accomplished!

 

Also, if I didn't previously note that the D13 LED is on the eyes...

here's a small script to make the corgi "blink" it's eyes...

 

void setup() {
  pinMode(LED_BUILTIN, OUTPUT);
}

void loop() {
  digitalWrite(LED_BUILTIN, HIGH);   
  delay(6000);                      
  digitalWrite(LED_BUILTIN, LOW);
  delay(300);            
}

 

You guys can probably write this in your sleep but code samples assist the project's standing inthe contest.

 

hehe.

 

Well, that's probably all.

 

If I can make a programming rig for this, I'll share it too, if I can make it work before the deadline.

 

Oh yeah, and btw:

 

void setup() {
  pinMode(LED_BUILTIN, OUTPUT);
  Serial.begin(9600);
}


void loop() {
  digitalWrite(LED_BUILTIN, HIGH);   
  delay(6000);                     
  Serial.println("Bark bark!");
  digitalWrite(LED_BUILTIN, LOW);   
  delay(300);                    
  Serial.println("WOOOOOOOF");
}

 

A very simple but corgi blinky sketch image

 

(The eye is supposed to blink every 6 seconds )

 

I would like to revisit the topic of "what could go wrong".

 

EVERYTHING.

 

It works, definitely, there are some issues that remain confusing-

 

A portion of boards(currently 1/3) are not able to be flashed.

 

I used the right chip, no solder bridges, everything checks out, but...

 

avrdude: Yikes!  Invalid device signature.

         Double check connections and try again, or use -F to override

         this check.

 

 

Error while burning bootloader.

 

Hello, I'm using a genuine ATmega328P, I know the connection works because I made a frickin' programming rig(more on this later), and...

 

Right now, 2 boards are not working image

 

Time to do a redesign.

 

A bit on my programming rig: it's just the 6 jumper wires in ICSP format and taped together image

 

image

Board without flux image

  • Sign in to reply

Top Comments

  • dwinhold
    dwinhold over 5 years ago +6
    So, wouldn't the Arduino be called a "Corgino"? I love it by the way!! Dale
  • hugohu
    hugohu over 5 years ago in reply to baldengineer +5
    CH340 drivers are really painful sometimes. Yeah, at least I mean SI Labs ones are more straightforward. CH340: you plug it in, sometimes it works, sometimes it doesn't. SI labs: if it's not detected,…
  • ralphjy
    ralphjy over 5 years ago in reply to hugohu +4
    Sorry to hear the USB isn't working. Hope you've figured it out by now.... Forgot to send you pictures of the granddog. I took a couple this morning. On top of the couch waiting for the Oregon rain to…
Parents
  • baldengineer
    baldengineer over 5 years ago

    You got me with the title! What an awesome idea.

     

    Super cute too.

     

    By the way, I totally agree with your comment on the SI Labs chip. I wish it came in something other than QFN. Even with my SARO (super advanced reflow oven), I cannot reliably solder them. Which is a shame, because I have much more success with their drivers than the CH340.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to baldengineer

    Agreed - I have a habit of avoiding anything using CH34x wherever I can because it isn't always reliable at high baud rates either.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 5 years ago in reply to baldengineer

    Agreed - I have a habit of avoiding anything using CH34x wherever I can because it isn't always reliable at high baud rates either.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hugohu
    hugohu over 5 years ago in reply to Gough Lui

    ha, well I don't normally do high baud rate things(I did get a fpga board recently which uses 115220 or something along those lines), but I should try to move to other types. FTDI is more expensive but comes in SOIC...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago in reply to hugohu

    Indeed - 115200bps is a "common" baud rate. In the old days of the 16550A UART, that would have been considered "high" as the 8250 only managed around 19200bps at the best of times.

    In modern times, I've ended up clocking out 921600bps/1M/2Mbps over USB to Serial bridges for that "extra" oomph. In fact, at that rate, the 16MHz AVR chips running Arduino code can't seem to fill their serial buffers quick enough and often it's the processing that's the bottleneck. I know that large flash uploads for ESP8266/ESP32-based boards go comfortably faster if you can do it at 921600bps ... otherwise each upload could take up to 40-seconds or so, but the WinChipHead CH34x-based solutions usually don't manage and have to run something like 460800bps or less for reliability.

     

    FTDI produces quite reliable solutions, but alas, since the "FTDI-gate" issue when they started producing drivers that would brick "clone" FTDI chips which sometimes ended up in legitimate products and unknowing consumer's hands, people started to turn their opinion about using them. SiLabs CP210x solutions became much more popular around that time. Before that, Prolific PL2303-based bridges were the most popular, but the vast number of counterfeits had resulted in lots of unreliability and then Prolific also made the annoying step of causing their drivers to throw a "Code 10" Device Cannot Start error in case it detected a clone chip. This meant that many people had to downgrade their drivers to get some devices with clone chips to operate, but Windows Update had a habit of automatically updating the driver to break things on the next insertion. Prolific really stuck their foot in it when they decided the plain older PL2303-based devices would not operate on Windows 8 or above simply by not providing a driver for it, insisting you needed to upgrade to a newer chip variant (HX or above if I recall correctly). This even means legitimate devices, like my Agilent USB-to-IR adapter for my multimeter will not work on Windows 8 or above - unless I buy their new "orange" Keysight branded one which has the newer 2303 variant inside.

     

    There were other USB-Serial solutions but few were as popular as many of these come from earlier times (i.e. large chips, lots of pins, not very power efficient). Texas Instruments had one which was commonly used in Digi EdgePort devices and was actually part of their USB-Hub chip. Intel had one too which I've seen in an old Belkin USB-RS232 adapter. Right now, I'm still rather partial to the CP2102 - wherever I've found it, it always seems to work just fine even on the cheapest ESP8266-board for about AU$5. Indeed a shame it cannot be as easily soldered.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hugohu
    hugohu over 5 years ago in reply to Gough Lui

    Wow thanks for the history and information dove this was very informational. I do re call them saying that the FTDI chips were very popular and reliable and their drivers were also really great but they’re were counterfeits and then they were also bricked.

    mostly nowadays my three types of chips I would go to use would be the silicon labs ones, CH340 for low cost and low reliability circuit and also there was this a Microchip Technology an Usb bridge that actually comes in dip and among other easy to solder chip packages but I have not used it yet.

    thanks again for the super useful explanation image