IoT: In the Cloud
  • Challenges & Projects
  • Project14
  • IoT: In the Cloud
  • More
  • Cancel
IoT: In the Cloud
Blog Temperature measurement with Arduino MKR WIFI 1010 and Cloud
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join IoT: In the Cloud to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 21 Mar 2019 5:04 PM Date Created
  • Views 6798 views
  • Likes 13 likes
  • Comments 7 comments
  • mkr_1010
  • p14 mkr 1010
  • arduino_iot_cloud
  • iotcloudch
  • arduino mkr1010
  • arduino cloud
  • arduino mkr rs485
Related
Recommended

Temperature measurement with Arduino MKR WIFI 1010 and Cloud

kk99
kk99
21 Mar 2019

image

The basic idea was to create a temperature monitor based on DS18B20 sensors with support for remote access. I have used a kit called AVT-1705 which allows to read data from two DS18B20 sensors via RS485 protocol. As master controller I have used a Arduino WIFI MKR1010 board with MKR485 expansion board. Arduino board is responsible for triggering temperature measurement and reading data. Received data is parsed and send via secure way to Arduino Cloud.

 

Below there is schematic of AVT-1705 kit:

image

We have a Attiny23 MCU which is responsible for reading data from two DS18B20 sensors, and transferring this information via RS485. Each AVT-1705 could has own unique address, so we are able to connect multiple of these modules in parallel.

Module accept following command to start measurement:

Txx[0x0D], where xx is module address.

In response after around 1 second we receive following data:

T00= 12.2"C;T01= 12.2"C[0x0D]

[0x0D] it is "Enter" character in hex.

 

In my project module is powered from six 1.5 V batteries. Lines L_A, L_B and GND are connected to following pins of MKR 485 expansion board: Y, Z, ISO GND. MKR 485 is configured to work in half mode.

 

First step was to configure board to connect to Arduino Cloud via WIFI. Below are images with steps to configure board and information about sensors values.

image

image

image

image

image

image

image

image

image

image

In first steps we need to choose board type, provide board name and enable chipset for secure connection. After that we need to create a new project for temperature measurement. For this project we need to define to properties of fields which will hold data from two sensors. After that we need to go to source code where we could provide information about SSID/password. Now we are able to connect to Arduino Cloud.

 

Below there is diagram for application flow.

image

In main loop in every 10 seconds we are reading temperature from module and update these values in Arduino Cloud. I have used Arduino library for RS485 communication.

Below there is diagram with steps of getTemperature() method.

image

In first step we need to send 4 bytes of command to module to start temperature measurement: 0x54 0x30 0x30 0x0D. After around 1500 ms we are able to read answer with 24 bytes. Then we are able to parse from string with answer and get a values of temperatures for sensors. Answer have following form: T00= 12.3"C;T01= 23.4"C[0xOD].

 

Here are sources:
Sketch

 

Here is video from soldering of AVT-1705 module:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here is short video presentation:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • kk99
    kk99 over 7 years ago +3
    Thank you. I have finished testing of these modules. If there is person interested to test these modules or would like to use them in project (I mean MKR1010, MKR485 and AVT-1705) please contact to me…
  • jamielanger
    jamielanger over 7 years ago +2
    Woohoo ! Great stuff. Remember doing similar stuff years back.
  • dubbie
    dubbie over 7 years ago +2
    kk99, A great project. I remember using similar temperature sensors several years ago when I discovered that not all temperature sensors were analogue and you could obtain a digital value directly from…
Parents
  • kk99
    kk99 over 7 years ago

    Thank you. I have finished testing of these modules. If there is person interested to test these modules or would like to use them in project (I mean MKR1010, MKR485 and AVT-1705) please contact to me via private message. I could send you these modules.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kk99
    kk99 over 7 years ago

    Thank you. I have finished testing of these modules. If there is person interested to test these modules or would like to use them in project (I mean MKR1010, MKR485 and AVT-1705) please contact to me via private message. I could send you these modules.

    • Cancel
    • Vote Up +3 Vote Down