Making Time
  • Challenges & Projects
  • Project14
  • Making Time
  • More
  • Cancel
Making Time
Blog BulbDial - A Tale of a Sundial without the Sun
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Making Time to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wolfgangfriedrich
  • Date Created: 10 Jan 2021 3:52 AM Date Created
  • Views 4676 views
  • Likes 12 likes
  • Comments 15 comments
  • bulbdial
  • makingtimech
  • project14
  • sundial
Related
Recommended

BulbDial - A Tale of a Sundial without the Sun

wolfgangfriedrich
wolfgangfriedrich
10 Jan 2021

When the Making Time competition started, my long-term memory forced my thoughts back into 2011 (sounds like a virtual time machine) when I was prototyping a sundial based on a regular clock movement and some LEDs, called a bulb dial.

History

It all started from a blog post with just a beautiful concept drawing at Ironic Sans (amazing the the blog is still up 13 years later). The idea is simple and elegant. 3 light sources circle a pin and cast shadows in different length for hours, minutes and seconds.

image

The idea of a bulb dial got picked up by several parties and got implemented with boatloads of static LEDs.

First were the geniuses at Mad Evil Scientists. I am not affiliated with them, just want to give them credit where credit is due.

Other implementations can be seen from Solarbotics and Taufeeq.

 

My Bulbdial

image

 

The idea was cooking in my mind for some time until I had enough pieces of the puzzle solved to build a prototype in the spirit of the original concept. I needed a mobile means of power transfer between the different light levels. The solution was multiple disks of decreasing radius for hours/minutes, stacked on top of each other with a shadow casting pin in the center and LEDs of different heights at the edge of each disk. Energy transfer was done through concentric rings of conductive material on the lower level and spring loaded wiper contacts coming down from the upper level. Wires, LEDs and current limiting resistors were the easy part. LEDs had to be narrow beam types, additionally enclosed in heat shrink/tape to reduce stay light all over the place. In the true spirit of prototyping I used wobbly disks of cardboard, copper and aluminium tape and copper EMC finger gaskets.

The clock movement was a continuous type with all arms running smooth in circles and not hopping from one second to the next. Contact was not perfect, so the LEDs went dim/off randomly, so I tried to improve contact resistance with solder and more conductive tape.

In the end, I could prove the concept, but never got to a good enough prototype that I would put on the wall as a working timekeeping piece.

 

Here are some pictures and a video of the (almost) working prototype.

{gallery} My Bulbdial

image

Bulbdial: The working prototype

image

Contacts and the pin: Bottom side with copper slide contacts and the shadow-casting pin.

image

Sliding Contacts: Copper contacts with added solder for better contact making.

image

Contact Rings: The middle disk with contacts and an LED in black heatshrink tubing

image

Contact Rings 2: More contact rings made out of copper tape at the clock base with feed wires

 

This is how it looks like in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Looking into the future

(More virtual time-machining in the positive direction of the time axis.)

When the project moves up high enough on my procrastination to-do list, I want to make real PCBs with trace inductors for wireless energy transfer to get rid of the wiper contacts.

Attached is an article, that implements a very simple wireless energy transfer. The plan is to have a single PCB, that can be populated with components to be either transmitter or receiver and it has to work with 1 tx and 2 rx boards stacked.

 

Cheers to the present and time will tell what the future brings.

Attachments:
image Wireless Power.pdf
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 5 years ago in reply to 14rhb +4
    "...Have you ever heard of Round the Pole (RTP) in the model aircraft world?..." I remember the 1970's Mattel Vertibird very well. Especially having the rotors clip your finger tips at the control console…
  • Fred27
    Fred27 over 5 years ago in reply to beacon_dave +4
    I remember having one of those! A great toy.
  • DAB
    DAB over 5 years ago +4
    Very cool implementation. DAB
Parents
  • 14rhb
    14rhb over 5 years ago

    I like your project a lot, especially your homemade slip-ring.

     

    One suggestion even for this pre-PCB would be to overlap the tape in the same direction, akin to roof tiles: assuming the motor only turns one way the wiper contacts would always drag from high tape (double thickness joint) to low (next section of single tape) and will create less loading to the motor....then again you mention wireless energy transfer is you goal so perhaps not necessary image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago in reply to 14rhb

    Thanks, 14rhb.

    The overlapping step-down is a good idea. I might do that if I resurrect the prototype or build a new one with balsa-wood instead of cardboard.

    Your note triggered another idea, I could add the exposed conductive rings ( reminder to self: no solder mask ) on the PCB and have 2 options not to fail. image Might need to spend some more money for that and go to shiny ENIG plating.

    - W.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 5 years ago in reply to 14rhb

    "...Have you ever heard of Round the Pole (RTP) in the model aircraft world?..."

    I remember the 1970's Mattel Vertibird very well. Especially having the rotors clip your finger tips at the control console when you got a little too close... image

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 5 years ago in reply to beacon_dave

    I remember having one of those! A great toy.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 5 years ago in reply to beacon_dave

    I never had one of those, but I had a friend that did.  We would play with that thing for hours.  Great fun!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 5 years ago in reply to beacon_dave

    Awesome, so such so that I'd like to make one now. I didn't know anyone who got one of these although I do vaguely recall knowing about it, not sure how as my nearest toy shop was about 10 miles away. Some classmates had the Airfix 'Super Flight Deck' which I played with but it wasn't a patch on that Vertibird. Trouble I found with most fun toys in the 70's was buying new batteries - not much money and not many places sold them cheaply !

    image

    [Source: Ebay.co.uk]

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 5 years ago in reply to 14rhb

    I remember the original Flight Deck. It took a while to set up though and parents always complained about it taking over the house so just as you had got it all adjusted and aligned, it was time to start packing it up again...

     

    Yes, the batteries were always an issue with toys in those days. Expensive and guaranteed to leak all over the place.

     

    The original Flight Deck I recall was gravity driven carrier deck landing only though. Looks like the Super Flight Deck may have added a motor to send the plane up to the top and turn it around for a landing run, allowing for single person operation ?  

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 5 years ago in reply to 14rhb

    I remember the original Flight Deck. It took a while to set up though and parents always complained about it taking over the house so just as you had got it all adjusted and aligned, it was time to start packing it up again...

     

    Yes, the batteries were always an issue with toys in those days. Expensive and guaranteed to leak all over the place.

     

    The original Flight Deck I recall was gravity driven carrier deck landing only though. Looks like the Super Flight Deck may have added a motor to send the plane up to the top and turn it around for a landing run, allowing for single person operation ?  

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • 14rhb
    14rhb over 5 years ago in reply to beacon_dave

    You are right about an earlier version, the ones I remember were actually blue rather than yellow and play was fairly basic....I'm thinking circa 1977/8? It shows what happens when I blindly search the internet without doing any research !

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 5 years ago in reply to 14rhb

    "...I'm thinking circa 1977/8?..."

     

    1970's yes.