Merry Boxes & LEDs
  • Challenges & Projects
  • Project14
  • Merry Boxes & LEDs
  • More
  • Cancel
Merry Boxes & LEDs
Blog Santa Incoming Chimney! [SIC]
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Merry Boxes & LEDs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robertwerner
  • Date Created: 16 Dec 2018 2:32 AM Date Created
  • Views 3377 views
  • Likes 11 likes
  • Comments 13 comments
  • merryboxesledsch
  • holidayspecialch
Related
Recommended

Santa Incoming Chimney! [SIC]

robertwerner
robertwerner
16 Dec 2018
image

Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

ESP-Now device for warning of the approach of Santa!  This device has a Master which detects with PIR or a wire break to set a pin low--it is monitored when a TPL 5111 wakes the unit up.  The solar charger keeps the device charged with a battery mounted on the roof.  The receiver device (Slave) constantly monitors for the ESP-Now communication from the master and announces the arrival of St. Nick with a bright cascade of Led's.

  • Sign in to reply

Top Comments

  • robertwerner
    robertwerner over 7 years ago in reply to 14rhb +3
  • robertwerner
    robertwerner over 7 years ago in reply to 14rhb +3
    Hardest part about this project is finding a good piece of bamboo to use--both the receiver and the master are made of bamboo which are cut in the forest. The tubes are cut to their appropriate length…
  • robertwerner
    robertwerner over 7 years ago +3
    https://gist.github.com/rabbitcreek/f578869b636e8de88c5abb2ab0bcc2f1 This is a link to the Slave software
Parents
  • robertwerner
    robertwerner over 7 years ago

    https://gist.github.com/rabbitcreek/1e269bb1eda54761611631f87e360e09

     

    This is a link to the Master software

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to robertwerner

    Hi Robert

     

    What a great project image

     

    Thanks for sharing the code; ESP-Now looks to be very interesting communications method. What sort of range will it operate over?

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robertwerner
    robertwerner over 7 years ago in reply to neilk

    https://www.youtube.com/watch?v=hMOwbNUpDQA&vl=en

    This youtube is great by Spiess for instructing on setting this up.  It is a wonderful interface in that it doesn't require any internet connection at all merely two very cheap microcontrollers talking to each other.  The only difficult thing is setting up the correct addresses and the direction to use them.  The program I set up uses data transfer of an array so you can send much more information than just whether Santa has come.  The project was originally built for a school instruction project for a perpetual rainstick that would send a signal when it rained...the small master being outside perpetually charging itself with the sun and hardly using any power...the slave which is very power dependent connected to 5 volts. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robertwerner
    robertwerner over 7 years ago in reply to neilk

    https://www.youtube.com/watch?v=hMOwbNUpDQA&vl=en

    This youtube is great by Spiess for instructing on setting this up.  It is a wonderful interface in that it doesn't require any internet connection at all merely two very cheap microcontrollers talking to each other.  The only difficult thing is setting up the correct addresses and the direction to use them.  The program I set up uses data transfer of an array so you can send much more information than just whether Santa has come.  The project was originally built for a school instruction project for a perpetual rainstick that would send a signal when it rained...the small master being outside perpetually charging itself with the sun and hardly using any power...the slave which is very power dependent connected to 5 volts. 

    • Cancel
    • Vote Up +3 Vote Down