Merry Boxes & LEDs
  • Challenges & Projects
  • Project14
  • Merry Boxes & LEDs
  • More
  • Cancel
Merry Boxes & LEDs
Blog The Christmas Joy Spreading Machine
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Merry Boxes & LEDs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 23 Dec 2018 5:25 PM Date Created
  • Views 5945 views
  • Likes 20 likes
  • Comments 35 comments
  • all-in-one robotic board
  • merryboxesledsch
  • rotating servo
  • kitronik
  • holidayspecial19ch
  • bbc micro bit
  • glowing
  • neopixel
  • light control
  • servo
  • javascript
  • merry boxes
  • maxim_rt
  • leds
  • buildapresentch
  • blocks
  • let's code
  • motor controller
  • cardboard
  • microservo
Related
Recommended

The Christmas Joy Spreading Machine

balearicdynamics
balearicdynamics
23 Dec 2018
  • The Holiday Boxes & LEDs Video Card (With my Best Wishes to All)
    • Parts and Design
      • Electronic Components
    • Hardware Setup
      • The City Skyline
      • The Big Rotating Gear
      • Coloured Flashlights
      • The Glowing Star
      • The Electret Microphone
    • Software
      • BBC micro:bit Firmware Update
      • Libraries and Sources

The Holiday Boxes & LEDs Video Card (With my Best Wishes to All)

First of all, this machine represents my virtual Best Wishes for these holidays, a  to all the community members So, enjoy the video first and see the notes on the build below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Parts and Design

 

Electronic Components

This project uses a bunch of components for motion and lighting:

 

  • N.4 Microservos for light rotating
  • N.1 Continuous rotation servo to move the big gear of the machine
  • N.4 High Power White LED Lamps (50 cents to the Chinese store)
  • N.2 White LED strip to illuminate the city skyline
  • N.1 12 Neopixel LED ring
  • N.1 Adafruit AGC Electret Microphone Amplifier based on the MAX9814 IC
  • A lot of cardboard, hot glue, paper glue, and spray paint

For those interested to the cardboard and other stuff design and building I have posted a showcase of this project on Hackster.io with some image galleries just on the carboard cutting and assembling.

 

The real challenge of the project has been to make everything working with a single microcontroller board: the BBC micro:bit . I should admit that when I started building the first prototype of the electronic parts on my bench I have considered to include something else like an Arduino Nano to work together but then, as much stuff I was adding to the micro:bit as much the device continued to work well and responsively.

Almost all the parts are controlled by a Kitronik's All-in-one Robotic Board; As I started to test the feature of this board I was very impressed! It can control up to four DC motors (or two stepper motors) AND up to 8 servos, with an independent power source to the external devices while powering the BBC micro:bit. One of the most interesting aspects of this expansion board, IMHO, is communicating to the micro:bit via I2C. In few words, after you have connected all the stuff for your robotic project the micro:bit has already all the available GPIO pins free. I found this invaluable for this project.

 

The design idea was to make a complete scenario representing - inside a box image - a metaphor of the most popular Christmas symbols. Maybe it is a bit distopyc but it moves, lights and reacts to music. The other not easy aspect of the building was just to use the cardboard as the primary material. The central moving parts have been inspired by the incredible quantity of DIY Marble Machines you can find on YouTube (just put the two terms for searching videos and you remain speechless).

 

image

At this point, let me show you what I have put inside.

 

Hardware Setup

 

The City Skyline

The hardware parts have been assembled and tested separately with small programs before starting the assembly of the box. The images below show the white LED strips and the testing effect when placed behind the city skyline. The power supplied to the robot controller - the main power line - is 6.5V 2.5A The two LED strips are originally provided with a USB port to be powered by a max 5V by a power charger or a laptop USB port; to avoid overvoltage I connected two strips together creating a 60 cm LED array.

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Big Rotating Gear

The big rotating gear is the main cardboard engine activated by a smaller gear to the base connected to a continuously rotating servo. The all-in-one robot controller can drive up to eight servos independently; I used five with great result: all of them worked as expected. The images below show the servo connected to the driving gear.

imageimage

imageimage

The video below shows the servo bench testing.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Coloured Flashlights

To make the colored flashlights I have used four cheap high brightness portable flashlights like the one shown in the photo after the complete disassembled.

image

Like the case of the white LED strips these lamps operate with three 1.5V AAA batteries so I connected a couple of them in series to avoid overvoltage. Also, the light reflecting support has been hacked to make it colored. To create the front screen of the lights I have used the top side of four of my preferred transparent sunshade caps.

imageimage

Every light has been glued in a support connected to a microservo to create the rotation

imageimage

Video showing the light mechanism under the bench test.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Glowing Star

The glowing star is a double cardboard star with the fronm side partially open - making a design - with transparent 3D printed plastic cover. The internal part of the star has a 12 NeoPixel LEDs.

imageimage

imageimage

Note that the star uses the micro:bit PIn 16 of the GPIO. Together with the electret microphone is the only device directly connected to the board pinout while all the other parts are managed by the all-in-one robotic board.

 

The Electret Microphone

This device from Adafruit is a simple electret microphone breakout board with the Max 9814 amplifier. It is connected to the analog input Pin 2 of the micro:bit and the periodically read value changes the intensity of the lights depending on the music level. If no music is played around, the rhythmic noise of the servos anyway generates a nice light floating effect.

 

Software

image

I wrote the software in Javascript, to make it easy to be used (fully or partially) also with the visual editor Blocks (that is a different javascript representation). About the software, some important notes.

 

BBC micro:bit Firmware Update

As far as I know, the micro:bit internal libraries managing the I2C and SPI protocols has serious bugs. Someone has no difficulty to use them while in other cases (like me) it seems impossible to work correctly. The Kitronik's all-in-one robotic board communicate with the micro:bit through the I2C protocol; I had serious issues on the first run then I checked the firmware version of my board and it was 2.30 while the last update from the microbit.org site is the version 2.50. Everything worked fine after the firmware update.

To update the firmware of the micro:bit follow the instruction on the microbit.org specific link: https://microbit.org/guide/firmware/

 

Libraries and Sources

The last updated version of the javascript sources is available under a CC 3.0 NC-ND-SA license on GitHub under the Java folder

If you just copy and paste the java sources in the online micro:bit editor does not work. Don't forget to download the libraries from the Extensions option in the blocks online editor. you should install the Kitronik Robotic Library and the Adafruit Neopixel Library.

 

Together with the Javascript source, the folder Components of the repository contains the SVG files with the design of all the cardboard parts you can see in that building as well as the 3D printable STL file with the transparent pieces of the glowing star. These parts have been printed with transparent resing and an ELEGOO MARS LCD 3D printer.

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +5
    Very nice, love the construction. As always, your creation made me smile.
  • 14rhb
    14rhb over 7 years ago +5
    Hi Enrico, That is a great project, and as you usually manage, plenty of fun. It looks like you've made the whole scenario from corrugated cardboard. Are the teeth on the cog also the cardboard with the…
  • kk99
    kk99 over 7 years ago +4
    Enrico, Awesome construction and excellent video. Merry Christmas and Happy New Year.
Parents
  • 14rhb
    14rhb over 7 years ago

    Hi Enrico,

     

    That is a great project, and as you usually manage, plenty of fun.

     

    It looks like you've made the whole scenario from corrugated cardboard. Are the teeth on the cog also the cardboard with the outer layer of paper stripped off?

     

    Happy Christmas to you as well.

     

    Rod

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to 14rhb

    Rod, I am sorry but I have pressed "Publish" instead of "Save to draft" and for this action... There is no way to rollback. I am updating the project with the parts, including on how I made the building so I will document this part in details too.

     

    BTW, yes all has been done with cardboard excluding the transparent glowing part of the star, 3D printed and the base of the machine that is styrene foam because should be thick to keep the servos in place.

     

    Stay in touch on the updates of this project during the next hours.

     

    Cheers, Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to 14rhb

    Rod, I am sorry but I have pressed "Publish" instead of "Save to draft" and for this action... There is no way to rollback. I am updating the project with the parts, including on how I made the building so I will document this part in details too.

     

    BTW, yes all has been done with cardboard excluding the transparent glowing part of the star, 3D printed and the base of the machine that is styrene foam because should be thick to keep the servos in place.

     

    Stay in touch on the updates of this project during the next hours.

     

    Cheers, Enrico

    • Cancel
    • Vote Up +4 Vote Down